<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 P1010 Basic SW Example</title>
    <link>https://community.nxp.com/t5/P-Series/P1010-Basic-SW-Example/m-p/1077459#M4915</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am evaluating the CodeWarior for an embedded platform having P1010 processor.&lt;/P&gt;&lt;P&gt;Currently we are using OS and considering moving without OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P1010 starts at the end of the flash - where we program the boot SW.&lt;/P&gt;&lt;P&gt;Today, out boot SW copies the application SW to the ram and executes it.&lt;/P&gt;&lt;P&gt;So it already configures the processor (TLBs etc) in asm - so it ca be reused in the codewarior (as it has no OS).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is - as I want to create an Application to be loaded by the boot.&lt;/P&gt;&lt;P&gt;How should I do it?&lt;/P&gt;&lt;P&gt;Should I create a the second application and just jump to the start of it, then it will be copied to the ram - per the linker files (.lcf)?&lt;/P&gt;&lt;P&gt;Since I also want the .text and everything to reside in the RAM so will fully execute from RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe can reference to an example project from which I can start?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yoav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Aug 2020 08:44:36 GMT</pubDate>
    <dc:creator>yoavbaryoseph</dc:creator>
    <dc:date>2020-08-10T08:44:36Z</dc:date>
    <item>
      <title>P1010 Basic SW Example</title>
      <link>https://community.nxp.com/t5/P-Series/P1010-Basic-SW-Example/m-p/1077459#M4915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am evaluating the CodeWarior for an embedded platform having P1010 processor.&lt;/P&gt;&lt;P&gt;Currently we are using OS and considering moving without OS.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P1010 starts at the end of the flash - where we program the boot SW.&lt;/P&gt;&lt;P&gt;Today, out boot SW copies the application SW to the ram and executes it.&lt;/P&gt;&lt;P&gt;So it already configures the processor (TLBs etc) in asm - so it ca be reused in the codewarior (as it has no OS).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The question is - as I want to create an Application to be loaded by the boot.&lt;/P&gt;&lt;P&gt;How should I do it?&lt;/P&gt;&lt;P&gt;Should I create a the second application and just jump to the start of it, then it will be copied to the ram - per the linker files (.lcf)?&lt;/P&gt;&lt;P&gt;Since I also want the .text and everything to reside in the RAM so will fully execute from RAM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maybe can reference to an example project from which I can start?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yoav&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2020 08:44:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010-Basic-SW-Example/m-p/1077459#M4915</guid>
      <dc:creator>yoavbaryoseph</dc:creator>
      <dc:date>2020-08-10T08:44:36Z</dc:date>
    </item>
    <item>
      <title>Re: P1010 Basic SW Example</title>
      <link>https://community.nxp.com/t5/P-Series/P1010-Basic-SW-Example/m-p/1077460#M4916</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&amp;nbsp;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Yoav,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Please download and install CodeWarrior 10.5.1 for PowerPC architecture.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Then create a sample bareboard project from File-&amp;gt;New-&amp;gt;CodeWarrior Bareboard project Wizards, please refer to "Section B: Creating, Building, and Debugging a Project" in the attached document.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Thanks,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;Yiping&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 11 Aug 2020 07:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1010-Basic-SW-Example/m-p/1077460#M4916</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-08-11T07:33:55Z</dc:date>
    </item>
  </channel>
</rss>