<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: P4080DS reflector is not working in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249748#M475</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The application reflector is a USDPAA based sample program, please make sure that you have boot up your system with a USDPAA dtb "uImage-p4080ds-usdpaa.dtb".&lt;/P&gt;&lt;P&gt;Before running USDPAA application, it is required to configure frame manger for the interfaces that will receive traffic. please use FMC commands on your target before start the reflector application. for example,&lt;/P&gt;&lt;P&gt;$ cd /usr/etc/&lt;/P&gt;&lt;P&gt;$ fmc –c usdpaa_config_p4_serdes_0x10.xml –p usdpaa_policy_hash_ipv4.xml –a.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use shared MAC between USDPAA and Linux, you could use the shared MAC dtb file&amp;nbsp; p4080ds-usdpaa-shared-interfaces.dtb and shared MAC policy usdpaa_policy_hash_shared_mac_ipv4.xml.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the Linux Kernel ping problem, please make sure fman ucode has been flashed correctly and MAC address has been configured correctly, please check whether this port can work in u-boot.&lt;/P&gt;&lt;P&gt;In application, please pay attention to the following configuration.&lt;/P&gt;&lt;P&gt;• SGMII card goes in P4080DS slot 3.&lt;/P&gt;&lt;P&gt;• Use SerDes 0x10 and RCW file: R_PPSXN_0x10/rcw_5g_1500mhz.bin in the&lt;/P&gt;&lt;P&gt;P4080DS NOR flash. This is a different RCW file than the one discussed above.&lt;/P&gt;&lt;P&gt;• Boot into bank 4 (assuming you are using bank 4 for USDPAA).&lt;/P&gt;&lt;P&gt;• Add text ";serdes:fsl_srds_lpd_b2=0xf" to u-boot environment variable hwconfig,&lt;/P&gt;&lt;P&gt;saveenv, and reset the system again into bank 4. This disables fm2-10g. The leading&lt;/P&gt;&lt;P&gt;";" separates the information added to hwconfig from what was already there. Note&lt;/P&gt;&lt;P&gt;that fm1-10g is never available in SerDes 0x10.&lt;/P&gt;&lt;P&gt;• Delete references to any of the 10 Gbps interfaces and ensure references to all&lt;/P&gt;&lt;P&gt;USDPAA 1 Gbps interfaces are present in the fmc configuration file. For example, it&lt;/P&gt;&lt;P&gt;should like the following after you edit it:&lt;/P&gt;&lt;P&gt;&amp;lt;cfgdata&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;config&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;engine name="fm1"&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="0" policy="hash_ipv4_policy_5"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="1" policy="hash_ipv4_policy_6"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="2" policy="hash_ipv4_policy_7"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="3" policy="hash_ipv4_policy_8"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/engine&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/config&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/cfgdata&amp;gt;&lt;/P&gt;&lt;P&gt;Run the USDPAA application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Nov 2013 09:11:15 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2013-11-01T09:11:15Z</dc:date>
    <item>
      <title>P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249747#M474</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am new to Freescale so my questions might be very basic&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. How to identify the revision of P4080DS board?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; My u-boot prints "CPU0:&amp;nbsp; P4080E, Version: 3.0" in the very startup, is this the revision?&lt;/P&gt;&lt;P&gt;2. as per the SDK fm1-gb1 port is used for Linux kernel which is on the main board, I am not able to ping through this port even the ifconfig shows it is RUNNING, port has RED led&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; contantly.&lt;/P&gt;&lt;P&gt;3. I do not have any XAUI card so I programmed SerDes 0x10 RCW &lt;STRONG style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;rcw_5g_1500mhz.bin, uboot, fman&lt;/STRONG&gt; to the flash and boot from bank4, I loaded fsl-image-core and trying sample&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; application reflector but it is giving following error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERR : Invocation of FM_PORT_Open for fm1/port/1G/3 failed&lt;/P&gt;&lt;P&gt;ERR : Invocation of FM_PCD_Disable for fm0/pcd failed with error code 0x00010028&lt;/P&gt;&lt;P&gt;Found /fsl,dpaa/dpa-fman0-oh@1, Tx Channel = 46, FMAN = 0, Port ID = 1&lt;/P&gt;&lt;P&gt;Found /fsl,dpaa/ethernet@5, Tx Channel = 61, FMAN = 1, Port ID = 0&lt;/P&gt;&lt;P&gt;Found /fsl,dpaa/ethernet@6, Tx Channel = 62, FMAN = 1, Port ID = 1&lt;/P&gt;&lt;P&gt;Found /fsl,dpaa/ethernet@7, Tx Channel = 63, FMAN = 1, Port ID = 2&lt;/P&gt;&lt;P&gt;ERR: drivers/fman/fman.c:279:fman_if_init()&lt;/P&gt;&lt;P&gt;Unknown error -22: /soc@ffe000000/fman@500000/ethernet@e6000: no local-mac-address&lt;/P&gt;&lt;P&gt;ERR: drivers/fman/fman.c:449:fman_init()&lt;/P&gt;&lt;P&gt;Unknown error -22: if_init(/fsl,dpaa/ethernet@8)&lt;/P&gt;&lt;P&gt;Tearing down /fsl,dpaa/ethernet@5&lt;/P&gt;&lt;P&gt;Tearing down /fsl,dpaa/ethernet@6&lt;/P&gt;&lt;P&gt;Tearing down /fsl,dpaa/ethernet@7&lt;/P&gt;&lt;P&gt;apps/lib/usdpaa_netcfg_layer.c:488:usdpaa_netcfg_acquire(): fman driver init failed (ERRNO = -22)&lt;/P&gt;&lt;P&gt;error: failed to load configuration&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I followed the steps given by the SDK. Any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Oct 2013 09:29:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249747#M474</guid>
      <dc:creator>ankur</dc:creator>
      <dc:date>2013-10-31T09:29:34Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249748#M475</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The application reflector is a USDPAA based sample program, please make sure that you have boot up your system with a USDPAA dtb "uImage-p4080ds-usdpaa.dtb".&lt;/P&gt;&lt;P&gt;Before running USDPAA application, it is required to configure frame manger for the interfaces that will receive traffic. please use FMC commands on your target before start the reflector application. for example,&lt;/P&gt;&lt;P&gt;$ cd /usr/etc/&lt;/P&gt;&lt;P&gt;$ fmc –c usdpaa_config_p4_serdes_0x10.xml –p usdpaa_policy_hash_ipv4.xml –a.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you want to use shared MAC between USDPAA and Linux, you could use the shared MAC dtb file&amp;nbsp; p4080ds-usdpaa-shared-interfaces.dtb and shared MAC policy usdpaa_policy_hash_shared_mac_ipv4.xml.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About the Linux Kernel ping problem, please make sure fman ucode has been flashed correctly and MAC address has been configured correctly, please check whether this port can work in u-boot.&lt;/P&gt;&lt;P&gt;In application, please pay attention to the following configuration.&lt;/P&gt;&lt;P&gt;• SGMII card goes in P4080DS slot 3.&lt;/P&gt;&lt;P&gt;• Use SerDes 0x10 and RCW file: R_PPSXN_0x10/rcw_5g_1500mhz.bin in the&lt;/P&gt;&lt;P&gt;P4080DS NOR flash. This is a different RCW file than the one discussed above.&lt;/P&gt;&lt;P&gt;• Boot into bank 4 (assuming you are using bank 4 for USDPAA).&lt;/P&gt;&lt;P&gt;• Add text ";serdes:fsl_srds_lpd_b2=0xf" to u-boot environment variable hwconfig,&lt;/P&gt;&lt;P&gt;saveenv, and reset the system again into bank 4. This disables fm2-10g. The leading&lt;/P&gt;&lt;P&gt;";" separates the information added to hwconfig from what was already there. Note&lt;/P&gt;&lt;P&gt;that fm1-10g is never available in SerDes 0x10.&lt;/P&gt;&lt;P&gt;• Delete references to any of the 10 Gbps interfaces and ensure references to all&lt;/P&gt;&lt;P&gt;USDPAA 1 Gbps interfaces are present in the fmc configuration file. For example, it&lt;/P&gt;&lt;P&gt;should like the following after you edit it:&lt;/P&gt;&lt;P&gt;&amp;lt;cfgdata&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;config&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;engine name="fm1"&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="0" policy="hash_ipv4_policy_5"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="1" policy="hash_ipv4_policy_6"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="2" policy="hash_ipv4_policy_7"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;port type="1G" number="3" policy="hash_ipv4_policy_8"/&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/engine&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/config&amp;gt;&lt;/P&gt;&lt;P&gt;&amp;lt;/cfgdata&amp;gt;&lt;/P&gt;&lt;P&gt;Run the USDPAA application.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2013 09:11:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249748#M475</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2013-11-01T09:11:15Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249749#M476</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your inputs, I will cross check on the dtb in use, for ping&lt;/P&gt;&lt;P&gt;issue some more questions&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. I am not able to ping using FM1@DTSEC2 port at all, I tried many times.&lt;/P&gt;&lt;P&gt;FMan was loaded, following is the boot log&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. I also do not have p4080ds-usdpaa-shared-interfaces.dtb file in image&lt;/P&gt;&lt;P&gt;directory, do we need to generate it by running some&lt;/P&gt;&lt;P&gt;special command.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2013.01 (Oct 21 2013 - 20:07:45)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU0:  P4080E, Version: 3.0, (0x82080030)&lt;/P&gt;&lt;P&gt;Core:  E500MC, Version: 3.1, (0x80230031)&lt;/P&gt;&lt;P&gt;Clock Configuration:&lt;/P&gt;&lt;P&gt;       CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,&lt;/P&gt;&lt;P&gt;CPU3:1499.985 MHz,&lt;/P&gt;&lt;P&gt;       CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,&lt;/P&gt;&lt;P&gt;CPU7:1499.985 MHz,&lt;/P&gt;&lt;P&gt;       CCB:799.992 MHz,&lt;/P&gt;&lt;P&gt;       DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999&lt;/P&gt;&lt;P&gt;MHz&lt;/P&gt;&lt;P&gt;       FMAN1: 599.994 MHz&lt;/P&gt;&lt;P&gt;       FMAN2: 599.994 MHz&lt;/P&gt;&lt;P&gt;       QMAN:  399.996 MHz&lt;/P&gt;&lt;P&gt;       PME:   599.994 MHz&lt;/P&gt;&lt;P&gt;L1:    D-cache 32 kB enabled&lt;/P&gt;&lt;P&gt;       I-cache 32 kB enabled&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;/P&gt;&lt;P&gt;       00000000: 105a0000 00000000 1e1e181e 0000cccc&lt;/P&gt;&lt;P&gt;       00000010: 40464000 3c3c2000 de800000 e1000000&lt;/P&gt;&lt;P&gt;       00000020: 00000000 00000000 00000000 008b6000&lt;/P&gt;&lt;P&gt;       00000030: 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4&lt;/P&gt;&lt;P&gt;SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz&lt;/P&gt;&lt;P&gt;I2C:   ready&lt;/P&gt;&lt;P&gt;SPI:   ready&lt;/P&gt;&lt;P&gt;DRAM:  Initializing....using SPD&lt;/P&gt;&lt;P&gt;Detected UDIMM i-DIMM&lt;/P&gt;&lt;P&gt;Detected UDIMM i-DIMM&lt;/P&gt;&lt;P&gt;2 GiB left unmapped&lt;/P&gt;&lt;P&gt;4 GiB (DDR3, 64-bit, CL=9, ECC off)&lt;/P&gt;&lt;P&gt;       DDR Controller Interleaving Mode: cache line&lt;/P&gt;&lt;P&gt;       DDR Chip-Select Interleaving Mode: CS0+CS1&lt;/P&gt;&lt;P&gt;Testing 0x00000000 - 0x7fffffff&lt;/P&gt;&lt;P&gt;Testing 0x80000000 - 0xffffffff&lt;/P&gt;&lt;P&gt;Remap DDR 2 GiB left unmapped&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POST memory PASSED&lt;/P&gt;&lt;P&gt;Flash: 128 MiB&lt;/P&gt;&lt;P&gt;L2:    128 KB enabled&lt;/P&gt;&lt;P&gt;Corenet Platform Cache: 2048 KB enabled&lt;/P&gt;&lt;P&gt;SERDES: bank 2 disabled&lt;/P&gt;&lt;P&gt;SERDES: bank 3 disabled&lt;/P&gt;&lt;P&gt;SRIO1: disabled&lt;/P&gt;&lt;P&gt;SRIO2: disabled&lt;/P&gt;&lt;P&gt;MMC:  FSL_SDHC: 0&lt;/P&gt;&lt;P&gt;EEPROM: NXID v1&lt;/P&gt;&lt;P&gt;PCIe1: Root Complex, no link, regs @ 0xfe200000&lt;/P&gt;&lt;P&gt;PCIe1: Bus 00 - 00&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex, x1, regs @ 0xfe202000&lt;/P&gt;&lt;P&gt;  02:00.0     - 1095:3132 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe3: Bus 01 - 02&lt;/P&gt;&lt;P&gt;In:    serial&lt;/P&gt;&lt;P&gt;Out:   serial&lt;/P&gt;&lt;P&gt;Err:   serial&lt;/P&gt;&lt;P&gt;Net:   Fman1: Uploading microcode version 106.2.9&lt;/P&gt;&lt;P&gt;PHY reset timed out&lt;/P&gt;&lt;P&gt;Fman2: Uploading microcode version 106.2.9&lt;/P&gt;&lt;P&gt;FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot: 10     0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ankur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Fri, Nov 1, 2013 at 2:41 PM, Yiping Wang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Nov 2013 09:29:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249749#M476</guid>
      <dc:creator>ankur</dc:creator>
      <dc:date>2013-11-01T09:29:39Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249750#M477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you set these parameters in u-boot?&lt;/P&gt;&lt;P&gt;setenv ethact FM1@DTSEC2&lt;/P&gt;&lt;P&gt;setenv ethprime FM1@DTSEC2&lt;/P&gt;&lt;P&gt;Would you please share your u-boot environment variables and ping log?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In order to build p4080ds-usdpaa-shared-interfaces.dtb, please add "${S}/arch/powerpc/boot/dts/p4080ds-usdpaa-shared-interfaces.dts in variable&amp;nbsp; KERNEL_DEVICETREE in meta-fsl-ppc/conf/machine/p4080ds.conf.&lt;/P&gt;&lt;P&gt;Then rebuild Kernel.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 08:37:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249750#M477</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2013-11-04T08:37:07Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249751#M478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for you reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am attaching logs from our board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;######################################################&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2011.12-00064-gbfb0c9a (Jun 15 2012 - 16:09:09)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU0:  P4080E, Version: 3.0, (0x82080030)&lt;/P&gt;&lt;P&gt;Core:  E500MC, Version: 3.1, (0x80230031)&lt;/P&gt;&lt;P&gt;Clock Configuration:&lt;/P&gt;&lt;P&gt;       CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,&lt;/P&gt;&lt;P&gt;CPU3:1499.985 MHz,&lt;/P&gt;&lt;P&gt;       CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,&lt;/P&gt;&lt;P&gt;CPU7:1499.985 MHz,&lt;/P&gt;&lt;P&gt;       CCB:799.992 MHz,&lt;/P&gt;&lt;P&gt;       DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999&lt;/P&gt;&lt;P&gt;MHz&lt;/P&gt;&lt;P&gt;       FMAN1: 599.994 MHz&lt;/P&gt;&lt;P&gt;       FMAN2: 599.994 MHz&lt;/P&gt;&lt;P&gt;       PME:   399.996 MHz&lt;/P&gt;&lt;P&gt;L1:    D-cache 32 kB enabled&lt;/P&gt;&lt;P&gt;       I-cache 32 kB enabled&lt;/P&gt;&lt;P&gt;Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 0&lt;/P&gt;&lt;P&gt;36-bit Addressing&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;/P&gt;&lt;P&gt;       00000000: 105a0000 00000000 1e1e181e 0000cccc&lt;/P&gt;&lt;P&gt;       00000010: 40464000 3c3c2000 fe800000 61000000&lt;/P&gt;&lt;P&gt;       00000020: 00000000 00000000 00000000 008b6000&lt;/P&gt;&lt;P&gt;       00000030: 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz&lt;/P&gt;&lt;P&gt;I2C:   ready&lt;/P&gt;&lt;P&gt;SPI:   ready&lt;/P&gt;&lt;P&gt;DRAM:  Initializing....using SPD&lt;/P&gt;&lt;P&gt;Detected UDIMM i-DIMM&lt;/P&gt;&lt;P&gt;Detected UDIMM i-DIMM&lt;/P&gt;&lt;P&gt;CS2 is disabled.&lt;/P&gt;&lt;P&gt;CS3 is disabled.&lt;/P&gt;&lt;P&gt;CS2 is disabled.&lt;/P&gt;&lt;P&gt;CS3 is disabled.&lt;/P&gt;&lt;P&gt;2 GiB left unmapped&lt;/P&gt;&lt;P&gt;4 GiB (DDR3, 64-bit, CL=9, ECC off)&lt;/P&gt;&lt;P&gt;       DDR Controller Interleaving Mode: cache line&lt;/P&gt;&lt;P&gt;       DDR Chip-Select Interleaving Mode: CS0+CS1&lt;/P&gt;&lt;P&gt;Testing 0x00000000 - 0x7fffffff&lt;/P&gt;&lt;P&gt;Testing 0x80000000 - 0xffffffff&lt;/P&gt;&lt;P&gt;Remap DDR 2 GiB left unmapped&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POST memory PASSED&lt;/P&gt;&lt;P&gt;Flash: 128 MiB&lt;/P&gt;&lt;P&gt;L2:    128 KB enabled&lt;/P&gt;&lt;P&gt;Corenet Platform Cache: 2048 KB enabled&lt;/P&gt;&lt;P&gt;SERDES: bank 2 disabled&lt;/P&gt;&lt;P&gt;SERDES: bank 3 disabled&lt;/P&gt;&lt;P&gt;SRIO1: disabled&lt;/P&gt;&lt;P&gt;SRIO2: disabled&lt;/P&gt;&lt;P&gt;MMC:  FSL_SDHC: 0&lt;/P&gt;&lt;P&gt;EEPROM: NXID v1&lt;/P&gt;&lt;P&gt;PCIe1: Root Complex, no link, regs @ 0xfe200000&lt;/P&gt;&lt;P&gt;PCIe1: Bus 00 - 00&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex, x1, regs @ 0xfe202000&lt;/P&gt;&lt;P&gt;  02:00.0     - 1095:3132 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe3: Bus 01 - 02&lt;/P&gt;&lt;P&gt;In:    serial&lt;/P&gt;&lt;P&gt;Out:   serial&lt;/P&gt;&lt;P&gt;Err:   serial&lt;/P&gt;&lt;P&gt;Net:   Fman1: Uploading microcode version 106.2.0&lt;/P&gt;&lt;P&gt;Fman2: Uploading microcode version 106.2.0&lt;/P&gt;&lt;P&gt;FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot:  5     4     3     2     1     0 ÿ&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;U-Boot 2013.01 (Oct 21 2013 - 20:07:45)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;CPU0:  P4080E, Version: 3.0, (0x82080030)&lt;/P&gt;&lt;P&gt;Core:  E500MC, Version: 3.1, (0x80230031)&lt;/P&gt;&lt;P&gt;Clock Configuration:&lt;/P&gt;&lt;P&gt;       CPU0:1499.985 MHz, CPU1:1499.985 MHz, CPU2:1499.985 MHz,&lt;/P&gt;&lt;P&gt;CPU3:1499.985 MHz,&lt;/P&gt;&lt;P&gt;       CPU4:1499.985 MHz, CPU5:1499.985 MHz, CPU6:1499.985 MHz,&lt;/P&gt;&lt;P&gt;CPU7:1499.985 MHz,&lt;/P&gt;&lt;P&gt;       CCB:799.992 MHz,&lt;/P&gt;&lt;P&gt;       DDR:649.994 MHz (1299.987 MT/s data rate) (Asynchronous), LBC:99.999&lt;/P&gt;&lt;P&gt;MHz&lt;/P&gt;&lt;P&gt;       FMAN1: 599.994 MHz&lt;/P&gt;&lt;P&gt;       FMAN2: 599.994 MHz&lt;/P&gt;&lt;P&gt;       QMAN:  399.996 MHz&lt;/P&gt;&lt;P&gt;       PME:   599.994 MHz&lt;/P&gt;&lt;P&gt;L1:    D-cache 32 kB enabled&lt;/P&gt;&lt;P&gt;       I-cache 32 kB enabled&lt;/P&gt;&lt;P&gt;Reset Configuration Word (RCW):&lt;/P&gt;&lt;P&gt;       00000000: 105a0000 00000000 1e1e181e 0000cccc&lt;/P&gt;&lt;P&gt;       00000010: 40464000 3c3c2000 de800000 e1000000&lt;/P&gt;&lt;P&gt;       00000020: 00000000 00000000 00000000 008b6000&lt;/P&gt;&lt;P&gt;       00000030: 00000000 00000000 00000000 00000000&lt;/P&gt;&lt;P&gt;Board: P4080DS, Sys ID: 0x17, Sys Ver: 0x01, FPGA Ver: 0x0c, vBank: 4&lt;/P&gt;&lt;P&gt;SERDES Reference Clocks: Bank1=100MHz Bank2=125MHz Bank3=125MHz&lt;/P&gt;&lt;P&gt;I2C:   ready&lt;/P&gt;&lt;P&gt;SPI:   ready&lt;/P&gt;&lt;P&gt;DRAM:  Initializing....using SPD&lt;/P&gt;&lt;P&gt;Detected UDIMM i-DIMM&lt;/P&gt;&lt;P&gt;Detected UDIMM i-DIMM&lt;/P&gt;&lt;P&gt;2 GiB left unmapped&lt;/P&gt;&lt;P&gt;4 GiB (DDR3, 64-bit, CL=9, ECC off)&lt;/P&gt;&lt;P&gt;       DDR Controller Interleaving Mode: cache line&lt;/P&gt;&lt;P&gt;       DDR Chip-Select Interleaving Mode: CS0+CS1&lt;/P&gt;&lt;P&gt;Testing 0x00000000 - 0x7fffffff&lt;/P&gt;&lt;P&gt;Testing 0x80000000 - 0xffffffff&lt;/P&gt;&lt;P&gt;Remap DDR 2 GiB left unmapped&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;POST memory PASSED&lt;/P&gt;&lt;P&gt;Flash: 128 MiB&lt;/P&gt;&lt;P&gt;L2:    128 KB enabled&lt;/P&gt;&lt;P&gt;Corenet Platform Cache: 2048 KB enabled&lt;/P&gt;&lt;P&gt;SERDES: bank 2 disabled&lt;/P&gt;&lt;P&gt;SERDES: bank 3 disabled&lt;/P&gt;&lt;P&gt;SRIO1: disabled&lt;/P&gt;&lt;P&gt;SRIO2: disabled&lt;/P&gt;&lt;P&gt;MMC:  FSL_SDHC: 0&lt;/P&gt;&lt;P&gt;EEPROM: NXID v1&lt;/P&gt;&lt;P&gt;PCIe1: Root Complex, no link, regs @ 0xfe200000&lt;/P&gt;&lt;P&gt;PCIe1: Bus 00 - 00&lt;/P&gt;&lt;P&gt;PCIe2: disabled&lt;/P&gt;&lt;P&gt;PCIe3: Root Complex, x1, regs @ 0xfe202000&lt;/P&gt;&lt;P&gt;  02:00.0     - 1095:3132 - Mass storage controller&lt;/P&gt;&lt;P&gt;PCIe3: Bus 01 - 02&lt;/P&gt;&lt;P&gt;In:    serial&lt;/P&gt;&lt;P&gt;Out:   serial&lt;/P&gt;&lt;P&gt;Err:   serial&lt;/P&gt;&lt;P&gt;Net:   Fman1: Uploading microcode version 106.2.9&lt;/P&gt;&lt;P&gt;PHY reset timed out&lt;/P&gt;&lt;P&gt;Fman2: Uploading microcode version 106.2.9&lt;/P&gt;&lt;P&gt;FM1@DTSEC2, FM2@DTSEC1, FM2@DTSEC2, FM2@DTSEC3, FM2@DTSEC4&lt;/P&gt;&lt;P&gt;Hit any key to stop autoboot: 10     0&lt;/P&gt;&lt;P&gt;=&amp;gt; printenv&lt;/P&gt;&lt;P&gt;baudrate=115200&lt;/P&gt;&lt;P&gt;bdev=sda3&lt;/P&gt;&lt;P&gt;bootargs=root=/dev/nfs rw nfsroot=172.16.124.136:/home/hitachi/tftpboot/yocto&lt;/P&gt;&lt;P&gt;ip=172.16.124.153:172.16.124.136::255.255.255.128::eth1:off&lt;/P&gt;&lt;P&gt;console=ttyS0,115200 usdpaa_mem=256M,1G&lt;/P&gt;&lt;P&gt;bootcmd=run cboot&lt;/P&gt;&lt;P&gt;bootdef=bootm 0xec020000 0xed300000 0xec800000&lt;/P&gt;&lt;P&gt;bootdelay=10&lt;/P&gt;&lt;P&gt;bootfile=uImage-p4080ds.bin&lt;/P&gt;&lt;P&gt;c=ffe&lt;/P&gt;&lt;P&gt;cboot=tftp 1000000 uImage-p4080ds.bin;tftp 0x2000000&lt;/P&gt;&lt;P&gt;fsl-image-core-p4080ds.ext2.gz.u-boot; tftp c00000&lt;/P&gt;&lt;P&gt;uImage-p4080ds-usdpaa.dtb;setenv bootargs usdpaa_mem=256M&lt;/P&gt;&lt;P&gt;usdpaa_mem=256M,1G;bootm 1000000 0x2000000 c00000&lt;/P&gt;&lt;P&gt;consoledev=ttyS0&lt;/P&gt;&lt;P&gt;eth1addr=00:04:9F:02:85:91&lt;/P&gt;&lt;P&gt;eth2addr=00:04:9F:02:85:92&lt;/P&gt;&lt;P&gt;eth3addr=00:04:9F:02:85:93&lt;/P&gt;&lt;P&gt;eth4addr=00:04:9F:02:85:94&lt;/P&gt;&lt;P&gt;eth5addr=00:04:9F:02:85:95&lt;/P&gt;&lt;P&gt;eth6addr=00:04:9F:02:85:96&lt;/P&gt;&lt;P&gt;eth7addr=00:04:9F:02:85:97&lt;/P&gt;&lt;P&gt;ethact=FM1@DTSEC2&lt;/P&gt;&lt;P&gt;ethaddr=00:04:9F:02:85:90&lt;/P&gt;&lt;P&gt;ethprime=FM1@DTSEC1&lt;/P&gt;&lt;P&gt;fdtaddr=c00000&lt;/P&gt;&lt;P&gt;fdtfile=uImage-p4080ds-usdpaa.dtb&lt;/P&gt;&lt;P&gt;fman_ucode=0xeff40000&lt;/P&gt;&lt;P&gt;gateway=172.16.124.129&lt;/P&gt;&lt;P&gt;hwconfig=serdes:fsl_srds_lpd_b2=0xf;fsl_ddr:ctlr_intlv=cacheline,bank_intlv=cs0_cs1,ecc=off&lt;/P&gt;&lt;P&gt;ipaddr=172.16.124.153&lt;/P&gt;&lt;P&gt;loadaddr=1000000&lt;/P&gt;&lt;P&gt;netdev=eth1&lt;/P&gt;&lt;P&gt;netmask=255.255.255.128&lt;/P&gt;&lt;P&gt;nfsboot=setenv bootargs root=/dev/nfs rw nfsroot=$serverip:$rootpath&lt;/P&gt;&lt;P&gt;ip=$ipaddr:$serverip:$gatewayip:$netmask:$hostname:$netdev:off&lt;/P&gt;&lt;P&gt;console=$consoledev,$baudrate $othbootargs;tftp $loadaddr $bootfile;tftp&lt;/P&gt;&lt;P&gt;$fdtaddr $fdtfile;bootm $loadaddr - $fdtaddr&lt;/P&gt;&lt;P&gt;othbootargs=bportals=s0-1 qportals=s0-1&lt;/P&gt;&lt;P&gt;ramboot=setenv bootargs root=/dev/ram rw console=$consoledev,$baudrate&lt;/P&gt;&lt;P&gt;$othbootargs;tftp $ramdiskaddr $ramdiskfile;tftp $loadaddr $bootfile;tftp&lt;/P&gt;&lt;P&gt;$fdtaddr $fdtfile;bootm $loadaddr $ramdiskaddr $fdtaddr&lt;/P&gt;&lt;P&gt;ramdiskaddr=2000000&lt;/P&gt;&lt;P&gt;ramdiskfile=p4080ds/ramdisk.uboot&lt;/P&gt;&lt;P&gt;rfsaddr=0x2000000&lt;/P&gt;&lt;P&gt;rfsfile=fsl-image-core-p4080ds.ext2.gz.u-boot&lt;/P&gt;&lt;P&gt;rootpath=/home/hitachi/tftpboot/yocto&lt;/P&gt;&lt;P&gt;serverip=172.16.124.136&lt;/P&gt;&lt;P&gt;stderr=serial&lt;/P&gt;&lt;P&gt;stdin=serial&lt;/P&gt;&lt;P&gt;stdout=serial&lt;/P&gt;&lt;P&gt;tftpflash=tftpboot $loadaddr $uboot &amp;amp;&amp;amp; protect off $ubootaddr +$filesize &amp;amp;&amp;amp;&lt;/P&gt;&lt;P&gt;erase $ubootaddr +$filesize &amp;amp;&amp;amp; cp.b $loadaddr $ubootaddr $filesize &amp;amp;&amp;amp;&lt;/P&gt;&lt;P&gt;protect on $ubootaddr +$filesize &amp;amp;&amp;amp; cmp.b $loadaddr $ubootaddr $filesize&lt;/P&gt;&lt;P&gt;uboot=u-boot.bin&lt;/P&gt;&lt;P&gt;ubootaddr=0xeff80000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Environment size: 2117/8188 bytes&lt;/P&gt;&lt;P&gt;=&amp;gt; run coo      boot&lt;/P&gt;&lt;P&gt;Using FM1@DTSEC2 device&lt;/P&gt;&lt;P&gt;TFTP from server 172.16.124.136; our IP address is 172.16.124.153&lt;/P&gt;&lt;P&gt;Filename 'uImage-p4080ds.bin'.&lt;/P&gt;&lt;P&gt;Load address: 0x1000000&lt;/P&gt;&lt;P&gt;Loading: * T T T T T T T T T T&lt;/P&gt;&lt;P&gt;Retry count exceeded; starting again&lt;/P&gt;&lt;P&gt;Using FM2@DTSEC1 device&lt;/P&gt;&lt;P&gt;TFTP from server 172.16.124.136; our IP address is 172.16.124.153&lt;/P&gt;&lt;P&gt;Filename 'uImage-p4080ds.bin'.&lt;/P&gt;&lt;P&gt;Load address: 0x1000000&lt;/P&gt;&lt;P&gt;Loading: * #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; ##########&lt;/P&gt;&lt;P&gt; 12.9 MiB/s&lt;/P&gt;&lt;P&gt;done&lt;/P&gt;&lt;P&gt;Bytes transferred = 3956560 (3c5f50 hex)&lt;/P&gt;&lt;P&gt;Using FM2@DTSEC1 device&lt;/P&gt;&lt;P&gt;TFTP from server 172.16.124.136; our IP address is 172.16.124.153&lt;/P&gt;&lt;P&gt;Filename 'fsl-image-core-p4080ds.ext2.gz.u-boot'.&lt;/P&gt;&lt;P&gt;Load address: 0x2000000&lt;/P&gt;&lt;P&gt;Loading: * #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #################################################################&lt;/P&gt;&lt;P&gt; #######################################################&lt;/P&gt;&lt;P&gt; 13 MiB/s&lt;/P&gt;&lt;P&gt;done&lt;/P&gt;&lt;P&gt;Bytes transferred = 27522881 (1a3f741 hex)&lt;/P&gt;&lt;P&gt;Using FM2@DTSEC1 device&lt;/P&gt;&lt;P&gt;TFTP from server 172.16.124.136; our IP address is 172.16.124.153&lt;/P&gt;&lt;P&gt;Filename 'uImage-p4080ds-usdpaa.dtb'.&lt;/P&gt;&lt;P&gt;Load address: 0xc00000&lt;/P&gt;&lt;P&gt;Loading: * ####&lt;/P&gt;&lt;P&gt; 10.2 MiB/s&lt;/P&gt;&lt;P&gt;done&lt;/P&gt;&lt;P&gt;Bytes transferred = 53467 (d0db hex)&lt;/P&gt;&lt;P&gt;WARNING: adjusting available memory to 30000000&lt;/P&gt;&lt;OL&gt;&lt;OL&gt;&lt;LI level="2" type="ol"&gt;&lt;P&gt;Booting kernel from Legacy Image at 01000000 ...&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/OL&gt;&lt;P&gt;   Image Name:   Linux-3.8.13-rt9-QorIQ-SDK-V1.4&lt;/P&gt;&lt;P&gt;   Image Type:   PowerPC Linux Kernel Image (gzip compressed)&lt;/P&gt;&lt;P&gt;   Data Size:    3956496 Bytes = 3.8 MiB&lt;/P&gt;&lt;P&gt;   Load Address: 00000000&lt;/P&gt;&lt;P&gt;   Entry Point:  00000000&lt;/P&gt;&lt;P&gt;   Verifying Checksum ... OK&lt;/P&gt;&lt;OL&gt;&lt;OL&gt;&lt;LI level="2" type="ol"&gt;&lt;P&gt;Loading init Ramdisk from Legacy Image at 02000000 ...&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/OL&gt;&lt;P&gt;   Image Name:   fsl-image-core-p4080ds-201310240&lt;/P&gt;&lt;P&gt;   Image Type:   PowerPC Linux RAMDisk Image (gzip compressed)&lt;/P&gt;&lt;P&gt;   Data Size:    27522817 Bytes = 26.2 MiB&lt;/P&gt;&lt;P&gt;   Load Address: 00000000&lt;/P&gt;&lt;P&gt;   Entry Point:  00000000&lt;/P&gt;&lt;P&gt;   Verifying Checksum ... OK&lt;/P&gt;&lt;OL&gt;&lt;OL&gt;&lt;LI level="2" type="ol"&gt;&lt;P&gt;Flattened Device Tree blob at 00c00000&lt;/P&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;/OL&gt;&lt;P&gt;   Booting using the fdt blob at 0x00c00000&lt;/P&gt;&lt;P&gt;   Uncompressing Kernel Image ... OK&lt;/P&gt;&lt;P&gt;   Loading Ramdisk to 2e5c0000, end 2ffff701 ... OK&lt;/P&gt;&lt;P&gt;   Loading Device Tree to 03fdf000, end 03fff0da ... OK&lt;/P&gt;&lt;P&gt;ERROR, usdpaa_mem arg is invalid&lt;/P&gt;&lt;P&gt;Using P4080 DS machine description&lt;/P&gt;&lt;P&gt;Memory CAM mapping: 256/256/256 Mb, residual: 3328Mb&lt;/P&gt;&lt;P&gt;Linux version 3.8.13-rt9-QorIQ-SDK-V1.4 (hitachi@HITTACHI-24) (gcc version&lt;/P&gt;&lt;P&gt;4.7.2 (GCC) ) #1 SMP Mon Oct 21 20:10:34 IST 2013&lt;/P&gt;&lt;P&gt;Found initrd at 0xee5c0000:0xeffff701&lt;/P&gt;&lt;P&gt;No /soc@ffe000000/qman@318000 property 'fsl,qman-fqd', using&lt;/P&gt;&lt;P&gt;memblock_alloc(0000000000400000)&lt;/P&gt;&lt;P&gt;No /soc@ffe000000/qman@318000 property 'fsl,qman-pfdr', using&lt;/P&gt;&lt;P&gt;memblock_alloc(0000000002000000)&lt;/P&gt;&lt;P&gt;Qman ver:0a01,01,02&lt;/P&gt;&lt;P&gt;No /soc@ffe000000/bman@31a000 property 'fsl,bman-fbpr', using&lt;/P&gt;&lt;P&gt;memblock_alloc(0000000001000000)&lt;/P&gt;&lt;P&gt;Bman ver:0a02,01,00&lt;/P&gt;&lt;P&gt;pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-pdsr', using&lt;/P&gt;&lt;P&gt;memblock_alloc(0x0000000001000000)&lt;/P&gt;&lt;P&gt;pme: No /soc@ffe000000/pme@316000 property 'fsl,pme-sre', using&lt;/P&gt;&lt;P&gt;memblock_alloc(0x0000000000a00000)&lt;/P&gt;&lt;P&gt;USDPAA region at 10000000:10000000(10000:10000), 1 TLB1 entries)&lt;/P&gt;&lt;P&gt;CPU maps initialized for 1 thread per core&lt;/P&gt;&lt;P&gt;bootconsole  enabled&lt;/P&gt;&lt;P&gt;setup_arch: bootmem&lt;/P&gt;&lt;P&gt;P4080 DS board from Freescale Semiconductor&lt;/P&gt;&lt;P&gt;arch: exit&lt;/P&gt;&lt;P&gt;Zone ranges:&lt;/P&gt;&lt;P&gt;  DMA      &lt;/P&gt;&lt;P&gt;  Normal   empty&lt;/P&gt;&lt;P&gt;  HighMem  &lt;/P&gt;&lt;P&gt;Movable zone start for each node&lt;/P&gt;&lt;P&gt;Early memory node ranges&lt;/P&gt;&lt;P&gt;  node   0: &lt;/P&gt;&lt;P&gt;MMU: Allocated 1088 bytes of context maps for 255 contexts&lt;/P&gt;&lt;P&gt;PERCPU: Embedded 10 pages/cpu @c28d9000 s17216 r8192 d15552 u40960&lt;/P&gt;&lt;P&gt;Built 1 zonelists in Zone order, mobility grouping on.  Total pages: 1040384&lt;/P&gt;&lt;P&gt;Kernel command line: usdpaa_mem=256M usdpaa_mem=256M,1G&lt;/P&gt;&lt;P&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;/P&gt;&lt;P&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;/P&gt;&lt;P&gt;Memory: 3716020k/4194304k available (8116k kernel code, 478284k reserved,&lt;/P&gt;&lt;P&gt;304k data, 558k bss, 268k init)&lt;/P&gt;&lt;P&gt;Kernel virtual memory layout:&lt;/P&gt;&lt;P&gt;  &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;0xfff5f000..0xfffff000  : fixmap&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;  &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;0xffc00000..0xffe00000  : highmem PTEs&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;  &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;0xffbfa000..0xffc00000  : early ioremap&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;  &lt;/P&gt;&lt;UL&gt;&lt;LI level="1" type="ul"&gt;&lt;P&gt;0xf1000000..0xffbfa000  : vmalloc &amp;amp; ioremap&lt;/P&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;Hierarchical RCU implementation.&lt;/P&gt;&lt;P&gt;RCU debugfs-based tracing is enabled.&lt;/P&gt;&lt;P&gt;NR_IRQS:512 nr_irqs:512 16&lt;/P&gt;&lt;P&gt;mpic: Setting up MPIC " OpenPIC  " version 1.2 at ffe040000, max 8 CPUs&lt;/P&gt;&lt;P&gt;mpic: ISU size: 512, shift: 9, mask: 1ff&lt;/P&gt;&lt;P&gt;mpic: Initializing for 512 sources&lt;/P&gt;&lt;P&gt;clocksource: timebase mult[14000d1b] shift[24] registered&lt;/P&gt;&lt;P&gt;Console: colour dummy device 80x25&lt;/P&gt;&lt;P&gt;pid_max: default: 32768 minimum: 301&lt;/P&gt;&lt;P&gt;Mount-cache hash table entries: 512&lt;/P&gt;&lt;P&gt;mpic: requesting IPIs...&lt;/P&gt;&lt;P&gt;e500 family performance monitor hardware support registered&lt;/P&gt;&lt;P&gt;Brought up 8 CPUs&lt;/P&gt;&lt;P&gt;devtmpfs: initialized&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 16&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Found FSL PCI host bridge at 0x0000000ffe200000. Firmware bus number: 0-&amp;gt;0&lt;/P&gt;&lt;P&gt;PCI host bridge /pcie@ffe200000 (primary) ranges:&lt;/P&gt;&lt;P&gt; MEM 0x0000000c00000000..0x0000000c1fffffff -&amp;gt; 0x00000000e0000000&lt;/P&gt;&lt;P&gt;  IO 0x0000000ff8000000..0x0000000ff800ffff -&amp;gt; 0x0000000000000000&lt;/P&gt;&lt;P&gt;/pcie@ffe200000: PCICSRBAR @ 0xdf000000&lt;/P&gt;&lt;P&gt;/pcie@ffe200000: Setup 64-bit PCI DMA window&lt;/P&gt;&lt;P&gt;/pcie@ffe200000: DMA window size is 0xdf000000&lt;/P&gt;&lt;P&gt;EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller&lt;/P&gt;&lt;P&gt;'mpc85xx_pci_err': DEV 'ffe200000.pcie' (INTERRUPT)&lt;/P&gt;&lt;P&gt;MPC85xx_edac acquired irq 482 for PCI Err&lt;/P&gt;&lt;P&gt;MPC85xx_edac PCI err registered&lt;/P&gt;&lt;P&gt;Found FSL PCI host bridge at 0x0000000ffe202000. Firmware bus number: 0-&amp;gt;1&lt;/P&gt;&lt;P&gt;PCI host bridge /pcie@ffe202000  ranges:&lt;/P&gt;&lt;P&gt; MEM 0x0000000c40000000..0x0000000c5fffffff -&amp;gt; 0x00000000e0000000&lt;/P&gt;&lt;P&gt;  IO 0x0000000ff8020000..0x0000000ff802ffff -&amp;gt; 0x0000000000000000&lt;/P&gt;&lt;P&gt;/pcie@ffe202000: PCICSRBAR @ 0xdf000000&lt;/P&gt;&lt;P&gt;/pcie@ffe202000: Setup 64-bit PCI DMA window&lt;/P&gt;&lt;P&gt;/pcie@ffe202000: DMA window size is 0xdf000000&lt;/P&gt;&lt;P&gt;EDAC PCI1: Giving out device to module 'MPC85xx_edac' controller&lt;/P&gt;&lt;P&gt;'mpc85xx_pci_err': DEV 'ffe202000.pcie' (INTERRUPT)&lt;/P&gt;&lt;P&gt;MPC85xx_edac acquired irq 480 for PCI Err&lt;/P&gt;&lt;P&gt;MPC85xx_edac PCI err registered&lt;/P&gt;&lt;P&gt;software IO TLB  (64MB) mapped at&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;PCI: Probing PCI hardware&lt;/P&gt;&lt;P&gt;fsl-pci ffe200000.pcie: PCI host bridge to bus 0000:00&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource &lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource  (bus&lt;/P&gt;&lt;P&gt;address )&lt;/P&gt;&lt;P&gt;pci_bus 0000:00: root bus resource &lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: bridge configuration invalid (), reconfiguring&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to &lt;/P&gt;&lt;P&gt;fsl-pci ffe202000.pcie: PCI host bridge to bus 0001:02&lt;/P&gt;&lt;P&gt;pci_bus 0001:02: root bus resource  (bus address&lt;/P&gt;&lt;P&gt;)&lt;/P&gt;&lt;P&gt;pci_bus 0001:02: root bus resource  (bus&lt;/P&gt;&lt;P&gt;address )&lt;/P&gt;&lt;P&gt;pci_bus 0001:02: root bus resource &lt;/P&gt;&lt;P&gt;pci 0001:02:00.0: ignoring class 0x0b2000 (doesn't match header type 01)&lt;/P&gt;&lt;P&gt;PCIE error(s) detected&lt;/P&gt;&lt;P&gt;pci 0001:02:00.0: Primary bus is hard wired to 0&lt;/P&gt;&lt;P&gt;pci 0001:02:00.0: bridge configuration invalid (), reconfiguring&lt;/P&gt;&lt;P&gt;pci 0001:02:00.0: PCI bridge to &lt;/P&gt;&lt;P&gt;PCIE ERR_DR register: 0x80020000&lt;/P&gt;&lt;P&gt;PCIE ERR_CAP_STAT register: 0x80000001&lt;/P&gt;&lt;P&gt;PCIE ERR_CAP_R0 register: 0x00000800&lt;/P&gt;&lt;P&gt;PCIE ERR_CAP_R1 register: 0x00000000&lt;/P&gt;&lt;P&gt;PCIE ERR_CAP_R2 register: 0x00000000&lt;/P&gt;&lt;P&gt;PCIE ERR_CAP_R3 register: 0x00000000&lt;/P&gt;&lt;P&gt;pci 0000:00:00.0: PCI bridge to &lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:   bridge window &lt;/P&gt;&lt;P&gt;pci 0000:00:00.0:   bridge window &lt;/P&gt;&lt;P&gt;pci 0001:02:00.0: BAR 9: can't assign mem pref (size 0x100000)&lt;/P&gt;&lt;P&gt;pci 0001:03:00.0: BAR 6: assigned &lt;/P&gt;&lt;P&gt;pci 0001:02:00.0: PCI bridge to &lt;/P&gt;&lt;P&gt;pci 0001:02:00.0:   bridge window &lt;/P&gt;&lt;P&gt;pci 0001:02:00.0:   bridge window &lt;/P&gt;&lt;P&gt;bio: create slab &amp;lt;bio-0&amp;gt; at 0&lt;/P&gt;&lt;P&gt;vgaarb: loaded&lt;/P&gt;&lt;P&gt;SCSI subsystem initialized&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usbfs&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver hub&lt;/P&gt;&lt;P&gt;usbcore: registered new device driver usb&lt;/P&gt;&lt;P&gt;Bman err interrupt handler present&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 0&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 1&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 2&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 3&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 4&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 5&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 6&lt;/P&gt;&lt;P&gt;Bman portal initialised, cpu 7&lt;/P&gt;&lt;P&gt;Bman portals initialised&lt;/P&gt;&lt;P&gt;Bman: BPID allocator includes range 32:32&lt;/P&gt;&lt;P&gt;Qman err interrupt handler present&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 0&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 1&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 2&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 3&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 4&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 5&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 6&lt;/P&gt;&lt;P&gt;Qman portal initialised, cpu 7&lt;/P&gt;&lt;P&gt;Qman portals initialised&lt;/P&gt;&lt;P&gt;Qman: FQID allocator includes range 256:256&lt;/P&gt;&lt;P&gt;Qman: FQID allocator includes range 32768:32768&lt;/P&gt;&lt;P&gt;Qman: CGRID allocator includes range 0:256&lt;/P&gt;&lt;P&gt;Qman: pool channel allocator includes range 33:15&lt;/P&gt;&lt;P&gt;Switching to clocksource timebase&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 2&lt;/P&gt;&lt;P&gt;TCP established hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP bind hash table entries: 8192 (order: 4, 65536 bytes)&lt;/P&gt;&lt;P&gt;TCP: Hash tables configured (established 8192 bind 8192)&lt;/P&gt;&lt;P&gt;TCP: reno registered&lt;/P&gt;&lt;P&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 1&lt;/P&gt;&lt;P&gt;RPC: Registered named UNIX socket transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered udp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp transport module.&lt;/P&gt;&lt;P&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;/P&gt;&lt;P&gt;Trying to unpack rootfs image as initramfs...&lt;/P&gt;&lt;P&gt;rootfs image is not initramfs (no cpio magic); looks like an initrd&lt;/P&gt;&lt;P&gt;Freeing initrd memory: 26880k freed&lt;/P&gt;&lt;P&gt;fsl-rcpm ffe0e2000.global-utilities: Freescale RCPM driver&lt;/P&gt;&lt;P&gt;audit: initializing netlink socket (disabled)&lt;/P&gt;&lt;P&gt;type=2000 audit(0.492:1): initialized&lt;/P&gt;&lt;P&gt;bounce pool size: 64 pages&lt;/P&gt;&lt;P&gt;HugeTLB registered 1 MB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;HugeTLB registered 4 MB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;HugeTLB registered 16 MB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;HugeTLB registered 64 MB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;HugeTLB registered 256 MB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;HugeTLB registered 1 GB page size, pre-allocated 0 pages&lt;/P&gt;&lt;P&gt;NFS: Registering the id_resolver key type&lt;/P&gt;&lt;P&gt;Key type id_resolver registered&lt;/P&gt;&lt;P&gt;Key type id_legacy registered&lt;/P&gt;&lt;P&gt;NTFS driver 2.1.30 .&lt;/P&gt;&lt;P&gt;jffs2: version 2.2. (NAND) Â© 2001-2006 Red Hat, Inc.&lt;/P&gt;&lt;P&gt;msgmni has been set to 654&lt;/P&gt;&lt;P&gt;io scheduler noop registered&lt;/P&gt;&lt;P&gt;io scheduler deadline registered&lt;/P&gt;&lt;P&gt;io scheduler cfq registered (default)&lt;/P&gt;&lt;P&gt;Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;/P&gt;&lt;P&gt;serial8250.0: ttyS0 at MMIO 0xffe11c500 (irq = 36) is a 16550A&lt;/P&gt;&lt;P&gt;console  enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;console  enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;serial8250.0: ttyS1 at MMIO 0xffe11c600 (irq = 36) is a 16550A&lt;/P&gt;&lt;P&gt;serial8250.0: ttyS2 at MMIO 0xffe11d500 (irq = 37) is a 16550A&lt;/P&gt;&lt;P&gt;serial8250.0: ttyS3 at MMIO 0xffe11d600 (irq = 37) is a 16550A&lt;/P&gt;&lt;P&gt;ePAPR hypervisor byte channel driver&lt;/P&gt;&lt;P&gt;Generic non-volatile memory driver v1.1&lt;/P&gt;&lt;P&gt;brd: module loaded&lt;/P&gt;&lt;P&gt;loop: module loaded&lt;/P&gt;&lt;P&gt;st: Version 20101219, fixed bufsize 32768, s/g segs 256&lt;/P&gt;&lt;P&gt;scsi0 : sata_sil24&lt;/P&gt;&lt;P&gt;scsi1 : sata_sil24&lt;/P&gt;&lt;P&gt;ata1: SATA max UDMA/100 host m128@0xc40000000 port 0xc40004000 irq 42&lt;/P&gt;&lt;P&gt;ata2: SATA max UDMA/100 host m128@0xc40000000 port 0xc40006000 irq 42&lt;/P&gt;&lt;P&gt;fe8000000.flash: Found 1 x16 devices at 0x0 in 16-bit bank. Manufacturer ID&lt;/P&gt;&lt;P&gt;0x000001 Chip ID 0x002801&lt;/P&gt;&lt;P&gt;Amd/Fujitsu Extended Query Table at 0x0040&lt;/P&gt;&lt;P&gt;  Amd/Fujitsu Extended Query version 1.3.&lt;/P&gt;&lt;P&gt;number of CFI chips: 1&lt;/P&gt;&lt;P&gt;fsl_espi ffe110000.spi: master is unqueued, this is deprecated&lt;/P&gt;&lt;P&gt;m25p80 spi32766.0: s25sl12801 (16384 Kbytes)&lt;/P&gt;&lt;P&gt;4 ofpart partitions found on MTD device spi32766.0&lt;/P&gt;&lt;P&gt;Creating 4 MTD partitions on "spi32766.0":&lt;/P&gt;&lt;P&gt;0x000000000000-0x000000100000 : "u-boot"&lt;/P&gt;&lt;P&gt;0x000000100000-0x000000600000 : "kernel"&lt;/P&gt;&lt;P&gt;0x000000600000-0x000000700000 : "dtb"&lt;/P&gt;&lt;P&gt;0x000000700000-0x000001000000 : "file system"&lt;/P&gt;&lt;P&gt;fsl_espi ffe110000.spi: at 0xf117c000 (irq = 53)&lt;/P&gt;&lt;P&gt;libphy: Fixed MDIO Bus: probed&lt;/P&gt;&lt;P&gt;platform mdio-mux-emi1.14: Driver mdio-mux-gpio requests probe deferral&lt;/P&gt;&lt;P&gt;platform mdio-mux-emi2.15: Driver mdio-mux-gpio requests probe deferral&lt;/P&gt;&lt;P&gt;libphy: Freescale PowerQUICC MII Bus: probed&lt;/P&gt;&lt;P&gt;libphy: Freescale XGMAC MDIO Bus: probed&lt;/P&gt;&lt;P&gt; FMAN(0) Fifo size settings:&lt;/P&gt;&lt;P&gt;  - Total buffers available(512 - 256B/buffer)&lt;/P&gt;&lt;P&gt;  - Total throughput(1Gbps)&lt;/P&gt;&lt;P&gt;  - Max frame size(1522B)&lt;/P&gt;&lt;P&gt;  - 1G ports TX 1(12 bufs set (min: 12))&lt;/P&gt;&lt;P&gt;  - 1G ports RX 1(452 bufs set (min: 14))&lt;/P&gt;&lt;P&gt;  - OH-HC ports 4(8)&lt;/P&gt;&lt;P&gt;  - Shared extra buffers(16)&lt;/P&gt;&lt;P&gt; FMAN(0) open dma settings:&lt;/P&gt;&lt;P&gt;  - Total open dma available(32)&lt;/P&gt;&lt;P&gt;  - 1G ports TX 1(14)&lt;/P&gt;&lt;P&gt;  - 1G ports RX 1(14)&lt;/P&gt;&lt;P&gt;  - OH-HC ports 4(1)&lt;/P&gt;&lt;P&gt;  - Shared extra open dma(0)&lt;/P&gt;&lt;P&gt; FMAN(0) Tnums settings:&lt;/P&gt;&lt;P&gt;  - Total Tnums available(128)&lt;/P&gt;&lt;P&gt;  - 1G ports TX 1(59)&lt;/P&gt;&lt;P&gt;  - 1G ports RX 1(59)&lt;/P&gt;&lt;P&gt;  - OH-HC ports 4(2)&lt;/P&gt;&lt;P&gt;  - Shared extra tnums(2)&lt;/P&gt;&lt;P&gt; FMAN(1) Fifo size settings:&lt;/P&gt;&lt;P&gt;  - Total buffers available(512 - 256B/buffer)&lt;/P&gt;&lt;P&gt;  - Total throughput(4Gbps)&lt;/P&gt;&lt;P&gt;  - Max frame size(1522B)&lt;/P&gt;&lt;P&gt;  - 1G ports TX 4(12 bufs set (min: 12))&lt;/P&gt;&lt;P&gt;  - 1G ports RX 4(104 bufs set (min: 14))&lt;/P&gt;&lt;P&gt;  - OH-HC ports 4(8)&lt;/P&gt;&lt;P&gt;  - Shared extra buffers(16)&lt;/P&gt;&lt;P&gt; FMAN(1) open dma settings:&lt;/P&gt;&lt;P&gt;  - Total open dma available(32)&lt;/P&gt;&lt;P&gt;  - 1G ports TX 4(4)&lt;/P&gt;&lt;P&gt;  - 1G ports RX 4(3)&lt;/P&gt;&lt;P&gt;  - OH-HC ports 4(1)&lt;/P&gt;&lt;P&gt;  - Shared extra open dma(0)&lt;/P&gt;&lt;P&gt; FMAN(1) Tnums settings:&lt;/P&gt;&lt;P&gt;  - Total Tnums available(128)&lt;/P&gt;&lt;P&gt;  - 1G ports TX 4(14)&lt;/P&gt;&lt;P&gt;  - 1G ports RX 4(15)&lt;/P&gt;&lt;P&gt;  - OH-HC ports 4(2)&lt;/P&gt;&lt;P&gt;  - Shared extra tnums(4)&lt;/P&gt;&lt;P&gt;Freescale FM module (Oct 21 2013:20:09:58), FMD API version 21.1.0&lt;/P&gt;&lt;P&gt;Freescale FM Ports module (Oct 21 2013:20:09:57)&lt;/P&gt;&lt;P&gt;dpaa_debugfs: FSL DPAA Ethernet debugfs entries ()&lt;/P&gt;&lt;P&gt;fsl_mac: mac.c:417:mac_load() fsl_mac: FSL FMan MAC API based driver ()&lt;/P&gt;&lt;P&gt;fsl_mac ffe4e0000.ethernet: FMan dTSEC version: 0x08240101&lt;/P&gt;&lt;P&gt;fsl_mac ffe4e0000.ethernet: FMan MAC address: 00:04:9f:02:85:90&lt;/P&gt;&lt;P&gt;fsl_mac ffe4e2000.ethernet: FMan dTSEC version: 0x08240101&lt;/P&gt;&lt;P&gt;fsl_mac ffe4e2000.ethernet: FMan MAC address: 00:04:9f:02:85:91&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e0000.ethernet: FMan dTSEC version: 0x08240101&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e0000.ethernet: FMan MAC address: 00:04:9f:02:85:95&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e2000.ethernet: FMan dTSEC version: 0x08240101&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e2000.ethernet: FMan MAC address: 00:04:9f:02:85:96&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e4000.ethernet: FMan dTSEC version: 0x08240101&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e4000.ethernet: FMan MAC address: 00:04:9f:02:85:97&lt;/P&gt;&lt;P&gt;fsl_mac ffe5e6000.ethernet: of_get_mac_address(/soc@ffe000000/fman@500000&lt;/P&gt;&lt;P&gt;/ethernet@e6000) failed&lt;/P&gt;&lt;P&gt;fsl_mac: probe of ffe5e6000.ethernet failed with error -22&lt;/P&gt;&lt;P&gt;fsl_dpa: dpaa_eth.c:4320:dpa_load() fsl_dpa: FSL DPAA Ethernet driver ()&lt;/P&gt;&lt;P&gt;fsl_dpa ethernet.17: Using private BM buffer pools&lt;/P&gt;&lt;P&gt;fsl_dpa: dpaa_eth.c:3715:dpa_rx_fq_init() Using dynamic RX QM frame queues&lt;/P&gt;&lt;P&gt;fsl_dpa: dpaa_eth.c:3739:dpa_tx_fq_init() Using dynamic TX QM frame queues&lt;/P&gt;&lt;P&gt;fsl_dpa ethernet.21: dev_get_drvdata(ffe5e6000.ethernet) failed&lt;/P&gt;&lt;P&gt;fsl_dpa: probe of ethernet.21 failed with error -22&lt;/P&gt;&lt;P&gt;fsl_oh: offline_port.c:439:oh_port_load() fsl_oh: FSL FMan Offline Parsing&lt;/P&gt;&lt;P&gt;port driver ()&lt;/P&gt;&lt;P&gt;fsl_oh dpa-fman0-oh.22: Found OH node handle compatible with fsl,dpa-oh.&lt;/P&gt;&lt;P&gt;fsl_oh dpa-fman0-oh.22: OH port /soc@ffe000000/fman@400000/port@82000 has&lt;/P&gt;&lt;P&gt;no buffer pool. Fragmentation will not be enabled&lt;/P&gt;&lt;P&gt;fsl_oh dpa-fman0-oh.22: OH port /soc@ffe000000/fman@400000/port@82000enabled.&lt;/P&gt;&lt;P&gt;e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI&lt;/P&gt;&lt;P&gt;e1000: Copyright (c) 1999-2006 Intel Corporation.&lt;/P&gt;&lt;P&gt;e1000e: Intel(R) PRO/1000 Network Driver - 2.1.4-k&lt;/P&gt;&lt;P&gt;e1000e: Copyright(c) 1999 - 2012 Intel Corporation.&lt;/P&gt;&lt;P&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;/P&gt;&lt;P&gt;ehci-pci: EHCI PCI platform driver&lt;/P&gt;&lt;P&gt;ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver&lt;/P&gt;&lt;P&gt;/soc@ffe000000/usb@210000: Invalid 'dr_mode' property, fallback to host mode&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: Freescale On-Chip EHCI Host Controller&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: new USB bus registered, assigned bus number 1&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: irq 44, io mem 0xffe210000&lt;/P&gt;&lt;P&gt;fsl-ehci fsl-ehci.0: USB 2.0 started, EHCI 1.00&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: USB hub found&lt;/P&gt;&lt;P&gt;hub 1-0:1.0: 1 port detected&lt;/P&gt;&lt;P&gt;Initializing USB Mass Storage driver...&lt;/P&gt;&lt;P&gt;usbcore: registered new interface driver usb-storage&lt;/P&gt;&lt;P&gt;USB Mass Storage support registered.&lt;/P&gt;&lt;P&gt;i2c /dev entries driver&lt;/P&gt;&lt;P&gt;mpc-i2c ffe118100.i2c: timeout 1000000 us&lt;/P&gt;&lt;P&gt;rtc-ds3232 0-0068: rtc core: registered ds3232 as rtc0&lt;/P&gt;&lt;P&gt;mpc-i2c ffe118000.i2c: timeout 1000000 us&lt;/P&gt;&lt;P&gt;mpc-i2c ffe119000.i2c: timeout 1000000 us&lt;/P&gt;&lt;P&gt;mpc-i2c ffe119100.i2c: timeout 1000000 us&lt;/P&gt;&lt;P&gt;EDAC MC: Ver: 3.0.0&lt;/P&gt;&lt;P&gt;Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software&lt;/P&gt;&lt;P&gt;mpc85xx_mc_err_probe: No ECC DIMMs discovered&lt;/P&gt;&lt;P&gt;mpc85xx_mc_err_probe: No ECC DIMMs discovered&lt;/P&gt;&lt;P&gt;sdhci: Secure Digital Host Controller Interface driver&lt;/P&gt;&lt;P&gt;sdhci: Copyright(c) Pierre Ossman&lt;/P&gt;&lt;P&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;/P&gt;&lt;P&gt;mmc0: SDHCI controller on ffe114000.sdhc  using DMA&lt;/P&gt;&lt;P&gt;platform caam_qi.0: Linux CAAM Queue I/F driver initialised&lt;/P&gt;&lt;P&gt;caam ffe300000.crypto: device ID = 0x0a10030000000000 (Era -524)&lt;/P&gt;&lt;P&gt;caam ffe300000.crypto: job rings = 4, qi = 1&lt;/P&gt;&lt;P&gt;caam ffe300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto&lt;/P&gt;&lt;P&gt;platform ffe301000.jr: registering rng-caam&lt;/P&gt;&lt;P&gt;platform caam_qi.0: fsl,sec-v4.0 algorithms registered in /proc/crypto&lt;/P&gt;&lt;P&gt;Freescale USDPAA process driver&lt;/P&gt;&lt;P&gt;Freescale USDPAA process IRQ driver&lt;/P&gt;&lt;P&gt;fsl-pme ffe316000.pme: ver: 0x00100201&lt;/P&gt;&lt;P&gt;Freescale pme2 db driver&lt;/P&gt;&lt;P&gt;Freescale pme2 scan driver&lt;/P&gt;&lt;P&gt;fsl-pme2-scan: device pme_scan registered&lt;/P&gt;&lt;P&gt;Freescale hypervisor management driver&lt;/P&gt;&lt;P&gt;fsl-hv: no hypervisor found&lt;/P&gt;&lt;P&gt;IPv4 over IPv4 tunneling driver&lt;/P&gt;&lt;P&gt;TCP: cubic registered&lt;/P&gt;&lt;P&gt;Initializing XFRM netlink socket&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 10&lt;/P&gt;&lt;P&gt;sit: IPv6 over IPv4 tunneling driver&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 17&lt;/P&gt;&lt;P&gt;NET: Registered protocol family 15&lt;/P&gt;&lt;P&gt;Key type dns_resolver registered&lt;/P&gt;&lt;P&gt;libphy: mdio_mux: probed&lt;/P&gt;&lt;P&gt;libphy: mdio_mux: probed&lt;/P&gt;&lt;P&gt;mdio-mux-gpio mdio-mux-emi1.14: Version 1.0&lt;/P&gt;&lt;P&gt;rtc-ds3232 0-0068: setting system clock to 2013-10-28 03:50:22 UTC&lt;/P&gt;&lt;P&gt;(1382932222)&lt;/P&gt;&lt;P&gt;ata1: SATA link up 3.0 Gbps (SStatus 123 SControl 0)&lt;/P&gt;&lt;P&gt;ata1.00: ATA-8: Hitachi HDS721050CLA360, JP2OA50E, max UDMA/133&lt;/P&gt;&lt;P&gt;ata1.00: 976773168 sectors, multi 0: LBA48 NCQ (depth 31/32)&lt;/P&gt;&lt;P&gt;ata1.00: configured for UDMA/100&lt;/P&gt;&lt;P&gt;scsi 0:0:0:0: Direct-Access     ATA      Hitachi HDS72105 JP2O PQ: 0 ANSI: 5&lt;/P&gt;&lt;P&gt;sd 0:0:0:0:  976773168 512-byte logical blocks: (500 GB/465 GiB)&lt;/P&gt;&lt;P&gt;sd 0:0:0:0: Attached scsi generic sg0 type 0&lt;/P&gt;&lt;P&gt;sd 0:0:0:0:  Write Protect is off&lt;/P&gt;&lt;P&gt;sd 0:0:0:0:  Write cache: enabled, read cache: enabled, doesn't&lt;/P&gt;&lt;P&gt;support DPO or FUA&lt;/P&gt;&lt;P&gt; sda: unknown partition table&lt;/P&gt;&lt;P&gt;sd 0:0:0:0:  Attached SCSI disk&lt;/P&gt;&lt;P&gt;ata2: SATA link down (SStatus 0 SControl 0)&lt;/P&gt;&lt;P&gt;RAMDISK: gzip image found at block 0&lt;/P&gt;&lt;P&gt;VFS: Mounted root (ext2 filesystem) readonly on device 1:0.&lt;/P&gt;&lt;P&gt;devtmpfs: mounted&lt;/P&gt;&lt;P&gt;Freeing unused kernel memory: 268k freed&lt;/P&gt;&lt;P&gt;INIT: version 2.88 booting&lt;/P&gt;&lt;P&gt;/etc/init.d/rcS: line 27: /etc/hostname: Read-only file system&lt;/P&gt;&lt;P&gt;Starting udev&lt;/P&gt;&lt;P&gt;udevd[966]: starting version 182&lt;/P&gt;&lt;P&gt;Starting Bootlog daemon: bootlogd: cannot allocate pseudo tty: No such file&lt;/P&gt;&lt;P&gt;or directory&lt;/P&gt;&lt;P&gt;bootlogd.&lt;/P&gt;&lt;P&gt;Configuring network interfaces... done.&lt;/P&gt;&lt;P&gt;net.ipv4.conf.default.rp_filter = 0&lt;/P&gt;&lt;P&gt;net.ipv4.conf.all.rp_filter = 0&lt;/P&gt;&lt;P&gt;Running postinst /etc/rpm-postinsts/debianutils...&lt;/P&gt;&lt;P&gt;Running postinst /etc/rpm-postinsts/sysvinit-inittab...&lt;/P&gt;&lt;P&gt;INIT: Entering runlevel: 5&lt;/P&gt;&lt;P&gt;Starting Dropbear SSH server: Will output 1024 bit rsa secret key to&lt;/P&gt;&lt;P&gt;'/etc/dropbear/dropbear_rsa_host_key'&lt;/P&gt;&lt;P&gt;Generating key, this may take a while...&lt;/P&gt;&lt;P&gt;Public key portion is:&lt;/P&gt;&lt;P&gt;ssh-rsa&lt;/P&gt;&lt;P&gt;AAAAB3NzaC1yc2EAAAADAQABAAAAgwCi7BQQH2u2JvfBYUA10hWa&lt;EM&gt;N8A9b4NCIr/gkRNQewAGInOQGjgoGR96psWLrsXsOVcwFxfeDvBStM8IcevAi3lbE8v&lt;/EM&gt;9raDfa/8ZCTWUiEmvL5ny5KU0kglqxW4lMe13k+uvjXR7cTiMfLvg7GpfA429miaByjAyDdhGZod2/jIGRp&lt;/P&gt;&lt;P&gt;root@p4080ds&lt;/P&gt;&lt;P&gt;Fingerprint: md5 dc:f5:02:08:8d:35:5e:24:2e:b3:ab:de:6a:c4:bb:b6&lt;/P&gt;&lt;P&gt;dropbear.&lt;/P&gt;&lt;P&gt;Starting network benchmark server: netserver.&lt;/P&gt;&lt;P&gt;Starting system log daemon...0&lt;/P&gt;&lt;P&gt;Starting kernel log daemon...0&lt;/P&gt;&lt;P&gt;Stopping Bootlog daemon: bootlogd.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Poky 9.0 (Yocto Project 1.4 Reference Distro) 1.4 p4080ds ttyS0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;p4080ds login: 0xebf40000                              root&lt;/P&gt;&lt;P&gt;root@p4080ds:~#&lt;/P&gt;&lt;P&gt;root@p4080ds:~#&lt;/P&gt;&lt;P&gt;root@p4080ds:~# cat /root/          ifcon fig&lt;/P&gt;&lt;P&gt;lo        Link encap:Local Loopback&lt;/P&gt;&lt;P&gt;          inet addr:127.0.0.1  Mask:255.0.0.0&lt;/P&gt;&lt;P&gt;          inet6 addr: ::1/128 Scope:Host&lt;/P&gt;&lt;P&gt;          UP LOOPBACK RUNNING  MTU:65536  Metric:1&lt;/P&gt;&lt;P&gt;          RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;/P&gt;&lt;P&gt;          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;/P&gt;&lt;P&gt;          collisions:0 txqueuelen:0&lt;/P&gt;&lt;P&gt;          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@p4080ds:~# ifconfig -a&lt;/P&gt;&lt;P&gt;fm1-gb1   Link encap:Ethernet  HWaddr 00:04:9f:02:85:91&lt;/P&gt;&lt;P&gt;          BROADCAST MULTICAST  MTU:1500  Metric:1&lt;/P&gt;&lt;P&gt;          RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;/P&gt;&lt;P&gt;          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;/P&gt;&lt;P&gt;          collisions:0 txqueuelen:1000&lt;/P&gt;&lt;P&gt;          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;          Memory:fe4e2000-fe4e2fff&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;lo        Link encap:Local Loopback&lt;/P&gt;&lt;P&gt;          inet addr:127.0.0.1  Mask:255.0.0.0&lt;/P&gt;&lt;P&gt;          inet6 addr: ::1/128 Scope:Host&lt;/P&gt;&lt;P&gt;          UP LOOPBACK RUNNING  MTU:65536  Metric:1&lt;/P&gt;&lt;P&gt;          RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;/P&gt;&lt;P&gt;          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;/P&gt;&lt;P&gt;          collisions:0 txqueuelen:0&lt;/P&gt;&lt;P&gt;          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;sit0      Link encap:UNSPEC  HWaddr&lt;/P&gt;&lt;P&gt;00-00-00-00-00-00-10-0D-00-00-00-00-00-00-00-00&lt;/P&gt;&lt;P&gt;          NOARP  MTU:1480  Metric:1&lt;/P&gt;&lt;P&gt;          RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;/P&gt;&lt;P&gt;          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;/P&gt;&lt;P&gt;          collisions:0 txqueuelen:0&lt;/P&gt;&lt;P&gt;          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;tunl0     Link encap:IPIP Tunnel  HWaddr&lt;/P&gt;&lt;P&gt;          NOARP  MTU:1480  Metric:1&lt;/P&gt;&lt;P&gt;          RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;/P&gt;&lt;P&gt;          TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;/P&gt;&lt;P&gt;          collisions:0 txqueuelen:0&lt;/P&gt;&lt;P&gt;          RX bytes:0 (0.0 B)  TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;######################################################&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Mon, Nov 4, 2013 at 2:07 PM, Yiping Wang&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 09:07:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249751#M478</guid>
      <dc:creator>ankur</dc:creator>
      <dc:date>2013-11-04T09:07:19Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249752#M479</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have attached logs to the thread.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Ankur.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Nov 2013 09:11:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249752#M479</guid>
      <dc:creator>ankur</dc:creator>
      <dc:date>2013-11-04T09:11:31Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS reflector is not working</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249753#M480</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have verified your u-boot environment on my target without any problem, please check whether there is physical connection problem on your target.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Nov 2013 08:58:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-reflector-is-not-working/m-p/249753#M480</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2013-11-05T08:58:45Z</dc:date>
    </item>
  </channel>
</rss>