<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Rapidio Demo for P2020 which run Linux OS?</title>
    <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984416#M4732</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks all the same&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 27 Feb 2020 14:44:55 GMT</pubDate>
    <dc:creator>liguofa</dc:creator>
    <dc:date>2020-02-27T14:44:55Z</dc:date>
    <item>
      <title>Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984406#M4722</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now ,We use yocto sdk 1.8,and we use fsl-image-full to get a full filesystem .but I can not find a rmu demo programe in it.Can anyone help .Where I can get a demo program for Rapidio demo ,which run in P2020 with Linux OS.&lt;/P&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/khumphri"&gt;khumphri&lt;/A&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/Mandar"&gt;Mandar&lt;/A&gt;‌&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/dhaval"&gt;dhaval&lt;/A&gt;‌&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2020 05:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984406#M4722</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-19T05:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984407#M4723</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/yipingwang"&gt;yipingwang&lt;/A&gt;‌ Can help me about this？Thanks very much！&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Feb 2020 13:19:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984407#M4723</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-19T13:19:24Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984408#M4724</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background-color: #ffffff; color: #646464; font-size: 18.004px; "&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;Hello guofa,&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to section "7.23 Serial Rapid I/O Interface" in QorIQ SDK 1.8 user manual.&lt;/P&gt;&lt;P&gt;Please refer to RIONET Ethernet over RapidIO use case.&amp;nbsp;RIONET ethernet over RapidIO driver&lt;BR /&gt;"rionet.ko" can be loaded as a module. To run the rionet.ko module, the Serial RapidIO controller must include RMU hardware module.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could get QorIQ SDK 1.8 user manual from&amp;nbsp;&lt;A class="link-titled" href="https://drive.google.com/open?id=1xBBSBnDkHgyBVRjf83-h2Ps001y-quwR" title="https://drive.google.com/open?id=1xBBSBnDkHgyBVRjf83-h2Ps001y-quwR"&gt;https://drive.google.com/open?id=1xBBSBnDkHgyBVRjf83-h2Ps001y-quwR&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 21 Feb 2020 09:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984408#M4724</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-02-21T09:31:25Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984409#M4725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/yipingwang"&gt;yipingwang&lt;/A&gt;‌;&lt;/P&gt;&lt;P&gt;But when I make if enable rionet in "make menuconfig";I can not find the rionet active in dmesg!&lt;/P&gt;&lt;P&gt;I found the mport_cdev of rapidio char device drive is patched after Kernel verision 4.6.7,but&lt;/P&gt;&lt;P&gt;The lastest version of fsl/git is 4.1.x。&lt;/P&gt;&lt;P&gt;If I just want to test a msg or doorbell send and recieve to other devices ，not use rionet module。So I should use&amp;nbsp;&lt;/P&gt;&lt;P&gt;a char device driver to active it。Did it is the only way that to test rapidio send and recieve not use rionet？&lt;BR /&gt;And by the way ！ Now the website of&amp;nbsp;&lt;A class="link-titled" href="http://git.freescale.com/" title="http://git.freescale.com/"&gt;http://git.freescale.com/&lt;/A&gt;&amp;nbsp; is down！ Can give a new web to git the last version of them。&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 22 Feb 2020 05:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984409#M4725</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-22T05:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984410#M4726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello guofa,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;RIONET should exist in SDK 1.8 Linux Kernel, however it have been removed from Linux Kernel 4.x.&lt;/P&gt;&lt;P&gt;Please check and rebuild Linux Kernel with the following Kernel option enabled.&lt;/P&gt;&lt;P&gt;CONFIG_RAPIDIO&lt;BR /&gt;CONFIG_RIONET&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/102598iCE86A0720D4F03E6/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Yiping&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Feb 2020 08:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984410#M4726</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-02-24T08:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984411#M4727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I try this options in SDK1.8, my chip is P2020 ，but failed,I can not find rionet.ko work well after insmod rionet.ko.or compiled in kernel.both failed,&lt;/P&gt;&lt;P&gt;The failed message is "There no ethX find in dmesg log"&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 02:49:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984411#M4727</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-27T02:49:18Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984412#M4728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check u-boot log, whether "SRIO1" is enabled.&lt;/P&gt;&lt;P&gt;Under u-boot, please add "riohdid=0" in bootargs.&lt;/P&gt;&lt;P&gt;Please check whether the following is included in dts file&lt;/P&gt;&lt;P&gt;rmu: rmu@d3000 {&lt;BR /&gt;#address-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt;#size-cells = &amp;lt;1&amp;gt;;&lt;BR /&gt;compatible = "fsl,srio-rmu";&lt;BR /&gt;reg = &amp;lt;0xd3000 0x500&amp;gt;;&lt;BR /&gt;ranges = &amp;lt;0x0 0xd3000 0x500&amp;gt;;&lt;BR /&gt;message-unit@0 {&lt;BR /&gt;compatible = "fsl,srio-msg-unit";&lt;BR /&gt;reg = &amp;lt;0x0 0x100&amp;gt;;&lt;BR /&gt;interrupts = &amp;lt;&lt;BR /&gt;60 2 0 0 /* msg1_tx_irq */&lt;BR /&gt;61 2 0 0&amp;gt;;/* msg1_rx_irq */&lt;BR /&gt;};&lt;BR /&gt;message-unit@100 {&lt;BR /&gt;compatible = "fsl,srio-msg-unit";&lt;BR /&gt;reg = &amp;lt;0x100 0x100&amp;gt;;&lt;BR /&gt;interrupts = &amp;lt;&lt;BR /&gt;62 2 0 0 /* msg2_tx_irq */&lt;BR /&gt;63 2 0 0&amp;gt;;/* msg2_rx_irq */&lt;/P&gt;&lt;P&gt;};&lt;BR /&gt;doorbell-unit@400 {&lt;BR /&gt;compatible = "fsl,srio-dbell-unit";&lt;BR /&gt;reg = &amp;lt;0x400 0x80&amp;gt;;&lt;BR /&gt;interrupts = &amp;lt;&lt;BR /&gt;56 2 0 0 /* bell_outb_irq */&lt;BR /&gt;57 2 0 0&amp;gt;;/* bell_inb_irq */&lt;BR /&gt;};&lt;BR /&gt;port-write-unit@4e0 {&lt;BR /&gt;compatible = "fsl,srio-port-write-unit";&lt;BR /&gt;reg = &amp;lt;0x4e0 0x20&amp;gt;;&lt;BR /&gt;interrupts = &amp;lt;16 2 1 11&amp;gt;;&lt;BR /&gt;};&lt;BR /&gt;};&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 08:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984412#M4728</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2020-02-27T08:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984413#M4729</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes,I check all about them,and they are right log as you discribed~,no I used linux kernel 4.19.x,which I get from linux website，Now，I used the code ，I can used the driver rio_mport_cdev.ko to test doorbell now,but when I use rio_cm.ko driver to test mbox(message) ,it comes a error which code -16,meaning BUSBUSY!.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question is can tell me where I can get the userspace test demo discribed in&amp;nbsp;&lt;A class="link-titled" href="https://github.com/torvalds/linux/blob/master/Documentation/driver-api/rapidio/rio_cm.rst#5-user-space-applications-and-api-library" title="https://github.com/torvalds/linux/blob/master/Documentation/driver-api/rapidio/rio_cm.rst#5-user-space-applications-and-api-library"&gt;linux/rio_cm.rst at master · torvalds/linux · GitHub&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;Messaging API library and applications that use this device driver are available from RapidIO.org.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;it means i can get applications demo in rapidio.org ? I try but failed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;Thanks very much ~.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #24292e; background-color: #ffffff;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;Best wishes.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 14:00:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984413#M4729</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-27T14:00:50Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984414#M4730</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Now the doorbell support well,and I test it with kernel driver in driver/rapidio/devices/rio_mport_cdev.c;&lt;/P&gt;&lt;P&gt;I read the code ,and From my side, the rapidio mode code in driver/rapidio/&lt;BR /&gt;and the driver for special control such as 721 and so on ,in driver/rapdio/devices;&lt;/P&gt;&lt;P&gt;but the fsl (nxp) rmu driver in arch/powerpc/sysdev/ ,is it right?&lt;/P&gt;&lt;P&gt;Tks again !&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 14:07:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984414#M4730</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-27T14:07:16Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984415#M4731</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have found it in github rapidio.org .thanks any more!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 14:44:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984415#M4731</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-27T14:44:39Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984416#M4732</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thanks all the same&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 27 Feb 2020 14:44:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984416#M4732</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-02-27T14:44:55Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984417#M4733</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;interrupts = &amp;lt;&lt;/SPAN&gt;&lt;BR style="color: #51626f; background-color: #ffffff;" /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;56 2 0 0 /* bell_outb_irq */&lt;/SPAN&gt;&lt;BR style="color: #51626f; background-color: #ffffff;" /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;57 2 0 0&amp;gt;;/* bell_inb_irq */&lt;/SPAN&gt;&lt;BR style="color: #51626f; background-color: #ffffff;" /&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;};&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; background-color: #ffffff;"&gt;can anyone tell me what is the mean of the irq of no. 56,57 ，it is interrupt no. of&amp;nbsp; hw interrupt in p2020rm? or something else？&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Mar 2020 02:33:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984417#M4733</guid>
      <dc:creator>liguofa</dc:creator>
      <dc:date>2020-03-27T02:33:55Z</dc:date>
    </item>
    <item>
      <title>Re: Rapidio Demo for P2020 which run Linux OS?</title>
      <link>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984418#M4734</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using Linux kernel 3.0.6 with a P5020 board.&amp;nbsp; If I include the 'Freescale Embedded SRIO Controller support' option I get a compile time error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can enable other SRIO options such as 'Enable RapidIO Input/Output Ports', 'IDT CPS Gen.2 SRIO switch support' and the RIONET support without an error.&amp;nbsp; Only with the&amp;nbsp;&lt;SPAN&gt;'Freescale Embedded SRIO Controller support' option do I get a compile time error.&amp;nbsp; Is this option applicable to the P5020 processor or only 8548, etc...?&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 May 2020 17:31:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Rapidio-Demo-for-P2020-which-run-Linux-OS/m-p/984418#M4734</guid>
      <dc:creator>alorusso</dc:creator>
      <dc:date>2020-05-12T17:31:03Z</dc:date>
    </item>
  </channel>
</rss>