<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: eLBC memory map</title>
    <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249060#M454</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure what you're referring to by "256KB as specified in the datasheet", but the eLBC NAND buffer is only an 8KiB window.&amp;nbsp; You can configure the chipselect for the minimum size of 32KiB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 May 2013 23:58:48 GMT</pubDate>
    <dc:creator>scottwood</dc:creator>
    <dc:date>2013-05-29T23:58:48Z</dc:date>
    <item>
      <title>eLBC memory map</title>
      <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249055#M449</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can I configure eLBC memory map of P1020 as below in a same LAW:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Start address: 0x0_F0000000&amp;nbsp; ----NOR Flash start address (256MB size)&lt;/P&gt;&lt;P&gt;End address: 0x0_FFFFFFFF ----NOR Flash end address&lt;/P&gt;&lt;P&gt;Start address: 0x1_00000000&amp;nbsp; ----NAND Flash start address (2GB size)&lt;/P&gt;&lt;P&gt;End address: 0x1_7FFFFFFF ----NAND Flash end address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do i need to maintain 4GB LAW size for eLBC?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have 2GB of DDR3, 512MB PCIe, 2GB NAND, 256MB NOR and 64KB of FPGA. what could be the LAW settings for this configuration?.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 12:09:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249055#M449</guid>
      <dc:creator>FreeScaleLogin</dc:creator>
      <dc:date>2013-05-21T12:09:16Z</dc:date>
    </item>
    <item>
      <title>Re: eLBC memory map</title>
      <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249056#M450</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NOR flash is a memory mapped flash, so for example if it has x GB, you must set up in the TLB, LAW and CS x GB (is not a problem if you set up more than x GB).&lt;/P&gt;&lt;P&gt;On the other hand, the NAND flash is not a memory mapped flash. For a 2GB flash (your example) is enough to set up in the TLB, LAW and eLBC CS only 64KB for controller size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The FPGA case must be regarded from point of allocation as the NOR flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Coming back to your example is enough to set up 512MB in TLB and LAW for eLBC space.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 12:19:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249056#M450</guid>
      <dc:creator>marius_grigoras</dc:creator>
      <dc:date>2013-05-21T12:19:26Z</dc:date>
    </item>
    <item>
      <title>Re: eLBC memory map</title>
      <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249057#M451</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marius,&lt;/P&gt;&lt;P&gt;Thanks for the Quick reply,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NAND flash chip select is assigned to CS3 of eLBC, that means it is memory mapped to eLBC, right?&amp;nbsp; &lt;/P&gt;&lt;P&gt;And I am not getting the point in your context "eLBC CS only 64KB for controller size"? could you please elaborate?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kumar&lt;/P&gt;&lt;P&gt;&lt;BR /&gt; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 13:57:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249057#M451</guid>
      <dc:creator>FreeScaleLogin</dc:creator>
      <dc:date>2013-05-21T13:57:52Z</dc:date>
    </item>
    <item>
      <title>Re: eLBC memory map</title>
      <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249058#M452</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Kumar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding the flash types from memory point of view there are 2 types: memory mapped and memory unmapped. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The NOR flash is memory mapped and the rest ones - NAND, SPI, SD - are not memory mapped. &lt;/P&gt;&lt;P&gt;Basically, a memory mapped flash means that reading is similar to reading from random-access memory. You can read any address from the flash zone without using any specific algorithm. Instead, for unmapped flashes (SPI, NAND, SD) you cannot do this - you need a specific flash algorithm who knows how to make the read operations via flash controller (eLBC in this case). You can read more information about flashes principles of operation here [1].&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Returning to your first question, a NAND flash is not a memory mapped flash. Any flash must be assigned to a CS - this is just a normal setting that basically means that a specific range of memory will be used for eLBC via GPCM (used for NOR) or/and FCM (used for NAND).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Being an unmapped flash, for NAND is enough to allocate space only for internal flash controller -&amp;gt; eLBC. This means to allocate space for eLBC registers/buffers that will be used by flash algorithm for controlling the flash device (for read/write operations).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Marius&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;[1] &lt;A href="http://en.wikipedia.org/wiki/Flash_memory" title="http://en.wikipedia.org/wiki/Flash_memory"&gt;Flash memory - Wikipedia, the free encyclopedia&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 14:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249058#M452</guid>
      <dc:creator>marius_grigoras</dc:creator>
      <dc:date>2013-05-21T14:22:35Z</dc:date>
    </item>
    <item>
      <title>Re: eLBC memory map</title>
      <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249059#M453</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Marius,&lt;/P&gt;&lt;P&gt;Well, thanks for the explanation.&lt;/P&gt;&lt;P&gt;I thought NAND is memory mapped to eLBC, and was trying to set the LAWs according to that. Now it is clear and i can map the NAND only for 256KB as specified in datasheet.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Kumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 May 2013 14:51:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249059#M453</guid>
      <dc:creator>FreeScaleLogin</dc:creator>
      <dc:date>2013-05-21T14:51:03Z</dc:date>
    </item>
    <item>
      <title>Re: eLBC memory map</title>
      <link>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249060#M454</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm not sure what you're referring to by "256KB as specified in the datasheet", but the eLBC NAND buffer is only an 8KiB window.&amp;nbsp; You can configure the chipselect for the minimum size of 32KiB.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 May 2013 23:58:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/eLBC-memory-map/m-p/249060#M454</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2013-05-29T23:58:48Z</dc:date>
    </item>
  </channel>
</rss>