<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Problem PCI RC Read_Configuration_Ready_Register from EP</title>
    <link>https://community.nxp.com/t5/P-Series/Problem-PCI-RC-Read-Configuration-Ready-Register-from-EP/m-p/787570#M4478</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="288026" data-username="zy_mooncity" href="https://community.nxp.com/people/zy_mooncity"&gt;Zuo Yun&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EP should run prior RC in order to initialize PEXIWARn and PEX_CFG_READY[&lt;SPAN style="font-size: 12.0pt;"&gt;CFG_READY], otherwise BARn is not write-accessible for RC. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;CFG_READY is set when in EP mode, then the host can start the enumeration process. The transaction layer handles configuration requests from external hosts only after the CFG_READY bit is set. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;So no need to read CFG_READY on EP from the RC.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Jul 2018 11:38:15 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2018-07-26T11:38:15Z</dc:date>
    <item>
      <title>Problem PCI RC Read_Configuration_Ready_Register from EP</title>
      <link>https://community.nxp.com/t5/P-Series/Problem-PCI-RC-Read-Configuration-Ready-Register-from-EP/m-p/787569#M4477</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There are two P2020 boards in my system, one is configured as PCI root complex, and the other is configured as endpoint . The CFG_READY bit of the Read_Configuration_Ready_Register is set once the EP initialization is completed, and the PCI read operation on the EP shows the CFG_READY bit is 1. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the PCI root complex, I want to know if the CFG_READY bit of the EP is set or not, then I try to read the&amp;nbsp;Read_Configuration_Ready_Register from the RC, but the result is always 0. I read Advanced_Error_Reporting_Capability_ID_Register in the same, the expected result is returned (0x0001).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is possible to get the value of&amp;nbsp;Read_Configuration_Ready_Register on the EP from the RC?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 06 Jul 2018 03:21:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Problem-PCI-RC-Read-Configuration-Ready-Register-from-EP/m-p/787569#M4477</guid>
      <dc:creator>zy_mooncity</dc:creator>
      <dc:date>2018-07-06T03:21:19Z</dc:date>
    </item>
    <item>
      <title>Re: Problem PCI RC Read_Configuration_Ready_Register from EP</title>
      <link>https://community.nxp.com/t5/P-Series/Problem-PCI-RC-Read-Configuration-Ready-Register-from-EP/m-p/787570#M4478</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="288026" data-username="zy_mooncity" href="https://community.nxp.com/people/zy_mooncity"&gt;Zuo Yun&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;EP should run prior RC in order to initialize PEXIWARn and PEX_CFG_READY[&lt;SPAN style="font-size: 12.0pt;"&gt;CFG_READY], otherwise BARn is not write-accessible for RC. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;CFG_READY is set when in EP mode, then the host can start the enumeration process. The transaction layer handles configuration requests from external hosts only after the CFG_READY bit is set. &lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 12.0pt;"&gt;So no need to read CFG_READY on EP from the RC.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Jul 2018 11:38:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Problem-PCI-RC-Read-Configuration-Ready-Register-from-EP/m-p/787570#M4478</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2018-07-26T11:38:15Z</dc:date>
    </item>
  </channel>
</rss>