<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Card synchronization in P1010 eSDHC driver multiblock transfers in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248790#M442</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, A D !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How did you solve your issue ?&lt;/P&gt;&lt;P&gt;Because I'm running into something similar on p1024rdb and I can't get 2 consecutive multiple block writes working ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion would be useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 04 Jul 2013 19:09:34 GMT</pubDate>
    <dc:creator>rautaioan-alin</dc:creator>
    <dc:date>2013-07-04T19:09:34Z</dc:date>
    <item>
      <title>Card synchronization in P1010 eSDHC driver multiblock transfers</title>
      <link>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248786#M438</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am implementing multiblock transfers in P1010 eSDHC driver in FreeBSD. The driver already uses SDMA with single block transfers.&lt;/P&gt;&lt;P&gt;The thing is, performing a multiblock write causes Command Timeout (read worked fine). The driver is always waiting for DAT and CMD line (I know I don't always have to wait for DAT line) reading PRSSTAT[CIHB, CDIHB, WTA, RTA], but that seems to be not enough - the driver is only working fine, when I have some debug printf's in interrupt_handler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suppose that I am sending next command before card copy the data from its internal buffer to the card, and thats why CMD Timeout is generated, but how to synchronise it, if PRSSTAT doesn't work? Watermark Level Register is also set to perform slowest transfer.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The code is in attachment.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;regards&lt;/P&gt;&lt;P&gt;Aleksander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG style="color: #51626f; background-color: #ffffff; border: 0px; font-weight: bold;"&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337175"&gt;fsl_sdhc.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2013 11:01:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248786#M438</guid>
      <dc:creator>aleksander</dc:creator>
      <dc:date>2013-04-02T11:01:51Z</dc:date>
    </item>
    <item>
      <title>Re: Card synchronization in P1010 eSDHC driver multiblock transfers</title>
      <link>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248787#M439</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;and related question - what is "stop at block gap" functionality? I don't understand it, and google lacks of answer. should I use it?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Apr 2013 12:19:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248787#M439</guid>
      <dc:creator>aleksander</dc:creator>
      <dc:date>2013-04-02T12:19:06Z</dc:date>
    </item>
    <item>
      <title>Re: Card synchronization in P1010 eSDHC driver multiblock transfers</title>
      <link>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248788#M440</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;See please attached file. This file contains SDHC driver code from Freescale SDK 1.3.2 (&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX&amp;amp;fsrch=1"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX&amp;amp;fsrch=1&lt;/A&gt;).&lt;/P&gt;&lt;P&gt;Compare this driver and your code.&lt;/P&gt;&lt;P&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 07 Apr 2013 06:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248788#M440</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2013-04-07T06:15:16Z</dc:date>
    </item>
    <item>
      <title>Re: Card synchronization in P1010 eSDHC driver multiblock transfers</title>
      <link>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248789#M441</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If the DMA/CPU does not keep up with reading data out of the buffers, SDHC stops the SD_CLK at the block gap to avoid an overflow situation.&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10pt; font-family: arial,helvetica,sans-serif;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10pt; font-family: arial,helvetica,sans-serif;"&gt;The block size can be a multiple of the size of the data buffer. However, it is recommended that the block size be equal to the data buffer size. This allows the SDHC to stop the SD_CLK during block gaps should an overflow or underrun condition occur. Stopping the SD_CLK while the data lines are active may cause data corruption on some cards. If an application or card driver needs to transfer larger sets of data, the host driver should divide the data set into multiple blocks.&lt;/SPAN&gt;&lt;SPAN class="mce_paste_marker"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Apr 2013 08:02:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248789#M441</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2013-04-10T08:02:56Z</dc:date>
    </item>
    <item>
      <title>Re: Card synchronization in P1010 eSDHC driver multiblock transfers</title>
      <link>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248790#M442</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, A D !&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How did you solve your issue ?&lt;/P&gt;&lt;P&gt;Because I'm running into something similar on p1024rdb and I can't get 2 consecutive multiple block writes working ...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any suggestion would be useful.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you in advance,&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 04 Jul 2013 19:09:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Card-synchronization-in-P1010-eSDHC-driver-multiblock-transfers/m-p/248790#M442</guid>
      <dc:creator>rautaioan-alin</dc:creator>
      <dc:date>2013-07-04T19:09:34Z</dc:date>
    </item>
  </channel>
</rss>