<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Using kernel v4.1 for P1022DS based board</title>
    <link>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743183#M4389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on P1022DS based board. I have already programmed the board with kernel v3.12 and file system as in QorIQ BSP v1.9.&lt;/P&gt;&lt;P&gt;BSP v2.0 contains kernel v4.1 but doesn't support P1022DS architecture. &lt;/P&gt;&lt;P&gt;Please suggest how to migrate to kernel v4.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Rajeev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 22 Jan 2018 11:01:58 GMT</pubDate>
    <dc:creator>nandan</dc:creator>
    <dc:date>2018-01-22T11:01:58Z</dc:date>
    <item>
      <title>Using kernel v4.1 for P1022DS based board</title>
      <link>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743183#M4389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on P1022DS based board. I have already programmed the board with kernel v3.12 and file system as in QorIQ BSP v1.9.&lt;/P&gt;&lt;P&gt;BSP v2.0 contains kernel v4.1 but doesn't support P1022DS architecture. &lt;/P&gt;&lt;P&gt;Please suggest how to migrate to kernel v4.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;BR /&gt;Rajeev&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Jan 2018 11:01:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743183#M4389</guid>
      <dc:creator>nandan</dc:creator>
      <dc:date>2018-01-22T11:01:58Z</dc:date>
    </item>
    <item>
      <title>Re: Using kernel v4.1 for P1022DS based board</title>
      <link>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743184#M4390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Look at the following pages:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&lt;A class="jive-link-thread-small" data-containerid="2009" data-containertype="14" data-objectid="457758" data-objecttype="1" href="https://community.nxp.com/thread/457758"&gt;https://community.nxp.com/thread/457758&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&lt;A class="jive-link-wiki-small" data-containerid="2009" data-containertype="14" data-objectid="99961" data-objecttype="102" href="https://community.nxp.com/docs/DOC-99961"&gt;https://community.nxp.com/docs/DOC-99961&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;See also attached file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Jan 2018 03:52:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743184#M4390</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2018-01-24T03:52:16Z</dc:date>
    </item>
    <item>
      <title>Re: Using kernel v4.1 for P1022DS based board</title>
      <link>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743185#M4391</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Both the methods mentioned above didn't work for me. Following is the error log. Please help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log data follows:&lt;BR /&gt;| DEBUG: Executing shell function do_compile&lt;BR /&gt;| NOTE: make -j 4 uImage CC=powerpc-fsl-linux-gnuspe-gcc&amp;nbsp;&amp;nbsp; --sysroot=/home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/sysroots/p1022ds LD=powerpc-fsl-linux-gnuspe-ld.bfd&amp;nbsp;&amp;nbsp; --sysroot=/home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/sysroots/p1022ds LOADADDR=20008000&lt;BR /&gt;| make[2]: Circular arch/powerpc/lib/crtsavres.o &amp;lt;- prepare dependency dropped.&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; HOSTCC&amp;nbsp; scripts/dtc/dtc-lexer.lex.o&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; HOSTCC&amp;nbsp; scripts/genksyms/lex.lex.o&lt;BR /&gt;| dtc-lexer.l:40:28: fatal error: dtc-parser.tab.h: No such file or directory&lt;BR /&gt;| compilation terminated.&lt;BR /&gt;| scripts/genksyms/lex.lex.c_shipped:567:23: fatal error: parse.tab.h: No such file or directory&lt;BR /&gt;| compilation terminated.&lt;BR /&gt;| scripts/Makefile.host:108: recipe for target 'scripts/genksyms/lex.lex.o' failed&lt;BR /&gt;| scripts/Makefile.host:108: recipe for target 'scripts/dtc/dtc-lexer.lex.o' failed&lt;BR /&gt;| make[4]: *** [scripts/dtc/dtc-lexer.lex.o] Error 1&lt;BR /&gt;| make[4]: *** [scripts/genksyms/lex.lex.o] Error 1&lt;BR /&gt;| /home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/work/p1022ds-fsl-linux-gnuspe/linux-qoriq/3.12-r0/git/scripts/Makefile.build:403: recipe for target 'scripts/dtc' failed&lt;BR /&gt;| make[3]: *** [scripts/dtc] Error 2&lt;BR /&gt;| make[3]: *** Waiting for unfinished jobs....&lt;BR /&gt;| /home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/work/p1022ds-fsl-linux-gnuspe/linux-qoriq/3.12-r0/git/scripts/Makefile.build:403: recipe for target 'scripts/genksyms' failed&lt;BR /&gt;| make[3]: *** [scripts/genksyms] Error 2&lt;BR /&gt;| /home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/work/p1022ds-fsl-linux-gnuspe/linux-qoriq/3.12-r0/git/Makefile:555: recipe for target 'scripts' failed&lt;BR /&gt;| make[2]: *** [scripts] Error 2&lt;BR /&gt;| Makefile:146: recipe for target 'sub-make' failed&lt;BR /&gt;| make[1]: *** [sub-make] Error 2&lt;BR /&gt;| Makefile:24: recipe for target '__sub-make' failed&lt;BR /&gt;| make: *** [__sub-make] Error 2&lt;BR /&gt;| ERROR: oe_runmake failed&lt;BR /&gt;| WARNING: /home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/work/p1022ds-fsl-linux-gnuspe/linux-qoriq/3.12-r0/temp/run.do_compile.522:1 exit 1 from&lt;BR /&gt;|&amp;nbsp;&amp;nbsp; exit 1&lt;BR /&gt;| ERROR: Function failed: do_compile (log file is located at /home/prateek/GPON/HPOH/QorIQ_SDK_V1.9-ISO/QorIQ-SDK-V1.9-20151210-yocto/build_p1022ds/tmp/work/p1022ds-fsl-linux-gnuspe/linux-qoriq/3.12-r0/temp/log.do_compile.522)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 26 Feb 2018 04:53:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Using-kernel-v4-1-for-P1022DS-based-board/m-p/743185#M4391</guid>
      <dc:creator>nandan</dc:creator>
      <dc:date>2018-02-26T04:53:02Z</dc:date>
    </item>
  </channel>
</rss>