<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 p1010 ttyS1 input/output error</title>
    <link>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742874#M4380</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI to all, please help me!&lt;/P&gt;&lt;P&gt;ttyS0 and ttyS1 both used duart1 of p1010.&lt;/P&gt;&lt;P&gt;/dev/ttyS0 and /dev/ttyS1 can open success both, ttyS0&amp;nbsp;all is ok, but ttyS1 log input/output error when call tcgetattr().&lt;/P&gt;&lt;P&gt;The kernel message about serial in startup as following:&lt;/P&gt;&lt;P&gt;/////////////////////////////////////////&lt;/P&gt;&lt;P&gt;Serial 825016550 driver, 2 ports, IRQ sharing enabled&lt;BR /&gt;serial8250.0 ttyS0 at MMIO 0xffe04500 (irq = 42, base_baud = 25000000) is a 16550A&lt;BR /&gt;console [ttyS0] enabled, bootconsole disabled&lt;BR /&gt;console [ttyS0] enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;//////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As above showing, there is no about ttyS1 message,but this two uart is configured in dts, as following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;///////////////////////////////////////////////////&lt;/P&gt;&lt;DIV&gt;serial0: &lt;A href="mailto:serial@4500"&gt;serial@4500&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;cell-index = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;device_type = "serial";&lt;BR /&gt;&amp;nbsp;compatible = "fsl,ns16550", "ns16550";&lt;BR /&gt;&amp;nbsp;reg = &amp;lt;0x4500 0x100&amp;gt;;&lt;BR /&gt;&amp;nbsp;clock-frequency = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;interrupts = &amp;lt;42 2 0 0&amp;gt;;&lt;BR /&gt;};&lt;/DIV&gt;&lt;DIV&gt;serial1: serial@4600 {&lt;BR /&gt;&amp;nbsp;cell-index = &amp;lt;1&amp;gt;;&lt;BR /&gt;&amp;nbsp;device_type = "serial";&lt;BR /&gt;&amp;nbsp;compatible = "fsl,ns16550", "ns16550";&lt;BR /&gt;&amp;nbsp;reg = &amp;lt;0x4600 0x100&amp;gt;;&lt;BR /&gt;&amp;nbsp;clock-frequency = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;interrupts = &amp;lt;42 2 0 0&amp;gt;;&lt;BR /&gt;};&lt;/DIV&gt;&lt;P&gt;///////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;There is more as following:&lt;/P&gt;&lt;P&gt;///////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@p1010rdb-pb:/proc/tty/driver"&gt;root@p1010rdb-pb:/proc/tty/driver&lt;/A&gt;# cat serial &lt;BR /&gt;serinfo:1.0 driver revision:&lt;BR /&gt;0: uart:16550A mmio:0xFFE04500 irq:42 tx:1779 rx:236 RTS|DTR&lt;BR /&gt;1: uart:unknown port:00000000 irq:0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//////////////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why no message about ttyS1? Why ttyS1 can not use?&lt;/P&gt;&lt;P&gt;Please help me !&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jun 2018 08:14:49 GMT</pubDate>
    <dc:creator>jungong</dc:creator>
    <dc:date>2018-06-01T08:14:49Z</dc:date>
    <item>
      <title>p1010 ttyS1 input/output error</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742874#M4380</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;HI to all, please help me!&lt;/P&gt;&lt;P&gt;ttyS0 and ttyS1 both used duart1 of p1010.&lt;/P&gt;&lt;P&gt;/dev/ttyS0 and /dev/ttyS1 can open success both, ttyS0&amp;nbsp;all is ok, but ttyS1 log input/output error when call tcgetattr().&lt;/P&gt;&lt;P&gt;The kernel message about serial in startup as following:&lt;/P&gt;&lt;P&gt;/////////////////////////////////////////&lt;/P&gt;&lt;P&gt;Serial 825016550 driver, 2 ports, IRQ sharing enabled&lt;BR /&gt;serial8250.0 ttyS0 at MMIO 0xffe04500 (irq = 42, base_baud = 25000000) is a 16550A&lt;BR /&gt;console [ttyS0] enabled, bootconsole disabled&lt;BR /&gt;console [ttyS0] enabled, bootconsole disabled&lt;/P&gt;&lt;P&gt;//////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As above showing, there is no about ttyS1 message,but this two uart is configured in dts, as following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;///////////////////////////////////////////////////&lt;/P&gt;&lt;DIV&gt;serial0: &lt;A href="mailto:serial@4500"&gt;serial@4500&lt;/A&gt; {&lt;BR /&gt;&amp;nbsp;cell-index = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;device_type = "serial";&lt;BR /&gt;&amp;nbsp;compatible = "fsl,ns16550", "ns16550";&lt;BR /&gt;&amp;nbsp;reg = &amp;lt;0x4500 0x100&amp;gt;;&lt;BR /&gt;&amp;nbsp;clock-frequency = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;interrupts = &amp;lt;42 2 0 0&amp;gt;;&lt;BR /&gt;};&lt;/DIV&gt;&lt;DIV&gt;serial1: serial@4600 {&lt;BR /&gt;&amp;nbsp;cell-index = &amp;lt;1&amp;gt;;&lt;BR /&gt;&amp;nbsp;device_type = "serial";&lt;BR /&gt;&amp;nbsp;compatible = "fsl,ns16550", "ns16550";&lt;BR /&gt;&amp;nbsp;reg = &amp;lt;0x4600 0x100&amp;gt;;&lt;BR /&gt;&amp;nbsp;clock-frequency = &amp;lt;0&amp;gt;;&lt;BR /&gt;&amp;nbsp;interrupts = &amp;lt;42 2 0 0&amp;gt;;&lt;BR /&gt;};&lt;/DIV&gt;&lt;P&gt;///////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;There is more as following:&lt;/P&gt;&lt;P&gt;///////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&lt;A href="mailto:root@p1010rdb-pb:/proc/tty/driver"&gt;root@p1010rdb-pb:/proc/tty/driver&lt;/A&gt;# cat serial &lt;BR /&gt;serinfo:1.0 driver revision:&lt;BR /&gt;0: uart:16550A mmio:0xFFE04500 irq:42 tx:1779 rx:236 RTS|DTR&lt;BR /&gt;1: uart:unknown port:00000000 irq:0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;//////////////////////////////////////////////////////&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Why no message about ttyS1? Why ttyS1 can not use?&lt;/P&gt;&lt;P&gt;Please help me !&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jun 2018 08:14:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742874#M4380</guid>
      <dc:creator>jungong</dc:creator>
      <dc:date>2018-06-01T08:14:49Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 ttyS1 input/output error</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742875#M4381</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please look this community topic:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/387283"&gt;https://community.nxp.com/thread/387283&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope it will be helpful&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Jun 2018 05:24:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742875#M4381</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2018-06-02T05:24:50Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 ttyS1 input/output error</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742876#M4382</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you very much!&lt;/P&gt;&lt;P&gt;It solves my problem.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Jun 2018 08:37:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-ttyS1-input-output-error/m-p/742876#M4382</guid>
      <dc:creator>jungong</dc:creator>
      <dc:date>2018-06-04T08:37:28Z</dc:date>
    </item>
  </channel>
</rss>