<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 FMAN_v2 L4 checksum computation when IPF is enabled</title>
    <link>https://community.nxp.com/t5/P-Series/FMAN-v2-L4-checksum-computation-when-IPF-is-enabled/m-p/740234#M4372</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any way to compute L4 checksum in HW with FMAN_v2 when IP fragmentation is also enabled ? In my scenario, the frames are forwarded from OP port to TX the port. It seems for FMAN_v3 it should be possible according to the docs by using HM commands, but what about FMAN_v2 (p4080 board, for example) ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 01 Nov 2017 17:49:39 GMT</pubDate>
    <dc:creator>alinrauta</dc:creator>
    <dc:date>2017-11-01T17:49:39Z</dc:date>
    <item>
      <title>FMAN_v2 L4 checksum computation when IPF is enabled</title>
      <link>https://community.nxp.com/t5/P-Series/FMAN-v2-L4-checksum-computation-when-IPF-is-enabled/m-p/740234#M4372</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is there any way to compute L4 checksum in HW with FMAN_v2 when IP fragmentation is also enabled ? In my scenario, the frames are forwarded from OP port to TX the port. It seems for FMAN_v3 it should be possible according to the docs by using HM commands, but what about FMAN_v2 (p4080 board, for example) ?&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Alin&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Nov 2017 17:49:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/FMAN-v2-L4-checksum-computation-when-IPF-is-enabled/m-p/740234#M4372</guid>
      <dc:creator>alinrauta</dc:creator>
      <dc:date>2017-11-01T17:49:39Z</dc:date>
    </item>
  </channel>
</rss>