<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Aurora Connector P2041</title>
    <link>https://community.nxp.com/t5/P-Series/Aurora-Connector-P2041/m-p/727833#M4339</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Is this normal?&lt;/P&gt;&lt;P&gt;This is "cut and paste" issue when the figures were taken from P3041 Hardware Specifications "as is", which is not correct for the P2041.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P2041 has only one Debug/Aurora lane - Lane A in the SerDes Bank2 (SD_TX/RX[10])&lt;/P&gt;&lt;P&gt;The corrected Figure 58:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8510i418696386F72B1E9/image-size/large?v=v2&amp;amp;px=999" title="2018-04-13_131308.jpg" alt="2018-04-13_131308.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 13 Apr 2018 06:17:09 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2018-04-13T06:17:09Z</dc:date>
    <item>
      <title>Aurora Connector P2041</title>
      <link>https://community.nxp.com/t5/P-Series/Aurora-Connector-P2041/m-p/727832#M4338</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a question about the Aurora connector of the P2041.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In document &lt;A href="https://www.nxp.com/webapp/Download?colCode=P2041EC&amp;amp;Parent_nodeId=1281971859333684758626&amp;amp;Parent_pageType=product&amp;amp;Parent_nodeId=1281971859333684758626&amp;amp;Parent_pageType=product"&gt;P2041 QorIQ Integrated Processor Hardware Specifications&lt;/A&gt;, Figure 58, SD_TX09_P and all others are not in "Table 1. Pin List by Bus".&lt;BR /&gt;Is this normal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I may not have understood the SerDes use.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thank you in advance&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Apr 2018 14:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Aurora-Connector-P2041/m-p/727832#M4338</guid>
      <dc:creator>guillaume17</dc:creator>
      <dc:date>2018-04-12T14:17:09Z</dc:date>
    </item>
    <item>
      <title>Re: Aurora Connector P2041</title>
      <link>https://community.nxp.com/t5/P-Series/Aurora-Connector-P2041/m-p/727833#M4339</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; Is this normal?&lt;/P&gt;&lt;P&gt;This is "cut and paste" issue when the figures were taken from P3041 Hardware Specifications "as is", which is not correct for the P2041.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P2041 has only one Debug/Aurora lane - Lane A in the SerDes Bank2 (SD_TX/RX[10])&lt;/P&gt;&lt;P&gt;The corrected Figure 58:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8510i418696386F72B1E9/image-size/large?v=v2&amp;amp;px=999" title="2018-04-13_131308.jpg" alt="2018-04-13_131308.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Apr 2018 06:17:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Aurora-Connector-P2041/m-p/727833#M4339</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-04-13T06:17:09Z</dc:date>
    </item>
  </channel>
</rss>