<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: p1010 localbus dead in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716531#M4315</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the log the SDK being used is very old.&lt;/P&gt;&lt;P&gt;In the SDK v1.9 the U-Boot is:&lt;/P&gt;&lt;P&gt;U-Boot 2015.01+SDKv1.9+geb3d4fc (Dec 03 2015 - 21:18:10)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is recommended to use the latest SDK v1.9.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Jan 2018 05:12:45 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2018-01-16T05:12:45Z</dc:date>
    <item>
      <title>p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716526#M4310</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;p1010 localbus hardconnet such as:cs1--norflash ;cs2--nandflash; cs3--cpld&lt;BR /&gt;I find cpu dead when I operation of three peripherals at the same time in diffrent task (in linux), I want to know if the driver needs mutual protection? but norflash nandflash are linux itself drvier.&lt;/P&gt;&lt;P&gt;I wonder if there's a design flaws with localbus ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 07:47:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716526#M4310</guid>
      <dc:creator>helloboy</dc:creator>
      <dc:date>2018-01-12T07:47:09Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716527#M4311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Which NXP SDK is used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 07:57:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716527#M4311</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-12T07:57:43Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716528#M4312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;it seems like QorIQ-SDK-V1.4&amp;nbsp; (linux2.6.35)&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 08:11:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716528#M4312</guid>
      <dc:creator>helloboy</dc:creator>
      <dc:date>2018-01-12T08:11:36Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716529#M4313</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please provide U-Boot booting log as text attachment.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Jan 2018 10:34:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716529#M4313</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-12T10:34:08Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716530#M4314</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;U-Boot 2010.12 (May 12 2016 - 21:40:36) V1.01&lt;/P&gt;&lt;P&gt;CPU: P1010, Version: 2.0, (0x80f10020)&lt;BR /&gt;Core: E500, Version: 5.2, (0x80212152)&lt;BR /&gt;Clock Configuration:&lt;BR /&gt; CPU0:800 MHz, &lt;BR /&gt; CCB:400 MHz,&lt;BR /&gt; DDR:400 MHz (800 MT/s data rate) (Asynchronous), IFC:100 MHz&lt;BR /&gt;L1: D-cache 32 kB enabled&lt;BR /&gt; I-cache 32 kB enabled&lt;BR /&gt;Board: P1010ACCE &lt;BR /&gt;I2C: ready&lt;BR /&gt;SPI: ready&lt;BR /&gt;DRAM: Configuring DDR for 667 MT/s data rate&lt;BR /&gt;DDR: 1 GiB (DDR3, 32-bit, CL=6, ECC off)&lt;BR /&gt;FLASH: 32 MiB&lt;BR /&gt;L2: 256 KB enabled&lt;BR /&gt;NAND: NAND device: Manufacturer ID: 0xef, Chip ID: 0xd3 (Unknown NAND 1GiB 3,3V 8-bit)&lt;BR /&gt;1024 MiB&lt;BR /&gt;PCIe1: Root Complex of mini PCIe Slot, no link, regs @ 0xffe0a000&lt;BR /&gt;PCIe1: Bus 00 - 00&lt;BR /&gt;PCIe2: Root Complex of PCIe Slot, no link, regs @ 0xffe09000&lt;BR /&gt;PCIe2: Bus 01 - 01&lt;BR /&gt;In: serial&lt;BR /&gt;Out: serial&lt;BR /&gt;Err: serial&lt;/P&gt;&lt;P&gt;Net: eTSEC1: Not support &lt;BR /&gt;eTSEC2: No support for PHY id ffffffff; assuming generic&lt;BR /&gt;eTSEC3: No support for PHY id ffffffff; assuming generic&lt;BR /&gt;eTSEC1, eTSEC2, eTSEC3&lt;/P&gt;&lt;P&gt;................................................................&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 04:06:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716530#M4314</guid>
      <dc:creator>helloboy</dc:creator>
      <dc:date>2018-01-16T04:06:31Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716531#M4315</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;According to the log the SDK being used is very old.&lt;/P&gt;&lt;P&gt;In the SDK v1.9 the U-Boot is:&lt;/P&gt;&lt;P&gt;U-Boot 2015.01+SDKv1.9+geb3d4fc (Dec 03 2015 - 21:18:10)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is recommended to use the latest SDK v1.9.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 05:12:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716531#M4315</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2018-01-16T05:12:45Z</dc:date>
    </item>
    <item>
      <title>Re: p1010 localbus dead</title>
      <link>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716532#M4316</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there &amp;nbsp;localbus problem &amp;nbsp;in old sdk ? &amp;nbsp; uboot &amp;nbsp;or linux driver has problem ? &amp;nbsp;Please describe more in detail &amp;nbsp;at this problem. update sdk is huge job, i want to reslove this problem quickly!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Jan 2018 11:52:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/p1010-localbus-dead/m-p/716532#M4316</guid>
      <dc:creator>helloboy</dc:creator>
      <dc:date>2018-01-16T11:52:07Z</dc:date>
    </item>
  </channel>
</rss>