<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic P4080DS Srio performance issue in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/P4080DS-Srio-performance-issue/m-p/712097#M4293</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´ve a performance problem writing to a SRIO (1x &amp;nbsp;lane) device using outbound window with NWRITE.&lt;/P&gt;&lt;P&gt;When I write to the outbound window all data transmitted correct to the device but &amp;nbsp;the speed is very slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A loop writing 200 32 Bit values (800 Byte) to the outbound window takes about 46 µs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint32_t *&lt;SPAN&gt;OutboundAddr =...;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;for(i = 0; i &amp;lt; 200; i++)&lt;BR /&gt; {&lt;BR /&gt;*OutboundAddr = 123;&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRIO is configured to have 2.5 GBit so I would expect a time ~3.2 µs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other direction (device to Inbound window) works much better. Here transmission time is very near to the theoretical value.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I don´t understand why the the NWRITE to the outbound window is so slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 31 Aug 2017 05:12:26 GMT</pubDate>
    <dc:creator>andrewesterholz</dc:creator>
    <dc:date>2017-08-31T05:12:26Z</dc:date>
    <item>
      <title>P4080DS Srio performance issue</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-Srio-performance-issue/m-p/712097#M4293</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I´ve a performance problem writing to a SRIO (1x &amp;nbsp;lane) device using outbound window with NWRITE.&lt;/P&gt;&lt;P&gt;When I write to the outbound window all data transmitted correct to the device but &amp;nbsp;the speed is very slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;A loop writing 200 32 Bit values (800 Byte) to the outbound window takes about 46 µs.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;uint32_t *&lt;SPAN&gt;OutboundAddr =...;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;for(i = 0; i &amp;lt; 200; i++)&lt;BR /&gt; {&lt;BR /&gt;*OutboundAddr = 123;&lt;BR /&gt; }&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SRIO is configured to have 2.5 GBit so I would expect a time ~3.2 µs&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The other direction (device to Inbound window) works much better. Here transmission time is very near to the theoretical value.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Currently I don´t understand why the the NWRITE to the outbound window is so slow.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards&lt;/P&gt;&lt;P&gt;Andre&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Aug 2017 05:12:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-Srio-performance-issue/m-p/712097#M4293</guid>
      <dc:creator>andrewesterholz</dc:creator>
      <dc:date>2017-08-31T05:12:26Z</dc:date>
    </item>
  </channel>
</rss>