<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: T2080 SPI /dev/spi is not creating.</title>
    <link>https://community.nxp.com/t5/P-Series/T2080-SPI-dev-spi-is-not-creating/m-p/711878#M4292</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vidya,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPI is not like I2C, there are not typically SPI devices nodes and the SPI isn't accessed directly by userspace. Each SPI device connect to SPI interface must have a SPI client driver for it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could refer to drivers/mtd/devices/m25p80.c for SPI device driver development.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sun, 17 Sep 2017 09:01:03 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2017-09-17T09:01:03Z</dc:date>
    <item>
      <title>T2080 SPI /dev/spi is not creating.</title>
      <link>https://community.nxp.com/t5/P-Series/T2080-SPI-dev-spi-is-not-creating/m-p/711877#M4291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are using SDK2.0 to boot T2080RDB, we can see in the kernel log spi memory device is detecting with CS0 and working fine.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are four spi CS is configured in the dts file but there is no /dev/spi device is creating in the linux user space.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know how /dev/spi will create.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Vidya&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Aug 2017 13:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/T2080-SPI-dev-spi-is-not-creating/m-p/711877#M4291</guid>
      <dc:creator>vidyasagartata</dc:creator>
      <dc:date>2017-08-30T13:00:06Z</dc:date>
    </item>
    <item>
      <title>Re: T2080 SPI /dev/spi is not creating.</title>
      <link>https://community.nxp.com/t5/P-Series/T2080-SPI-dev-spi-is-not-creating/m-p/711878#M4292</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Vidya,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SPI is not like I2C, there are not typically SPI devices nodes and the SPI isn't accessed directly by userspace. Each SPI device connect to SPI interface must have a SPI client driver for it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You could refer to drivers/mtd/devices/m25p80.c for SPI device driver development.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Sep 2017 09:01:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/T2080-SPI-dev-spi-is-not-creating/m-p/711878#M4292</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-09-17T09:01:03Z</dc:date>
    </item>
  </channel>
</rss>