<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic XPedite5501 P2020e. Active ethernet issue (u boot) in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/XPedite5501-P2020e-Active-ethernet-issue-u-boot/m-p/705208#M4279</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When powering-on XPedite5501, u boot shows: Net: eTSEC1, eTSEC2. Indicating&amp;nbsp;there are two Ethernet ports available. When I run "printenv" I see ethact = eTSEC1. I set ethact to etSEC2 by "setenv ethact eTSEC2", then save ("saveenv"). If I power cycle, ethact defaults to eTSEC1. Both ethernet ports have worked. I managed to switch between them once before. Now I can't seem to prevent P2020e from defaulting to ethact = eTSEC1. My goal is to have both ethernet ports talking "simultaneously". From what I've tried, I'm only allowed to have one talking&amp;nbsp;even though they are both connected to a single switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 22 Aug 2017 20:21:59 GMT</pubDate>
    <dc:creator>nfarabee</dc:creator>
    <dc:date>2017-08-22T20:21:59Z</dc:date>
    <item>
      <title>XPedite5501 P2020e. Active ethernet issue (u boot)</title>
      <link>https://community.nxp.com/t5/P-Series/XPedite5501-P2020e-Active-ethernet-issue-u-boot/m-p/705208#M4279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When powering-on XPedite5501, u boot shows: Net: eTSEC1, eTSEC2. Indicating&amp;nbsp;there are two Ethernet ports available. When I run "printenv" I see ethact = eTSEC1. I set ethact to etSEC2 by "setenv ethact eTSEC2", then save ("saveenv"). If I power cycle, ethact defaults to eTSEC1. Both ethernet ports have worked. I managed to switch between them once before. Now I can't seem to prevent P2020e from defaulting to ethact = eTSEC1. My goal is to have both ethernet ports talking "simultaneously". From what I've tried, I'm only allowed to have one talking&amp;nbsp;even though they are both connected to a single switch.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any advice on this?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Aug 2017 20:21:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/XPedite5501-P2020e-Active-ethernet-issue-u-boot/m-p/705208#M4279</guid>
      <dc:creator>nfarabee</dc:creator>
      <dc:date>2017-08-22T20:21:59Z</dc:date>
    </item>
    <item>
      <title>Re: XPedite5501 P2020e. Active ethernet issue (u boot)</title>
      <link>https://community.nxp.com/t5/P-Series/XPedite5501-P2020e-Active-ethernet-issue-u-boot/m-p/705209#M4280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It looks that&amp;nbsp; you can only (easily) access one port at a time. There is also only one static IP address assignment and the &lt;STRONG&gt;ipaddr&lt;/STRONG&gt; environment variable.&lt;/P&gt;&lt;P&gt;Please set the default to eTSEC2 as the following.&lt;/P&gt;&lt;P&gt;=&amp;gt; setenv ethact eTSEC2&lt;BR /&gt;=&amp;gt; setenv ethprime eTSEC2&lt;BR /&gt;=&amp;gt; save&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Sep 2017 12:31:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/XPedite5501-P2020e-Active-ethernet-issue-u-boot/m-p/705209#M4280</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-09-17T12:31:56Z</dc:date>
    </item>
  </channel>
</rss>