<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Re: Programming the Flash gives Sector Protection Error</title>
    <link>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699828#M4248</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP was very helpful in getting this fixed. The solution was a new elf file for the new chip set. The new one seems to work on the older one too. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ram Krishnan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Dec 2017 14:34:12 GMT</pubDate>
    <dc:creator>ramkrishnan</dc:creator>
    <dc:date>2017-12-01T14:34:12Z</dc:date>
    <item>
      <title>Programming the Flash gives Sector Protection Error</title>
      <link>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699826#M4246</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We have a board with the P1022 processor and we had a Cypress (formerly spansion) chip S29GL01GP11TFIR1 for the flash. But that has been obsoleted now and we had to replace it with S29GL01GT10TF1010 chip.&amp;nbsp;&lt;/P&gt;&lt;P&gt;When we trying put the u-boot.bin file using codewarrior we get the following error.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Error: Program with Verify failed. Flash driver reports the following error(s): Sector Protection Error&lt;BR /&gt;Error: Program with Verify failed. Flash driver reports the following error(s): Sector Protection Error&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;One thing we do see is that the only device listed under "Add Device" is&amp;nbsp;S29GL01GP (We also tried the&amp;nbsp;S29GL01GP-Simics, but for our case 64Mx16X2 it is the same in both the xml files which is amd16x2.elf) , we do not see a S29GL01GT.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there an elf file for this chip ?&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;The erase, dump (read operation) all seems to work fine and goes thru sucessfully.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have also attached the Diagnose for both the old flash(S29GL01GP11TFIR1) and the new flash(S29GL01GT10TF1010) and attached it.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Please let me know if you need any more information.&amp;nbsp;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Ram Krishnan&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337250"&gt;OldFlashDiagnose.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337250"&gt;NewFlashDiagnose.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 Oct 2017 17:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699826#M4246</guid>
      <dc:creator>ramkrishnan</dc:creator>
      <dc:date>2017-10-05T17:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the Flash gives Sector Protection Error</title>
      <link>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699827#M4247</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please create a Technical Case for the in-depth issue investigation:&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fcommunity.freescale.com%2Fthread%2F381898" rel="nofollow" target="_blank"&gt;https://community.freescale.com/thread/381898&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Oct 2017 15:56:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699827#M4247</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-10-09T15:56:55Z</dc:date>
    </item>
    <item>
      <title>Re: Programming the Flash gives Sector Protection Error</title>
      <link>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699828#M4248</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;NXP was very helpful in getting this fixed. The solution was a new elf file for the new chip set. The new one seems to work on the older one too. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Ram Krishnan&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Dec 2017 14:34:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Programming-the-Flash-gives-Sector-Protection-Error/m-p/699828#M4248</guid>
      <dc:creator>ramkrishnan</dc:creator>
      <dc:date>2017-12-01T14:34:12Z</dc:date>
    </item>
  </channel>
</rss>