<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: DDR3 Memory Interface Configuration for U-boot</title>
    <link>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691716#M4221</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DDR_DDR_SDRAM_CFG[x32_EN] is not correct option if you use x16 chips to form 32-bit DDR bus. You need to set DDR_DDR_SDRAM_CFG[x32_EN] = 0, and DDR_DDR_SDRAM_CFG[DBW] = 01. In other words you do not need to modify value of the DDR_DDR_SDRAM_CFG register in the p1_p2_rdb_pc.h file. Also you need to set correctly CS0_BNDS register, (0x0000000F in your case) and number of rows in the CS0_CONFIG register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 26 May 2017 11:43:17 GMT</pubDate>
    <dc:creator>Bulat</dc:creator>
    <dc:date>2017-05-26T11:43:17Z</dc:date>
    <item>
      <title>DDR3 Memory Interface Configuration for U-boot</title>
      <link>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691715#M4220</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Our board design involves a P1015 processor which is connected to two DDR3 SDRAM chips in 64M*16 (8 bank * 8Mbit * 16). That is the whole 32 bit bus of memory controller in the processor is connected to two 16 bit DDR3 chips. To configure this in u-boot we have&amp;nbsp;made use of DDR_DDR_SDRAM_CFG[x32_EN] bit, which we have cleared as instructed by the definition of that bit. We have correspondingly changed the bit in the p1_p2_rdb_pc.h file in the /include/configs folder in u-boot. Is this it or do we have to make any further changes elsewhere to reflect this configuration.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;References used were &amp;nbsp;- P1024RM, AN4039&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also if possible could you suggest any other references with regard to configuring this part for the&amp;nbsp;u-boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S. - The reference board P1024RDB uses a x8 configuration(of 4 chips) as compared to our board's configuration of x16.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 May 2017 06:37:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691715#M4220</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-05-24T06:37:18Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Memory Interface Configuration for U-boot</title>
      <link>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691716#M4221</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;DDR_DDR_SDRAM_CFG[x32_EN] is not correct option if you use x16 chips to form 32-bit DDR bus. You need to set DDR_DDR_SDRAM_CFG[x32_EN] = 0, and DDR_DDR_SDRAM_CFG[DBW] = 01. In other words you do not need to modify value of the DDR_DDR_SDRAM_CFG register in the p1_p2_rdb_pc.h file. Also you need to set correctly CS0_BNDS register, (0x0000000F in your case) and number of rows in the CS0_CONFIG register.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 11:43:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691716#M4221</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2017-05-26T11:43:17Z</dc:date>
    </item>
    <item>
      <title>Re: DDR3 Memory Interface Configuration for U-boot</title>
      <link>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691717#M4222</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Bulat,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for your reply. I have set the DDR_DDR_SDRAM_CFG[x32_EN] = 0 and the DDR_DDR_SDRAM_CFG[DBW] to be 01. Other than this, I will try setting the address to the DDR device as per your suggestion. Is this it, do we need any other configuration change to reflect this in the software (u-boot) part?&lt;/P&gt;&lt;P&gt;(asking this out of curiosity) In that case how is this value reflected in the u-boot?&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Pavankumar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 May 2017 11:59:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/DDR3-Memory-Interface-Configuration-for-U-boot/m-p/691717#M4222</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-05-26T11:59:41Z</dc:date>
    </item>
  </channel>
</rss>