<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot? in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Do-the-RGMII-reference-clock-inputs-EC1-GTX-CLK125-and-EC2-GTX/m-p/689647#M4215</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do the RGMII reference clock inputs,&amp;nbsp; EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040have to running at boot time or can they be enabled after boot?&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;.&amp;nbsp; I need to know if those two clocks have to be running at power up or if they can be enabled after boot up.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jun 2017 14:44:17 GMT</pubDate>
    <dc:creator>aduarte</dc:creator>
    <dc:date>2017-06-16T14:44:17Z</dc:date>
    <item>
      <title>Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?</title>
      <link>https://community.nxp.com/t5/P-Series/Do-the-RGMII-reference-clock-inputs-EC1-GTX-CLK125-and-EC2-GTX/m-p/689647#M4215</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Do the RGMII reference clock inputs,&amp;nbsp; EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040have to running at boot time or can they be enabled after boot?&amp;nbsp;&lt;SPAN style="font-size: 11.0pt;"&gt;.&amp;nbsp; I need to know if those two clocks have to be running at power up or if they can be enabled after boot up.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2017 14:44:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Do-the-RGMII-reference-clock-inputs-EC1-GTX-CLK125-and-EC2-GTX/m-p/689647#M4215</guid>
      <dc:creator>aduarte</dc:creator>
      <dc:date>2017-06-16T14:44:17Z</dc:date>
    </item>
    <item>
      <title>Re: Do the RGMII reference clock inputs,  EC1_GTX_CLK125 and EC2_GTX_CLK125, on the P2040 have to running at boot time or can they be enabled after boot?</title>
      <link>https://community.nxp.com/t5/P-Series/Do-the-RGMII-reference-clock-inputs-EC1-GTX-CLK125-and-EC2-GTX/m-p/689648#M4216</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;EC1_GTX_CLK125 and EC2_GTX_CLK125 on the P2040&lt;/SPAN&gt; can be enabled after boot.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 19 Jun 2017 10:32:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Do-the-RGMII-reference-clock-inputs-EC1-GTX-CLK125-and-EC2-GTX/m-p/689648#M4216</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2017-06-19T10:32:34Z</dc:date>
    </item>
  </channel>
</rss>