<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Internal Boot ROM configuration on P1015</title>
    <link>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687785#M4210</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the&amp;nbsp;QorIQ SDK 1.3 Info Center document available at:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=6055991" title="https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=6055991"&gt;https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=6055991&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Corresponding sections are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.2.11.3 3. System Memory Map&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Table 3-54. NOR flash memory map&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4.2.2.1 Flashing U-Boot&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 16 Jun 2017 03:31:25 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2017-06-16T03:31:25Z</dc:date>
    <item>
      <title>Internal Boot ROM configuration on P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687782#M4207</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a P1015 bareboard that needs to be brought up using U-boot. I have built&amp;nbsp;the necessary u-boot.bin for the board. I have also configured the DDR3 that is connected to this processor. I noticed an internal BOOT ROM reserved on the processor in the CCSR device specific utilities in the address space&amp;nbsp;0xF_0000 - 0xF_FFFF . Is this Boot ROM pre-configured (does it have some code that can configure the boot or load the boot using this code) or should it be configured for our specific use. If it must be configured should I try the QCVS tool for BOOT ROM configuration? Please advise.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;P.S - I have only NOR Flash on my board using which I plan to boot up my board.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 06:33:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687782#M4207</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-06-15T06:33:17Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Boot ROM configuration on P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687783#M4208</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The internal on-chip ROM contains code required for booting from eSPI or eSDHC interface - refer to the P1024 QorIQ Integrated Processor Reference Manual, 4.6 Initialization/applications information.&lt;/P&gt;&lt;P&gt;The on-chip ROM code can't be altered by any means and can't be used for different purposes except booting from eSPI or eSDHC.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 07:03:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687783#M4208</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-06-15T07:03:58Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Boot ROM configuration on P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687784#M4209</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How do I go about booting the board? Should I just flash the code onto the NOR Flash (I am using the same chip as that of the reference board on my custom board - that of &amp;nbsp;S29GL128P. Like I mentioned this is the only source of boot). I am a newbie with this aspect, so could you brief me about the flashing of u-boot.(whether I can directly write the u-boot onto the flash).&lt;/P&gt;&lt;P&gt;Thank you for your reply!&amp;nbsp;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Jun 2017 08:26:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687784#M4209</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-06-15T08:26:02Z</dc:date>
    </item>
    <item>
      <title>Re: Internal Boot ROM configuration on P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687785#M4210</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please refer to the&amp;nbsp;QorIQ SDK 1.3 Info Center document available at:&lt;/P&gt;&lt;P&gt;&lt;A class="link-titled" href="https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=6055991" title="https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=6055991"&gt;https://nxp.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=6055991&lt;/A&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Corresponding sections are:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;3.2.11.3 3. System Memory Map&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Table 3-54. NOR flash memory map&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;4.2.2.1 Flashing U-Boot&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2017 03:31:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Internal-Boot-ROM-configuration-on-P1015/m-p/687785#M4210</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2017-06-16T03:31:25Z</dc:date>
    </item>
  </channel>
</rss>