<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Memory Mapping in P1015</title>
    <link>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678228#M4117</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually external device memory map and memory controller (eLBC) bank sizes can be different. The memory controller bank size is set in the bank option register as bit mask for address. Due to that continuous memory block will be aligned on its size boundary. You can set bank memory size greater than the FPGA requires and use only unaligned part of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Jul 2017 03:30:32 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2017-07-03T03:30:32Z</dc:date>
    <item>
      <title>Memory Mapping in P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678225#M4114</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am currently using a P1015 based custom board which is to be booted using U-boot. I am currently planning to have a custom memory mapping for the board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The memory mapping of the custom board is as follows:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;0x0000_0000 - 0x0FFF_FFFF &amp;nbsp;&amp;nbsp; DDR3 (Size - 256M)&lt;/P&gt;&lt;P&gt;0x1010_0000 - 0x101F_FFFF&amp;nbsp;&amp;nbsp;&amp;nbsp; NVRAM (Size - 1M)&lt;/P&gt;&lt;P&gt;0x1030_0000 - 0x122F_FFFF&amp;nbsp;&amp;nbsp;&amp;nbsp; FPGA&amp;nbsp; (Size - 32M)&lt;/P&gt;&lt;P&gt;0xF7F0_0000 - 0xF7FF_FFFF&amp;nbsp;&amp;nbsp; CCSR (Size - 1M)&lt;/P&gt;&lt;P&gt;0xF800_0000 - 0xF8FF_FFFF&amp;nbsp;&amp;nbsp;&amp;nbsp; Boot Flash (Size - 16M)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I correct in assuming that the memory mapping can be changed to suit our requirements. Or are there any constraints to be followed in the memory mapping. Please advice.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 14:03:08 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678225#M4114</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-06-29T14:03:08Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Mapping in P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678226#M4115</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes the memory mapping can be changed. Notice in the memory controller you should set base address aligned to the bank size. I.e. for 32 M you cannot set 0x1030_0000 as base address. Set for example 0x1200_0000.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 17:04:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678226#M4115</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2017-06-29T17:04:40Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Mapping in P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678227#M4116</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Should the constraint of setting the base address aligned to bank size be followed for FPGA strictly, because the FPGA's internal memory mapping has been done using 0x1030_0000 as the base address. Also should this alignment of base address mentioned by you be followed for other devices too (like the NVRAM or CCSR) ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 05:14:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678227#M4116</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-06-30T05:14:57Z</dc:date>
    </item>
    <item>
      <title>Re: Memory Mapping in P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678228#M4117</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Actually external device memory map and memory controller (eLBC) bank sizes can be different. The memory controller bank size is set in the bank option register as bit mask for address. Due to that continuous memory block will be aligned on its size boundary. You can set bank memory size greater than the FPGA requires and use only unaligned part of it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 03:30:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Memory-Mapping-in-P1015/m-p/678228#M4117</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2017-07-03T03:30:32Z</dc:date>
    </item>
  </channel>
</rss>