<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Adding a file/folder in rootfs nxp yocto build in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677370#M4109</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pavel for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After step 5 , when I try to copy binaries into the location /mnt/iso_1, it says "No space left on device". How the size of mounted location can be increased to accommodate more binaries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Jun 2017 05:12:57 GMT</pubDate>
    <dc:creator>rammurmu</dc:creator>
    <dc:date>2017-06-30T05:12:57Z</dc:date>
    <item>
      <title>Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677368#M4107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi ,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I am trying to add a file in rootfs so that the subsequent built image contain the added file/folder. I am performing the following steps -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Adding an entry for file in base-files_3.0.14.bb&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. Keeping corresponding file under ../poky/meta/recipes-core/base-files/base-files/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. bitbake -c compile base-files&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;4. bitbake fsl-image-minimal&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am getting the following error -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;ERROR: QA Issue: non debug package contains .debug directory: base-files path /work/p1022ds-fsl-linux-gnuspe/base-files/3.0.14-r86/packages-split/base-files/.debug/test_i2c_p1022&lt;BR /&gt;ERROR: QA run found fatal errors. Please consider fixing them.&lt;BR /&gt;ERROR: Function failed: do_package_qa&lt;BR /&gt;ERROR: Logfile of failure stored in: /home/ram/POTP/SDK-V1.8/QorIQ-SDK-V1.8-20150619-yocto/build_p1022ds_release/tmp/work/p1022ds-fsl-linux-gnuspe/base-files/3.0.14-r86/temp/log.do_package.8502&lt;BR /&gt;ERROR: Task 747 (/home/ram/POTP/SDK-V1.8/QorIQ-SDK-V1.8-20150619-yocto/poky/meta/recipes-core/base-files/base-files_3.0.14.bb, do_package) failed with exit code '1'&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;What is the problem and how to rectify it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 03:48:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677368#M4107</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2017-06-29T03:48:59Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677369#M4108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Look at SDK 2.0-1703 documentation about &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;adding a pre-built binary into the rootfs:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.nxp.com%2Fdocs%2Fen%2Fsupporting-information%2FQORIQ-SDK-2.0-IC-REV0.pdf" rel="nofollow" target="_blank"&gt;http://www.nxp.com/docs/en/supporting-information/QORIQ-SDK-2.0-IC-REV0.pdf&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Find &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;FAQ in this document.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;There is the other method for adding your files to &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;RAM disk image&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Use the following command sequence for adding file to RAM disk image.&lt;/SPAN&gt;&lt;/P&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; rename your RAM disk image to rootfs.ext2.gz.uboot&lt;/SPAN&gt;&lt;/LI&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; sudo apt-get install u-boot-tools&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Following are the steps for adding files into rootfilesystem:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="2"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; dd if=rootfs.ext2.gz.uboot of=rootfs.ext2.gz bs=64 skip=1&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="3"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; gunzip rootfs.ext2.gz&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="4"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; mkdir /mnt/iso_1&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="5"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; sudo mount -oloop rootfs.ext2 /mnt/iso_1&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="6"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; Now, one can copy files into appropriate location under “./mnt/iso_1” directory.&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="7"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; sudo umount /mnt/iso_1&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="8"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; gzip -9 rootfs.ext2&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="9"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt;"&gt; mkimage -A ppc -O linux -T ramdisk -C gzip -n 'rootfs.ext2.gz.uboot' -d rootfs.ext2.gz rootfs.ext2.gz.uboot&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jun 2017 05:59:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677369#M4108</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-06-29T05:59:22Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677370#M4109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Pavel for your reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After step 5 , when I try to copy binaries into the location /mnt/iso_1, it says "No space left on device". How the size of mounted location can be increased to accommodate more binaries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 05:12:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677370#M4109</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2017-06-30T05:12:57Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677371#M4110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; background: white;"&gt;Check permissions for this folder. It looks like that this folder is read-only.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 05:41:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677371#M4110</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-06-30T05:41:14Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677372#M4111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Pavel,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I could copy some of the binaries(smaller in size). The problem is something related to size I doubt.&lt;/P&gt;&lt;P&gt;The error is as follows on coping binary to that folder (/mnt/iso_1)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;cp: error writing ‘/mnt/iso_1/./bcm.user’: No space left on device&lt;BR /&gt;cp: failed to extend ‘/mnt/iso_1/./bcm.user’: No space left on device&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 06:20:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677372#M4111</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2017-06-30T06:20:19Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677373#M4112</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;OL&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt; Create new empty file system using mkfs command:&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fen.wikipedia.org%2Fwiki%2FMkfs" rel="nofollow" target="_blank"&gt;https://en.wikipedia.org/wiki/Mkfs&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;and&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Flinux.die.net%2Fman%2F8%2Fmkfs" rel="nofollow" target="_blank"&gt;https://linux.die.net/man/8/mkfs&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;OL start="2"&gt;&lt;LI&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt; Copy you file system to new empty file system using command: cp -af&lt;/SPAN&gt;&lt;/LI&gt;&lt;/OL&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;See the following page:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsuperuser.com%2Fquestions%2F307541%2Fcopy-entire-file-system-hierarchy-from-one-drive-to-another" rel="nofollow" target="_blank"&gt;https://superuser.com/questions/307541/copy-entire-file-system-hierarchy-from-one-drive-to-another&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Other method:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;Change size of your file system.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;See the following pages:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Faccess.redhat.com%2Farticles%2F1196333" rel="nofollow" target="_blank"&gt;https://access.redhat.com/articles/1196333&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Faccess.redhat.com%2Fdocumentation%2Fen-US%2FRed_Hat_Enterprise_Linux%2F6%2Fhtml%2FStorage_Administration_Guide%2Fext4grow.html" rel="nofollow" target="_blank"&gt;https://access.redhat.com/documentation/en-US/Red_Hat_Enterprise_Linux/6/html/Storage_Administration_Guide/ext4grow.html&lt;/A&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jun 2017 09:33:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677373#M4112</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2017-06-30T09:33:06Z</dc:date>
    </item>
    <item>
      <title>Re: Adding a file/folder in rootfs nxp yocto build</title>
      <link>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677374#M4113</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;How to increase the size of your ramdisk -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Rename your RAM disk image to rootfs.ext2.gz.uboot and keep it under say '/home/ram/ramdisk_work'&lt;/P&gt;&lt;P&gt;2. Run 'sudo apt-get install u-boot-tools'&lt;/P&gt;&lt;P&gt;3. Run 'dd if=rootfs.ext2.gz.uboot of=rootfs.ext2.gz bs=64 skip=1'&lt;/P&gt;&lt;P&gt;4. Run 'gunzip rootfs.ext2.gz'&lt;/P&gt;&lt;P&gt;5. Run 'mkdir /mnt/iso_1'&lt;/P&gt;&lt;P&gt;6. Run 'sudo mount -o loop rootfs.ext2 /mnt/iso_1'&lt;/P&gt;&lt;P&gt;7. Now resize(increase) the size of ramdisk using the following steps -&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7.1 Run 'sudo umount /mnt/iso_1'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7.2 Run 'sudo e2fsck -f /home/ram/ramdisk_work/rootfs.ext2'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7.3 Run 'resize2fs /home/ram/ramdisk_work/rootfs.ext2 50M'&amp;nbsp; ## to increase the size to 30M from prev. smaller size&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 7.4 Run 'sudo mount -o loop rootfs.ext2 /mnt/iso_1'&lt;/P&gt;&lt;P&gt;8. Now, one can copy files into appropriate location under “/mnt/iso_1” directory. e.g.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 8.1 Run 'sudo cp -af ~/xyz.bin .'&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 8.2 Run 'sudo cp -af ~/abc.ko .'&lt;/P&gt;&lt;P&gt;9. Run 'sudo umount /mnt/iso_1'&lt;/P&gt;&lt;P&gt;10. Run 'gzip -9 rootfs.ext2'&lt;/P&gt;&lt;P&gt;11. Run 'mkimage -A ppc -O linux -T ramdisk -C gzip -n 'rootfs.ext2.gz.uboot' -d rootfs.ext2.gz rootfs.ext2.gz.uboot'&lt;/P&gt;&lt;P&gt;12. rootfs.ext2.gz.uboot thus created under '/home/ram/ramdisk_work' may be programmed on the target, that will contain the required executables.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Jul 2017 06:51:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Adding-a-file-folder-in-rootfs-nxp-yocto-build/m-p/677374#M4113</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2017-07-03T06:51:00Z</dc:date>
    </item>
  </channel>
</rss>