<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックMode configuration in eLBC for P1015</title>
    <link>https://community.nxp.com/t5/P-Series/Mode-configuration-in-eLBC-for-P1015/m-p/675867#M4098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a few queries with regard to the eLBC controller in the P1015. I have 3 devices connected to the eLBC bus which are - NOR Flash, FPGA and a NVRAM.&amp;nbsp;&amp;nbsp; The NOR Flash is the boot device and is connected to the GPCM mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.Can I connect all the three devices in the GPCM mode. Will it have any effect or will it create any problems while booting from NOR Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.Are there any limitations to connecting these three devices in the GPCM mode of the eLBC bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.What mode of operation would be better for the FPGA and NVRAM - GPCM mode or UPM mode ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How does one choose which mode needs to be used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 19 Jul 2017 11:20:35 GMT</pubDate>
    <dc:creator>pavankumarg</dc:creator>
    <dc:date>2017-07-19T11:20:35Z</dc:date>
    <item>
      <title>Mode configuration in eLBC for P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Mode-configuration-in-eLBC-for-P1015/m-p/675867#M4098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a few queries with regard to the eLBC controller in the P1015. I have 3 devices connected to the eLBC bus which are - NOR Flash, FPGA and a NVRAM.&amp;nbsp;&amp;nbsp; The NOR Flash is the boot device and is connected to the GPCM mode.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.Can I connect all the three devices in the GPCM mode. Will it have any effect or will it create any problems while booting from NOR Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.Are there any limitations to connecting these three devices in the GPCM mode of the eLBC bus.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3.What mode of operation would be better for the FPGA and NVRAM - GPCM mode or UPM mode ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How does one choose which mode needs to be used?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 11:20:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Mode-configuration-in-eLBC-for-P1015/m-p/675867#M4098</guid>
      <dc:creator>pavankumarg</dc:creator>
      <dc:date>2017-07-19T11:20:35Z</dc:date>
    </item>
    <item>
      <title>Re: Mode configuration in eLBC for P1015</title>
      <link>https://community.nxp.com/t5/P-Series/Mode-configuration-in-eLBC-for-P1015/m-p/675868#M4099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;1. Yes you can connect all devices in GPCM mode, the mode is configured per chip select line in OR/BR register pair. I do not expect any problems at boot time.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. No limitations except total input capacitance all all 3 devices must be taken into account while timing calculations.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. There is no definitive answer to this question. I recommend starting from GPCM because it is significantly simple for programming, than UPM. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 19 Jul 2017 12:05:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Mode-configuration-in-eLBC-for-P1015/m-p/675868#M4099</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2017-07-19T12:05:32Z</dc:date>
    </item>
  </channel>
</rss>