<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Error with PCI in P2041 Kernel Boot log in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674052#M4086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="288986" data-username="sameerarvikar" href="https://community.nxp.com/people/sameerarvikar"&gt;sameerarvikar&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to your boot log, it seems that you are using Linux Kernel SDK 1.9 pre-built Linux Kernel. I didn't find this problem on P2041ARDB target board.&lt;/P&gt;&lt;P&gt;Did you modify the dts file? If yes, would you please also provide it? Probably there is problem in the dts file.&lt;/P&gt;&lt;P&gt;What kind of PCIe device did you use on your target board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Jun 2017 10:13:25 GMT</pubDate>
    <dc:creator>yipingwang</dc:creator>
    <dc:date>2017-06-12T10:13:25Z</dc:date>
    <item>
      <title>Error with PCI in P2041 Kernel Boot log</title>
      <link>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674051#M4085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;When&amp;nbsp; i am booting following error comes in kernel boot log&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;BLOCKQUOTE class="jive_macro_quote jive-quote jive_text_macro"&gt;&lt;P&gt;Found FSL PCI host bridge at 0x0000000ffe201000. Firmware bus number: 0-&amp;gt;7&lt;BR /&gt;PCI host bridge /pcie@ffe201000 ranges:&lt;BR /&gt; MEM 0x0000000c20000000..0x0000000c3fffffff -&amp;gt; 0x00000000e0000000 &lt;BR /&gt; IO 0x0000000ff8010000..0x0000000ff801ffff -&amp;gt; 0x0000000000000000&lt;BR /&gt;/pcie@ffe201000: PCICSRBAR @ 0xdf000000&lt;BR /&gt;EDAC PCI0: Giving out device to module 'MPC85xx_edac' controller 'mpc85xx_pci_err': DEV 'ffe201000.pcie' (INTERRUPT)&lt;BR /&gt;&lt;STRONG&gt;genirq: Flags mismatch irq 16. 000000a0 ([EDAC] PCI err) vs. 00010000 (mpic-error-int)&lt;/STRONG&gt;&lt;BR /&gt;CPU: 0 PID: 1 Comm: swapper/0 Not tainted 3.12.37-rt51+g43cecda #25&lt;BR /&gt;&lt;STRONG&gt;Call Trace:&lt;/STRONG&gt;&lt;BR /&gt;[e9083bb0] [c0007040] show_stack+0x40/0x170 (unreliable)&lt;BR /&gt;[e9083bf0] [c068d8b4] dump_stack+0x78/0xa0&lt;BR /&gt;[e9083c00] [c007a2d4] __setup_irq+0x594/0x5b0&lt;BR /&gt;[e9083c30] [c007a45c] request_threaded_irq+0xbc/0x160&lt;BR /&gt;[e9083c60] [c007c764] devm_request_threaded_irq+0x64/0xd0&lt;BR /&gt;[e9083c90] [c04d3e64] mpc85xx_pci_err_probe+0x324/0x470&lt;BR /&gt;[e9083cf0] [c00211ec] fsl_pci_probe+0x3c/0x60&lt;BR /&gt;[e9083d00] [c02cf2ac] really_probe+0x7c/0x280&lt;BR /&gt;[e9083d20] [c02ccfcc] bus_for_each_drv+0x6c/0xc0&lt;BR /&gt;[e9083d50] [c02cf208] device_attach+0xc8/0xf0&lt;BR /&gt;[e9083d70] [c02ce454] bus_probe_device+0xa4/0xe0&lt;BR /&gt;[e9083d90] [c02cbd94] device_add+0x494/0x720&lt;BR /&gt;[e9083de0] [c051f9a8] of_platform_device_create_pdata+0x68/0xc0&lt;BR /&gt;[e9083e00] [c051fb24] of_platform_bus_create+0x114/0x1b0&lt;BR /&gt;[e9083e60] [c051fc5c] of_platform_bus_probe+0x9c/0xf0&lt;BR /&gt;[e9083e80] [c00021a8] do_one_initcall+0x158/0x1d0&lt;BR /&gt;[e9083ef0] [c086b8e8] kernel_init_freeable+0x138/0x1d0&lt;BR /&gt;[e9083f20] [c0002828] kernel_init+0x18/0x170&lt;BR /&gt;[e9083f40] [c000ff5c] ret_from_kernel_thread+0x5c/0x64&lt;BR /&gt;&lt;STRONG&gt;mpc85xx_pci_err_probe: Unable to request irq 16 for MPC85xx PCI err&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;EDAC PCI: Removed device 0 for MPC85xx_edac mpc85xx_pci_err: DEV ffe201000.pcie&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;PCI: Probing PCI hardware&lt;/STRONG&gt;&lt;BR /&gt;fsl-pci ffe201000.pcie: PCI host bridge to bus 0000:00&lt;BR /&gt;pci_bus 0000:00: root bus resource [io 0xf1040000-0xf104ffff] (bus address [0x0000-0xffff])&lt;BR /&gt;pci_bus 0000:00: root bus resource [mem 0xc20000000-0xc3fffffff] (bus address [0xe0000000-0xffffffff])&lt;BR /&gt;pci_bus 0000:00: root bus resource [bus 00-ff]&lt;BR /&gt;pci 0000:00:00.0: ignoring class 0x0b2000 (doesn't match header type 01)&lt;BR /&gt;pci 0000:00:00.0: PCI bridge to [bus 01-ff]&lt;BR /&gt;pci 0000:01:00.0: PCI bridge to [bus 02-ff]&lt;BR /&gt;pci 0000:02:01.0: PCI bridge to [bus 03-ff]&lt;BR /&gt;pci 0000:02:02.0: PCI bridge to [bus 04-ff]&lt;BR /&gt;pci 0000:04:00.0: PCI bridge to [bus 05-ff]&lt;BR /&gt;pci 0000:02:03.0: PCI bridge to [bus 06-ff]&lt;BR /&gt;pci 0000:02:04.0: PCI bridge to [bus 07-ff]&lt;BR /&gt;PCI: Cannot allocate resource region 1 of PCI bridge 2, will remap&lt;BR /&gt;&lt;STRONG&gt;PCI: Cannot allocate resource region 1 of PCI bridge 4, will remap&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;PCI: Cannot allocate resource region 1 of PCI bridge 5, will remap&lt;/STRONG&gt;&lt;BR /&gt;&lt;STRONG&gt;PCI: Cannot allocate resource region 0 of device 0000:05:00.0, will remap&lt;/STRONG&gt;&lt;BR /&gt;PCI: Cannot allocate resource region 1 of device 0000:05:00.0, will remap&lt;BR /&gt;PCI: Cannot allocate resource region 0 of device 0000:05:01.0, will remap&lt;BR /&gt;PCI: Cannot allocate resource region 1 of device 0000:05:01.0, will remap&lt;BR /&gt;PCI: Cannot allocate resource region 0 of device 0000:05:02.0, will remap&lt;BR /&gt;PCI: Cannot allocate resource region 1 of device 0000:05:02.0, will remap&lt;BR /&gt;PCI: Cannot allocate resource region 0 of device 0000:05:03.0, will remap&lt;BR /&gt;PCI: Cannot allocate resource region 1 of device 0000:05:03.0, will remap&lt;BR /&gt;pci 0000:00:00.0: BAR 9: can't assign mem pref (size 0x800000)&lt;BR /&gt;pci 0000:00:00.0: BAR 9: can't assign mem pref (size 0x800000)&lt;BR /&gt;pci 0000:01:00.0: BAR 8: assigned [mem 0xc20000000-0xc208fffff]&lt;BR /&gt;pci 0000:01:00.0: BAR 9: assigned [mem 0xc20900000-0xc210fffff 64bit pref]&lt;BR /&gt;pci 0000:01:00.0: BAR 7: assigned [io 0xf1040000-0xf1043fff]&lt;BR /&gt;pci 0000:02:01.0: BAR 8: assigned [mem 0xc20000000-0xc201fffff]&lt;BR /&gt;pci 0000:02:01.0: BAR 9: assigned [mem 0xc20900000-0xc20afffff 64bit pref]&lt;BR /&gt;pci 0000:02:02.0: BAR 8: assigned [mem 0xc20200000-0xc204fffff]&lt;BR /&gt;pci 0000:02:02.0: BAR 9: assigned [mem 0xc20b00000-0xc20cfffff 64bit pref]&lt;BR /&gt;pci 0000:02:03.0: BAR 8: assigned [mem 0xc20500000-0xc206fffff]&lt;BR /&gt;pci 0000:02:03.0: BAR 9: assigned [mem 0xc20d00000-0xc20efffff 64bit pref]&lt;BR /&gt;pci 0000:02:04.0: BAR 8: assigned [mem 0xc20700000-0xc208fffff]&lt;BR /&gt;pci 0000:02:04.0: BAR 9: assigned [mem 0xc20f00000-0xc210fffff 64bit pref]&lt;BR /&gt;pci 0000:02:01.0: BAR 7: assigned [io 0xf1040000-0xf1040fff]&lt;BR /&gt;pci 0000:02:02.0: BAR 7: assigned [io 0xf1041000-0xf1041fff]&lt;BR /&gt;pci 0000:02:03.0: BAR 7: assigned [io 0xf1042000-0xf1042fff]&lt;BR /&gt;pci 0000:02:04.0: BAR 7: assigned [io 0xf1043000-0xf1043fff]&lt;BR /&gt;pci 0000:02:01.0: PCI bridge to [bus 03]&lt;BR /&gt;pci 0000:02:01.0: bridge window [io 0xf1040000-0xf1040fff]&lt;BR /&gt;pci 0000:02:01.0: bridge window [mem 0xc20000000-0xc201fffff]&lt;BR /&gt;pci 0000:02:01.0: bridge window [mem 0xc20900000-0xc20afffff 64bit pref]&lt;BR /&gt;pci 0000:04:00.0: BAR 8: assigned [mem 0xc20200000-0xc202fffff]&lt;BR /&gt;pci 0000:05:00.0: BAR 0: assigned [mem 0xc20200000-0xc2021ffff]&lt;BR /&gt;pci 0000:05:01.0: BAR 0: assigned [mem 0xc20220000-0xc2023ffff]&lt;BR /&gt;pci 0000:05:02.0: BAR 0: assigned [mem 0xc20240000-0xc2025ffff]&lt;BR /&gt;pci 0000:05:03.0: BAR 0: assigned [mem 0xc20260000-0xc2027ffff]&lt;BR /&gt;pci 0000:05:00.0: BAR 1: assigned [mem 0xc20280000-0xc20280fff]&lt;BR /&gt;pci 0000:05:01.0: BAR 1: assigned [mem 0xc20281000-0xc20281fff]&lt;BR /&gt;pci 0000:05:02.0: BAR 1: assigned [mem 0xc20282000-0xc20282fff]&lt;BR /&gt;pci 0000:05:03.0: BAR 1: assigned [mem 0xc20283000-0xc20283fff]&lt;BR /&gt;pci 0000:04:00.0: PCI bridge to [bus 05]&lt;BR /&gt;pci 0000:04:00.0: bridge window [mem 0xc20200000-0xc202fffff]&lt;BR /&gt;pci 0000:02:02.0: PCI bridge to [bus 04-05]&lt;BR /&gt;pci 0000:02:02.0: bridge window [io 0xf1041000-0xf1041fff]&lt;BR /&gt;pci 0000:02:02.0: bridge window [mem 0xc20200000-0xc204fffff]&lt;BR /&gt;pci 0000:02:02.0: bridge window [mem 0xc20b00000-0xc20cfffff 64bit pref]&lt;BR /&gt;pci 0000:02:03.0: PCI bridge to [bus 06]&lt;BR /&gt;pci 0000:02:03.0: bridge window [io 0xf1042000-0xf1042fff]&lt;BR /&gt;pci 0000:02:03.0: bridge window [mem 0xc20500000-0xc206fffff]&lt;BR /&gt;pci 0000:02:03.0: bridge window [mem 0xc20d00000-0xc20efffff 64bit pref]&lt;BR /&gt;pci 0000:02:04.0: PCI bridge to [bus 07]&lt;BR /&gt;pci 0000:02:04.0: bridge window [io 0xf1043000-0xf1043fff]&lt;BR /&gt;pci 0000:02:04.0: bridge window [mem 0xc20700000-0xc208fffff]&lt;BR /&gt;pci 0000:02:04.0: bridge window [mem 0xc20f00000-0xc210fffff 64bit pref]&lt;BR /&gt;pci 0000:01:00.0: PCI bridge to [bus 02-07]&lt;BR /&gt;pci 0000:01:00.0: bridge window [io 0xf1040000-0xf1043fff]&lt;BR /&gt;pci 0000:01:00.0: bridge window [mem 0xc20000000-0xc208fffff]&lt;BR /&gt;pci 0000:01:00.0: bridge window [mem 0xc20900000-0xc210fffff 64bit pref]&lt;BR /&gt;pci 0000:00:00.0: PCI bridge to [bus 01-07]&lt;BR /&gt;pci 0000:00:00.0: bridge window [io 0xf1040000-0xf104ffff]&lt;BR /&gt;pci 0000:00:00.0: bridge window [mem 0xc20000000-0xc3fffffff]&lt;/P&gt;&lt;/BLOCKQUOTE&gt;&lt;P&gt;How to solve the issue,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 05 Jun 2017 12:07:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674051#M4085</guid>
      <dc:creator>sameerarvikar</dc:creator>
      <dc:date>2017-06-05T12:07:12Z</dc:date>
    </item>
    <item>
      <title>Re: Error with PCI in P2041 Kernel Boot log</title>
      <link>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674052#M4086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" class="" data-content-finding="Community" data-userid="288986" data-username="sameerarvikar" href="https://community.nxp.com/people/sameerarvikar"&gt;sameerarvikar&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to your boot log, it seems that you are using Linux Kernel SDK 1.9 pre-built Linux Kernel. I didn't find this problem on P2041ARDB target board.&lt;/P&gt;&lt;P&gt;Did you modify the dts file? If yes, would you please also provide it? Probably there is problem in the dts file.&lt;/P&gt;&lt;P&gt;What kind of PCIe device did you use on your target board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;TIC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Jun 2017 10:13:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674052#M4086</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-06-12T10:13:25Z</dc:date>
    </item>
    <item>
      <title>Re: Error with PCI in P2041 Kernel Boot log</title>
      <link>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674053#M4087</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;No i have not changed anything&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 16 Jun 2017 10:33:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Error-with-PCI-in-P2041-Kernel-Boot-log/m-p/674053#M4087</guid>
      <dc:creator>sameerarvikar</dc:creator>
      <dc:date>2017-06-16T10:33:05Z</dc:date>
    </item>
  </channel>
</rss>