<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P4080 RGMII Port don't connecting with external PHY</title>
    <link>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657440#M3959</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on what I see in the attachment, there is still&amp;nbsp; "mdio-mux-emi1 {...}"&lt;BR /&gt;node which is not correct as you state there is no MDIO multiplexing,&lt;BR /&gt;and your "phyrgmii: ethernet-phy@0 {...}" is a child of that incorrect&lt;BR /&gt;node. Remove the multiplexed MDIO node, make sure your physical &lt;BR /&gt;PHY connection is properly reflected in the Device Tree.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For details, refer to the kernel source documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Documentation/devicetree/bindings/powerpc/fsl/fman_device_tree.txt&lt;BR /&gt;Documentation/devicetree/bindings/net/mdio-mux-gpio.tx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and to SDK online documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Ffreescale.sdlproducts.com%2FLiveContent%2Fcontent%2Fen-US%2FQorIQ_SDK%2FGUID-0B8EF5A8-F420-4038-BF95-07873C136F50" rel="nofollow" target="_blank"&gt;https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-0B8EF5A8-F420-4038-BF95-07873C136F50&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Ffreescale.sdlproducts.com%2FLiveContent%2Fcontent%2Fen-US%2FQorIQ_SDK%2FGUID-09446297-AAD5-4DCB-8118-A7B36778DF11" rel="nofollow" target="_blank"&gt;https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-09446297-AAD5-4DCB-8118-A7B36778DF11&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 14 Dec 2016 13:26:50 GMT</pubDate>
    <dc:creator>bpe</dc:creator>
    <dc:date>2016-12-14T13:26:50Z</dc:date>
    <item>
      <title>P4080 RGMII Port don't connecting with external PHY</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657439#M3958</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello folks,&lt;/P&gt;&lt;P&gt;&amp;nbsp;I'm doing the board "bring up" with linux on a customized QorIQ P4080 revision 3 board. And, I'm using QorIQ SDK v2.0&lt;BR /&gt;&amp;nbsp;I'm having a hard time trying to figure it out the right configuration of the DTS in order to enable the connection between the MAC on FMAN1 dTSEC1 and an external Marvel Alaska 1GB PHY (RGMII).&amp;nbsp; When linux boots up it seems to recognize the MAC just fine.&amp;nbsp; I can set an IP and ping to it, but no packets go out nor in.&amp;nbsp; Counters on the interface, shown using 'ifconfig', remain the same all the time (ie, no traffic).&lt;/P&gt;&lt;P&gt;&amp;nbsp;Also, the led on the cards on both sides (target and host) react properly when I plug or unplg the RJ45 cable; signaling there is an L1 link established.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Any help would be very much appreciated.&lt;/P&gt;&lt;P&gt;&amp;nbsp;Details follow below:&lt;BR /&gt;&amp;nbsp;--------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;- I don't use u-boot but an old bootloader based on vxWorks ancient code.&lt;BR /&gt;&amp;nbsp;- .DTS in attachments&lt;BR /&gt;&amp;nbsp;- External PHY is:&amp;nbsp; RGMII Used as the Management Interface Marvell Alaska 88E1512, 1GB&lt;BR /&gt;&amp;nbsp;&amp;nbsp; The MAC is supposed to be connected directly to the PHY (no MUX).&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&amp;nbsp;On boot linux kernel messages:&lt;BR /&gt;&amp;nbsp;-----------------------------&lt;BR /&gt;Reserved memory: initialized node qman-pfdr, compatible id fsl,qman-pfdr&lt;BR /&gt;Reserved memory: initialized node qman-fqd, compatible id fsl,qman-fqd&lt;BR /&gt;Reserved memory: initialized node bman-fbpr, compatible id fsl,bman-fbpr&lt;BR /&gt;Reserved memory: initialized node pme-pdsr, compatible id fsl,pme-pdsr&lt;BR /&gt;Reserved memory: initialized node pme-sre, compatible id fsl,pme-sre&lt;BR /&gt;Using CoreNet Generic machine description&lt;BR /&gt;Memory CAM mapping: 256/256/256 Mb, residual: 1280Mb&lt;BR /&gt;Linux version 4.1.8-rt8+gbd51baf (&lt;A class="jive-link-email-small" href="mailto:ppolo@localhost.localdomain"&gt;ppolo@localhost.localdomain&lt;/A&gt;) (gcc version 4.9.2 (GCC) ) #34 SMP Wed Nov 23 10:58:51 IST 2016&lt;BR /&gt;Found initrd at 0xc1001000:0xc2dc85b5&lt;BR /&gt;CPU maps initialized for 1 thread per core&lt;BR /&gt;bootconsole [udbg0] enabled&lt;BR /&gt;setup_arch: initmem&lt;BR /&gt;CoreNet Generic board&lt;BR /&gt;arch: exit&lt;BR /&gt;Zone ranges:&lt;BR /&gt;&amp;nbsp; DMA&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; [mem 0x0000000000000000-0x000000002fffffff]&lt;BR /&gt;&amp;nbsp; Normal&amp;nbsp;&amp;nbsp; empty&lt;BR /&gt;&amp;nbsp; HighMem&amp;nbsp; [mem 0x0000000030000000-0x000000007fffffff]&lt;BR /&gt;Movable zone start for each node&lt;BR /&gt;Early memory node ranges&lt;BR /&gt;&amp;nbsp; node&amp;nbsp;&amp;nbsp; 0: [mem 0x0000000000000000-0x000000007fffffff]&lt;BR /&gt;Initmem setup node 0 [mem 0x0000000000000000-0x000000007fffffff]&lt;BR /&gt;MMU: Allocated 1088 bytes of context maps for 255 contexts&lt;BR /&gt;PERCPU: Embedded 12 pages/cpu @eef1f000 s19148 r8192 d21812 u49152&lt;BR /&gt;Built 1 zonelists in Zone order, mobility grouping on.&amp;nbsp; Total pages: 522752&lt;BR /&gt;Kernel command line: root=/dev/ram rw ramdisk_size=10000000 log_buf_len=128K mem=2G console=ttyS0,115200n8&lt;BR /&gt;log_buf_len: 131072 bytes&lt;BR /&gt;early log buf free: 13304(81%)&lt;BR /&gt;PID hash table entries: 4096 (order: 2, 16384 bytes)&lt;BR /&gt;Dentry cache hash table entries: 131072 (order: 7, 524288 bytes)&lt;BR /&gt;Inode-cache hash table entries: 65536 (order: 6, 262144 bytes)&lt;BR /&gt;Sorting __ex_table...&lt;BR /&gt;Memory: 1887812K/2097152K available (7316K kernel code, 356K rwdata, 2200K rodata, 312K init, 458K bss, 209340K reserved, 0K cma-reserved, 1226752K highmem)&lt;BR /&gt;Kernel virtual memory layout:&lt;BR /&gt;&amp;nbsp; * 0xfff5f000..0xfffff000&amp;nbsp; : fixmap&lt;BR /&gt;&amp;nbsp; * 0xffc00000..0xffe00000&amp;nbsp; : highmem PTEs&lt;BR /&gt;&amp;nbsp; * 0xffbfd000..0xffc00000&amp;nbsp; : early ioremap&lt;BR /&gt;&amp;nbsp; * 0xf1000000..0xffbfd000&amp;nbsp; : vmalloc &amp;amp; ioremap&lt;BR /&gt;Hierarchical RCU implementation.&lt;BR /&gt;&amp;nbsp;RCU debugfs-based tracing is enabled.&lt;BR /&gt;&amp;nbsp;Additional per-CPU info printed with stalls.&lt;BR /&gt;NR_IRQS:512 nr_irqs:512 16&lt;BR /&gt;mpic: Setting up MPIC " OpenPIC&amp;nbsp; " version 1.2 at 190040000, max 8 CPUs&lt;BR /&gt;mpic: ISU size: 512, shift: 9, mask: 1ff&lt;BR /&gt;mpic: Initializing for 512 sources&lt;BR /&gt;clocksource timebase: mask: 0xffffffffffffffff max_cycles: 0x8a60dd6a9, max_idle_ns: 440795204056 ns&lt;BR /&gt;clocksource: timebase mult[1aaaaaab] shift[24] registered&lt;BR /&gt;Console: colour dummy device 80x25&lt;BR /&gt;pid_max: default: 32768 minimum: 301&lt;BR /&gt;Mount-cache hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;Mountpoint-cache hash table entries: 2048 (order: 1, 8192 bytes)&lt;BR /&gt;e500 family performance monitor hardware support registered&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 1 to reset&lt;BR /&gt;smp: failed starting cpu 1 (rc -11)&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 2 to reset&lt;BR /&gt;smp: failed starting cpu 2 (rc -11)&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 3 to reset&lt;BR /&gt;smp: failed starting cpu 3 (rc -11)&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 4 to reset&lt;BR /&gt;smp: failed starting cpu 4 (rc -11)&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 5 to reset&lt;BR /&gt;smp: failed starting cpu 5 (rc -11)&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 6 to reset&lt;BR /&gt;smp: failed starting cpu 6 (rc -11)&lt;BR /&gt;smp: smp_85xx_start_cpu: timeout waiting for cpu 7 to reset&lt;BR /&gt;smp: failed starting cpu 7 (rc -11)&lt;BR /&gt;Brought up 1 CPUs&lt;BR /&gt;devtmpfs: initialized&lt;BR /&gt;clocksource jiffies: mask: 0xffffffff max_cycles: 0xffffffff, max_idle_ns: 7645041785100000 ns&lt;BR /&gt;NET: Registered protocol family 16&lt;BR /&gt;Bman ver:0a02,01,00&lt;BR /&gt;qman-fqd addr 0x7d800000 size 0x800000&lt;BR /&gt;qman-pfdr addr 0x7e000000 size 0x2000000&lt;BR /&gt;Qman ver:0a01,01,02,00&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;BR /&gt;PCI: Probing PCI hardware&lt;BR /&gt;vgaarb: loaded&lt;BR /&gt;SCSI subsystem initialized&lt;BR /&gt;usbcore: registered new interface driver usbfs&lt;BR /&gt;usbcore: registered new interface driver hub&lt;BR /&gt;usbcore: registered new device driver usb&lt;BR /&gt;pps_core: LinuxPPS API ver. 1 registered&lt;BR /&gt;pps_core: Software ver. 5.3.6 - Copyright 2005-2007 Rodolfo Giometti &amp;lt;&lt;A class="jive-link-email-small" href="mailto:giometti@linux.it"&gt;giometti@linux.it&lt;/A&gt;&amp;gt;&lt;BR /&gt;PTP clock support registered&lt;BR /&gt;EDAC MC: Ver: 3.0.0&lt;BR /&gt;bman-fbpr addr 0x7c000000 size 0x1000000&lt;BR /&gt;Bman err interrupt handler present&lt;BR /&gt;Bman portal (shared) initialised, cpu 0&lt;BR /&gt;Bman portal (slave) initialised, cpu 1&lt;BR /&gt;Bman portal (slave) initialised, cpu 2&lt;BR /&gt;Bman portal (slave) initialised, cpu 3&lt;BR /&gt;Bman portal (slave) initialised, cpu 4&lt;BR /&gt;Bman portal (slave) initialised, cpu 5&lt;BR /&gt;Bman portal (slave) initialised, cpu 6&lt;BR /&gt;Bman portal (slave) initialised, cpu 7&lt;BR /&gt;Bman portals initialised&lt;BR /&gt;Qman err interrupt handler present&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@4000'"&gt;'/qman-portals@194200000/qman-portal@4000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@8000'"&gt;'/qman-portals@194200000/qman-portal@8000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@c000'"&gt;'/qman-portals@194200000/qman-portal@c000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@10000'"&gt;'/qman-portals@194200000/qman-portal@10000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@14000'"&gt;'/qman-portals@194200000/qman-portal@14000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@18000'"&gt;'/qman-portals@194200000/qman-portal@18000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@20000'"&gt;'/qman-portals@194200000/qman-portal@20000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@24000'"&gt;'/qman-portals@194200000/qman-portal@24000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@1c000'"&gt;'/qman-portals@194200000/qman-portal@1c000'&lt;/A&gt; has 0x0101&lt;BR /&gt;Revision=0x0102, but portal &lt;A _jive_internal="true" class="" href="https://community.nxp.com/discussion/mailto:'/qman-portals@194200000/qman-portal@0'"&gt;'/qman-portals@194200000/qman-portal@0'&lt;/A&gt; has 0x0101&lt;BR /&gt;Qman portal (shared) initialised, cpu 0&lt;BR /&gt;Qman portal (slave) initialised, cpu 1&lt;BR /&gt;Qman portal (slave) initialised, cpu 2&lt;BR /&gt;Qman portal (slave) initialised, cpu 3&lt;BR /&gt;Qman portal (slave) initialised, cpu 4&lt;BR /&gt;Qman portal (slave) initialised, cpu 5&lt;BR /&gt;Qman portal (slave) initialised, cpu 6&lt;BR /&gt;Qman portal (slave) initialised, cpu 7&lt;BR /&gt;Qman portals initialised&lt;BR /&gt;Bman: BPID allocator includes range 32:32&lt;BR /&gt;Qman: FQID allocator includes range 256:256&lt;BR /&gt;Qman: FQID allocator includes range 32768:32768&lt;BR /&gt;Qman: CGRID allocator includes range 0:256&lt;BR /&gt;Qman: pool channel allocator includes range 33:15&lt;BR /&gt;No USDPAA memory, no 'fsl,usdpaa-mem' in device-tree&lt;BR /&gt;Switched to clocksource timebase&lt;BR /&gt;NET: Registered protocol family 2&lt;BR /&gt;TCP established hash table entries: 8192 (order: 3, 32768 bytes)&lt;BR /&gt;TCP bind hash table entries: 8192 (order: 4, 65536 bytes)&lt;BR /&gt;TCP: Hash tables configured (established 8192 bind 8192)&lt;BR /&gt;UDP hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;UDP-Lite hash table entries: 512 (order: 2, 16384 bytes)&lt;BR /&gt;NET: Registered protocol family 1&lt;BR /&gt;RPC: Registered named UNIX socket transport module.&lt;BR /&gt;RPC: Registered udp transport module.&lt;BR /&gt;RPC: Registered tcp transport module.&lt;BR /&gt;RPC: Registered tcp NFSv4.1 backchannel transport module.&lt;BR /&gt;Trying to unpack rootfs image as initramfs...&lt;BR /&gt;rootfs image is not initramfs (no cpio magic); looks like an initrd&lt;BR /&gt;Freeing initrd memory: 30492K (c1001000 - c2dc8000)&lt;BR /&gt;futex hash table entries: 2048 (order: 5, 131072 bytes)&lt;BR /&gt;audit: initializing netlink subsys (disabled)&lt;BR /&gt;audit: type=2000 audit(0.684:1): initialized&lt;BR /&gt;HugeTLB registered 4 MB page size, pre-allocated 0 pages&lt;BR /&gt;HugeTLB registered 16 MB page size, pre-allocated 0 pages&lt;BR /&gt;HugeTLB registered 64 MB page size, pre-allocated 0 pages&lt;BR /&gt;HugeTLB registered 256 MB page size, pre-allocated 0 pages&lt;BR /&gt;HugeTLB registered 1 GB page size, pre-allocated 0 pages&lt;BR /&gt;NFS: Registering the id_resolver key type&lt;BR /&gt;Key type id_resolver registered&lt;BR /&gt;Key type id_legacy registered&lt;BR /&gt;ntfs: driver 2.1.32 [Flags: R/O].&lt;BR /&gt;jffs2: version 2.2. (NAND) © 2001-2006 Red Hat, Inc.&lt;BR /&gt;bounce: pool size: 64 pages&lt;BR /&gt;io scheduler noop registered&lt;BR /&gt;io scheduler deadline registered&lt;BR /&gt;io scheduler cfq registered (default)&lt;BR /&gt;Serial: 8250/16550 driver, 4 ports, IRQ sharing enabled&lt;BR /&gt;console [ttyS0] disabled&lt;BR /&gt;serial8250.0: ttyS0 at MMIO 0x19011c500 (irq = 36, base_baud = 18750000) is a 16550A&lt;BR /&gt;console [ttyS0] enabled&lt;BR /&gt;console [ttyS0] enabled&lt;BR /&gt;bootconsole [udbg0] disabled&lt;BR /&gt;bootconsole [udbg0] disabled&lt;BR /&gt;serial8250.0: ttyS1 at MMIO 0x19011c600 (irq = 36, base_baud = 18750000) is a 16550A&lt;BR /&gt;serial8250.0: ttyS2 at MMIO 0x19011d500 (irq = 37, base_baud = 18750000) is a 16550A&lt;BR /&gt;serial8250.0: ttyS3 at MMIO 0x19011d600 (irq = 37, base_baud = 18750000) is a 16550A&lt;BR /&gt;ePAPR hypervisor byte channel driver&lt;BR /&gt;Generic non-volatile memory driver v1.1&lt;BR /&gt;brd: module loaded&lt;BR /&gt;loop: module loaded&lt;BR /&gt;st: Version 20101219, fixed bufsize 32768, s/g segs 256&lt;BR /&gt;libphy: Fixed MDIO Bus: probed&lt;BR /&gt;libphy: Freescale PowerQUICC MII Bus: probed&lt;BR /&gt;libphy: Freescale XGMAC MDIO Bus: probed&lt;BR /&gt;Freescale FM module, FMD API version 21.1.0&lt;BR /&gt;Freescale FM Ports module&lt;BR /&gt;fsl_mac: fsl_mac: FSL FMan MAC API based driver&lt;BR /&gt;fsl_mac 1904e0000.ethernet: FMan dTSEC version: 0x08240101&lt;BR /&gt;fsl_mac 1904e0000.ethernet: FMan MAC address: 00:04:9f:02:1f:bb&lt;BR /&gt;fsl_mac 1904e2000.ethernet: FMan dTSEC version: 0x08240101&lt;BR /&gt;fsl_mac 1904e2000.ethernet: FMan MAC address: 00:04:9f:02:1f:bc&lt;BR /&gt;fsl_mac 1905e0000.ethernet: FMan dTSEC version: 0x08240101&lt;BR /&gt;fsl_mac 1905e0000.ethernet: FMan MAC address: 00:04:9f:02:1f:c0&lt;BR /&gt;fsl_mac 1905e2000.ethernet: FMan dTSEC version: 0x08240101&lt;BR /&gt;fsl_mac 1905e2000.ethernet: FMan MAC address: 00:04:9f:02:1f:c1&lt;BR /&gt;fsl_mac 1905e4000.ethernet: FMan dTSEC version: 0x08240101&lt;BR /&gt;fsl_mac 1905e4000.ethernet: FMan MAC address: 00:04:9f:02:1f:c2&lt;BR /&gt;fsl_dpa: FSL DPAA Ethernet driver&lt;BR /&gt;fsl_dpa: fsl_dpa: Probed interface eth0&lt;BR /&gt;fsl_dpa: fsl_dpa: Probed interface eth1&lt;BR /&gt;fsl_advanced: FSL DPAA Advanced drivers:&lt;BR /&gt;fsl_proxy: FSL DPAA Proxy initialization driver&lt;BR /&gt;fsl_dpa_shared: FSL DPAA Shared Ethernet driver&lt;BR /&gt;fsl_dpa_macless: FSL DPAA MACless Ethernet driver&lt;BR /&gt;fsl_oh: FSL FMan Offline Parsing port driver&lt;BR /&gt;e1000: Intel(R) PRO/1000 Network Driver - version 7.3.21-k8-NAPI&lt;BR /&gt;e1000: Copyright (c) 1999-2006 Intel Corporation.&lt;BR /&gt;e1000e: Intel(R) PRO/1000 Network Driver - 2.3.2-k&lt;BR /&gt;e1000e: Copyright(c) 1999 - 2014 Intel Corporation.&lt;BR /&gt;SLIP: version 0.8.4-NET3.019-NEWTTY (dynamic channels, max=256).&lt;BR /&gt;CSLIP: code copyright 1989 Regents of the University of California.&lt;BR /&gt;ehci_hcd: USB 2.0 'Enhanced' Host Controller (EHCI) Driver&lt;BR /&gt;ehci-pci: EHCI PCI platform driver&lt;BR /&gt;ohci_hcd: USB 1.1 'Open' Host Controller (OHCI) Driver&lt;BR /&gt;ohci-pci: OHCI PCI platform driver&lt;BR /&gt;usbcore: registered new interface driver usb-storage&lt;BR /&gt;i2c /dev entries driver&lt;BR /&gt;mpc-i2c 190118000.i2c: timeout 1000000 us&lt;BR /&gt;mpc-i2c 190118100.i2c: timeout 1000000 us&lt;BR /&gt;mpc-i2c 190119000.i2c: timeout 1000000 us&lt;BR /&gt;mpc-i2c 190119100.i2c: timeout 1000000 us&lt;BR /&gt;lm90 1-004c: Register 0x4 read failed (-6)&lt;BR /&gt;lm90 1-004c: Failed to read convrate register!&lt;BR /&gt;lm90 1-004c: Register 0x3 read failed (-6)&lt;BR /&gt;lm90 1-004c: Initialization failed!&lt;BR /&gt;Freescale(R) MPC85xx EDAC driver, (C) 2006 Montavista Software&lt;BR /&gt;EDAC MC0: Giving out device to module MPC85xx_edac controller mpc85xx_mc_err: DEV mpc85xx_mc_err (INTERRUPT)&lt;BR /&gt;MPC85xx_edac acquired irq 490 for MC&lt;BR /&gt;MPC85xx_edac MC err registered&lt;BR /&gt;EDAC MC1: Giving out device to module MPC85xx_edac controller mpc85xx_mc_err: DEV mpc85xx_mc_err (INTERRUPT)&lt;BR /&gt;MPC85xx_edac acquired irq 489 for MC&lt;BR /&gt;MPC85xx_edac MC err registered&lt;BR /&gt;qoriq_cpufreq: Freescale QorIQ CPU frequency scaling driver&lt;BR /&gt;sdhci: Secure Digital Host Controller Interface driver&lt;BR /&gt;sdhci: Copyright(c) Pierre Ossman&lt;BR /&gt;sdhci-pltfm: SDHCI platform and OF driver helper&lt;BR /&gt;sdhci-esdhc 190114000.sdhc: No vmmc regulator found&lt;BR /&gt;sdhci-esdhc 190114000.sdhc: No vqmmc regulator found&lt;BR /&gt;mmc0: SDHCI controller on 190114000.sdhc [190114000.sdhc] using DMA&lt;BR /&gt;platform caam_qi.0: Linux CAAM Queue I/F driver initialised&lt;BR /&gt;caam 190300000.crypto: device ID = 0x0a10030000000000 (Era 2)&lt;BR /&gt;caam 190300000.crypto: job rings = 4, qi = 1&lt;BR /&gt;caam_jr 190301000.jr: failed to flush job ring 0&lt;BR /&gt;caam_jr: probe of 190301000.jr failed with error -5&lt;BR /&gt;caam_jr 190302000.jr: failed to flush job ring 1&lt;BR /&gt;caam_jr: probe of 190302000.jr failed with error -5&lt;BR /&gt;caam_jr 190303000.jr: failed to flush job ring 2&lt;BR /&gt;caam_jr: probe of 190303000.jr failed with error -5&lt;BR /&gt;caam_jr 190304000.jr: failed to flush job ring 3&lt;BR /&gt;caam_jr: probe of 190304000.jr failed with error -5&lt;BR /&gt;caam algorithms registered in /proc/crypto&lt;BR /&gt;platform caam_qi.0: fsl,sec-v4.0 algorithms registered in /proc/crypto&lt;BR /&gt;Job Ring Device allocation for transform failed&lt;BR /&gt;caam 190300000.crypto: fsl,sec-v4.0 algorithms registered in /proc/crypto&lt;BR /&gt;Freescale USDPAA process driver&lt;BR /&gt;fsl-usdpaa: no region found&lt;BR /&gt;Freescale USDPAA process IRQ driver&lt;BR /&gt;fsl-pme 190316000.pme: ver: 0x00100201&lt;BR /&gt;Freescale pme2 db driver&lt;BR /&gt;Freescale pme2 scan driver&lt;BR /&gt;fsl-pme2-scan: device pme_scan registered&lt;BR /&gt;Freescale hypervisor management driver&lt;BR /&gt;fsl-hv: no hypervisor found&lt;BR /&gt;ipip: IPv4 over IPv4 tunneling driver&lt;BR /&gt;Initializing XFRM netlink socket&lt;BR /&gt;NET: Registered protocol family 10&lt;BR /&gt;sit: IPv6 over IPv4 tunneling driver&lt;BR /&gt;NET: Registered protocol family 17&lt;BR /&gt;NET: Registered protocol family 15&lt;BR /&gt;Key type dns_resolver registered&lt;BR /&gt;libphy: mdio_mux: probed&lt;BR /&gt;libphy: mdio_mux: probed&lt;BR /&gt;libphy: mdio_mux: probed&lt;BR /&gt;libphy: mdio_mux: probed&lt;BR /&gt;mdio-mux-gpio mdio-mux-emi1: Version 1.0&lt;BR /&gt;libphy: mdio_mux: probed&lt;BR /&gt;libphy: mdio_mux: probed&lt;BR /&gt;mdio-mux-gpio mdio-mux-emi2: Version 1.0&lt;BR /&gt;fsl_generic: FSL DPAA Generic Ethernet driver&lt;BR /&gt;hctosys: unable to open rtc device (rtc0)&lt;BR /&gt;RAMDISK: gzip image found at block 0&lt;BR /&gt;mmc0: MAN_BKOPS_EN bit is not set&lt;BR /&gt;mmc0: new high speed MMC card at address 0001&lt;BR /&gt;mmcblk0: mmc0:0001 MMC16G 14.5 GiB &lt;BR /&gt;mmcblk0boot0: mmc0:0001 MMC16G partition 1 16.0 MiB&lt;BR /&gt;mmcblk0boot1: mmc0:0001 MMC16G partition 2 16.0 MiB&lt;BR /&gt;&amp;nbsp;mmcblk0: p1&lt;BR /&gt;VFS: Mounted root (ext2 filesystem) on device 1:0.&lt;BR /&gt;devtmpfs: mounted&lt;BR /&gt;Freeing unused kernel memory: 312K (c094e000 - c099c000)&lt;BR /&gt;INIT: version 2.88 booting&lt;BR /&gt;Starting udev&lt;BR /&gt;udevd[1041]: starting version 182&lt;BR /&gt;fsl_dpa fsl,dpaa:ethernet@0 fm1-gb0: renamed from eth0&lt;BR /&gt;fsl_dpa fsl,dpaa:ethernet@1 fm1-gb1: renamed from eth1&lt;BR /&gt;udevd[1047]: renamed network interface eth0 to fm1-gb0&lt;BR /&gt;udevd[1048]: renamed network interface eth1 to fm1-gb1&lt;BR /&gt;bootlogd: cannot allocate pseudo tty: No such file or directory&lt;BR /&gt;random: dd urandom read with 12 bits of entropy available&lt;BR /&gt;Populating dev cache&lt;BR /&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;BR /&gt;Sun Jun&amp;nbsp; 5 08:11:01 UTC 2016&lt;BR /&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;BR /&gt;Running postinst /etc/rpm-postinsts/100-sysvinit-inittab...&lt;BR /&gt;Running postinst /etc/rpm-postinsts/101-inetutils-inetd...&lt;BR /&gt;Running postinst /etc/rpm-postinsts/102-inetutils-ftpd...&lt;BR /&gt;update-rc.d: /etc/init.d/run-postinsts exists during rc.d purge (continuing)&lt;BR /&gt;&amp;nbsp;Removing any system startup links for run-postinsts ...&lt;BR /&gt;&amp;nbsp; /etc/rcS.d/S99run-postinsts&lt;BR /&gt;INIT: Entering runlevel: 5&lt;BR /&gt;Configuring network interfaces... done.&lt;BR /&gt;Starting OpenBSD Secure Shell server: sshd&lt;BR /&gt;&amp;nbsp; generating ssh RSA key...&lt;BR /&gt;&amp;nbsp; generating ssh ECDSA key...&lt;BR /&gt;&amp;nbsp; generating ssh DSA key...&lt;BR /&gt;&amp;nbsp; generating ssh ED25519 key...&lt;BR /&gt;done.&lt;BR /&gt;hwclock: can't open '/dev/misc/rtc': No such file or directory&lt;BR /&gt;Starting network benchmark server: netserver.&lt;BR /&gt;Starting system log daemon...0&lt;BR /&gt;Starting kernel log daemon...0&lt;BR /&gt;Starting internet superserver: xinetd.&lt;/P&gt;&lt;P&gt;QorIQ SDK (FSL Reference Distro) 2.0 p4080ds /dev/ttyS0&lt;/P&gt;&lt;P&gt;p4080ds login:&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# ifconfig -a&lt;BR /&gt;fm1-gb0&amp;nbsp;&amp;nbsp; Link encap:Ethernet&amp;nbsp; HWaddr 00:04:9f:02:1f:bb&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BROADCAST MULTICAST&amp;nbsp; MTU:1500&amp;nbsp; Metric:1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:1000 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:0 (0.0 B)&amp;nbsp; TX bytes:0 (0.0 B)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Memory:904e0000-904e0fff&lt;/P&gt;&lt;P&gt;fm1-gb1&amp;nbsp;&amp;nbsp; Link encap:Ethernet&amp;nbsp; HWaddr 00:04:9f:02:1f:bc&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BROADCAST MULTICAST&amp;nbsp; MTU:1500&amp;nbsp; Metric:1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:1000 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:0 (0.0 B)&amp;nbsp; TX bytes:0 (0.0 B)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Memory:904e2000-904e2fff&lt;/P&gt;&lt;P&gt;lo&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Link encap:Local Loopback&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; inet addr:127.0.0.1&amp;nbsp; Mask:255.0.0.0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; inet6 addr: ::1/128 Scope:Host&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UP LOOPBACK RUNNING&amp;nbsp; MTU:65536&amp;nbsp; Metric:1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:0 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:0 (0.0 B)&amp;nbsp; TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;sit0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Link encap:UNSPEC&amp;nbsp; HWaddr 00-00-00-00-89-40-00-00-00-00-00-00-00-00-00-00&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NOARP&amp;nbsp; MTU:1480&amp;nbsp; Metric:1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:0 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:0 (0.0 B)&amp;nbsp; TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;tunl0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Link encap:IPIP Tunnel&amp;nbsp; HWaddr&amp;nbsp;&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; NOARP&amp;nbsp; MTU:1480&amp;nbsp; Metric:1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:0 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:0 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:0 (0.0 B)&amp;nbsp; TX bytes:0 (0.0 B)&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# ifconfig fm1-gb0 10.10.10.13 netmask 255.255.255.0 up&lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# random: nonblocking pool is initialized&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# ifconfig fm1-gb0&lt;BR /&gt;fm1-gb0&amp;nbsp;&amp;nbsp; Link encap:Ethernet&amp;nbsp; HWaddr 00:04:9f:02:1f:bb&amp;nbsp; &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; inet addr:10.10.10.13&amp;nbsp; Bcast:10.10.10.255&amp;nbsp; Mask:255.255.255.0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; inet6 addr: fe80::204:9fff:fe02:1fbb/64 Scope:Link&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; UP BROADCAST MULTICAST&amp;nbsp; MTU:1500&amp;nbsp; Metric:1&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TX packets:5 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; collisions:0 txqueuelen:1000 &lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; RX bytes:0 (0.0 B)&amp;nbsp; TX bytes:418 (418.0 B)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Memory:904e0000-904e0fff&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# &lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# ping 10.10.10.13&lt;BR /&gt;PING 10.10.10.13 (10.10.10.13) 56(84) bytes of data.&lt;BR /&gt;64 bytes from 10.10.10.13: icmp_seq=1 ttl=64 time=0.097 ms&lt;BR /&gt;64 bytes from 10.10.10.13: icmp_seq=2 ttl=64 time=0.054 ms&lt;BR /&gt;^C&lt;BR /&gt;--- 10.10.10.13 ping statistics ---&lt;BR /&gt;2 packets transmitted, 2 received, 0% packet loss, time 999ms&lt;BR /&gt;rtt min/avg/max/mdev = 0.054/0.075/0.097/0.023 ms&lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# &lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# ping 10.10.10.200&lt;BR /&gt;PING 10.10.10.200 (10.10.10.200) 56(84) bytes of data.&lt;BR /&gt;From 10.10.10.13 icmp_seq=1 Destination Host Unreachable&lt;BR /&gt;From 10.10.10.13 icmp_seq=2 Destination Host Unreachable&lt;BR /&gt;From 10.10.10.13 icmp_seq=3 Destination Host Unreachable&lt;BR /&gt;^C&lt;BR /&gt;--- 10.10.10.200 ping statistics ---&lt;BR /&gt;5 packets transmitted, 0 received, +3 errors, 100% packet loss, time 4022ms&lt;BR /&gt;pipe 3&lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# route -n&lt;BR /&gt;Kernel IP routing table&lt;BR /&gt;Destination&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Gateway&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Genmask&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; Flags Metric Ref&amp;nbsp;&amp;nbsp;&amp;nbsp; Use Iface&lt;BR /&gt;10.10.10.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0.0.0.0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 255.255.255.0&amp;nbsp;&amp;nbsp; U&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 0 fm1-gb0&lt;BR /&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~#&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-email-small" href="mailto:root@p4080ds"&gt;root@p4080ds&lt;/A&gt;:~# ethtool fm1-gb0&lt;BR /&gt;Settings for fm1-gb0:&lt;BR /&gt;&amp;nbsp;Supported ports: [ MII ]&lt;BR /&gt;&amp;nbsp;Supported link modes:&amp;nbsp;&amp;nbsp; Not reported&lt;BR /&gt;&amp;nbsp;Supported pause frame use: Symmetric Receive-only&lt;BR /&gt;&amp;nbsp;Supports auto-negotiation: No&lt;BR /&gt;&amp;nbsp;Advertised link modes:&amp;nbsp; Not reported&lt;BR /&gt;&amp;nbsp;Advertised pause frame use: Symmetric Receive-only&lt;BR /&gt;&amp;nbsp;Advertised auto-negotiation: No&lt;BR /&gt;&amp;nbsp;Speed: 10Mb/s&lt;BR /&gt;&amp;nbsp;Duplex: Half&lt;BR /&gt;&amp;nbsp;Port: MII&lt;BR /&gt;&amp;nbsp;PHYAD: 0&lt;BR /&gt;&amp;nbsp;Transceiver: external&lt;BR /&gt;&amp;nbsp;Auto-negotiation: on&lt;BR /&gt;&amp;nbsp;Supports Wake-on: d&lt;BR /&gt;&amp;nbsp;Wake-on: d&lt;BR /&gt;&amp;nbsp;Current message level: 0xffffffff (-1)&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; drv probe link timer ifdown ifup rx_err tx_err tx_queued intr tx_done rx_status pktdata hw wol 0xffff8000&lt;BR /&gt;&amp;nbsp;Link detected: no&lt;/P&gt;&lt;P&gt;----------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&amp;nbsp;Many thanks in advance,&lt;/P&gt;&lt;P&gt;&amp;nbsp;-Paramahansa&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-337180"&gt;p4080_target_v8.dts.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2016 15:26:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657439#M3958</guid>
      <dc:creator>paramahansapolo</dc:creator>
      <dc:date>2016-12-07T15:26:59Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 RGMII Port don't connecting with external PHY</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657440#M3959</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Based on what I see in the attachment, there is still&amp;nbsp; "mdio-mux-emi1 {...}"&lt;BR /&gt;node which is not correct as you state there is no MDIO multiplexing,&lt;BR /&gt;and your "phyrgmii: ethernet-phy@0 {...}" is a child of that incorrect&lt;BR /&gt;node. Remove the multiplexed MDIO node, make sure your physical &lt;BR /&gt;PHY connection is properly reflected in the Device Tree.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For details, refer to the kernel source documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Documentation/devicetree/bindings/powerpc/fsl/fman_device_tree.txt&lt;BR /&gt;Documentation/devicetree/bindings/net/mdio-mux-gpio.tx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;and to SDK online documentation:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Ffreescale.sdlproducts.com%2FLiveContent%2Fcontent%2Fen-US%2FQorIQ_SDK%2FGUID-0B8EF5A8-F420-4038-BF95-07873C136F50" rel="nofollow" target="_blank"&gt;https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-0B8EF5A8-F420-4038-BF95-07873C136F50&lt;/A&gt;&lt;BR /&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Ffreescale.sdlproducts.com%2FLiveContent%2Fcontent%2Fen-US%2FQorIQ_SDK%2FGUID-09446297-AAD5-4DCB-8118-A7B36778DF11" rel="nofollow" target="_blank"&gt;https://freescale.sdlproducts.com/LiveContent/content/en-US/QorIQ_SDK/GUID-09446297-AAD5-4DCB-8118-A7B36778DF11&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Dec 2016 13:26:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657440#M3959</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-12-14T13:26:50Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 RGMII Port don't connecting with external PHY</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657441#M3960</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&amp;nbsp; Indeed, I managed to connect to the PHY by using the following in the device tree:&lt;/P&gt;&lt;P&gt;(in node&amp;nbsp;&amp;nbsp; fman0: fman@400000 )&lt;/P&gt;&lt;P&gt;mdio0: mdio@e1120 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0xe1120 0xee0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; //interrupts = &amp;lt;0x64 0x1 0x0 0x0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "fsl,fman-mdio";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #address-cells = &amp;lt;0x1&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; #size-cells = &amp;lt;0x0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phandle = &amp;lt;0x4d&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; linux,phandle = &amp;lt;0x4d&amp;gt;;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tbi0: tbi-phy@1c {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x1c&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device_type = "tbi-phy";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phandle = &amp;lt;0x18&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; linux,phandle = &amp;lt;0x18&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phy0: ethernet-phy@0 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "marvell";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; device_type = "ethernet-phy";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phandle = &amp;lt;0x19&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; linux,phandle = &amp;lt;0x19&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; };&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;fman0_rx0: port@88000 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0x88000 0x1000&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "fsl,fman-port-1g-rx";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,liodn = &amp;lt;0x2b&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cell-index = &amp;lt;0x0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phandle = &amp;lt;0x1a&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; linux,phandle = &amp;lt;0x1a&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;fman0_tx0: port@a8000 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0xa8000 0x1000&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "fsl,fman-port-1g-tx";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,qman-channel-id = &amp;lt;0x41&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cell-index = &amp;lt;0x0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phandle = &amp;lt;0x1b&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; linux,phandle = &amp;lt;0x1b&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;enet0: ethernet@e0000 {&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; reg = &amp;lt;0xe0000 0x1000&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; compatible = "fsl,fman-1g-mac";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cell-index = &amp;lt;0x0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; local-mac-address = [00 04 9f 02 1f bb];&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; tbi-handle = &amp;lt;&amp;amp;tbi0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phy-handle = &amp;lt;&amp;amp;phy0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phy-mode = "rgmii-id";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phy-connection-type = "rgmii-id";&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl,port-handles = &amp;lt;&amp;amp;fman0_rx0 &amp;amp;fman0_tx0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ptimer-handle = &amp;lt;&amp;amp;ptp_timer0&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; phandle = &amp;lt;0x4f&amp;gt;;&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; linux,phandle = &amp;lt;0x4f&amp;gt;;&lt;BR /&gt;};&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However, I needed to set "rgmii-id" for it to be able to ping. And, although, I get to ping another computer,&amp;nbsp; the board freezes after few pings, with no error messages whatsoever; just freezes, no response at all from linux.&lt;/P&gt;&lt;P&gt;I will post a new question about.&lt;/P&gt;&lt;P&gt;10x.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Dec 2016 14:34:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-RGMII-Port-don-t-connecting-with-external-PHY/m-p/657441#M3960</guid>
      <dc:creator>paramahansapolo</dc:creator>
      <dc:date>2016-12-15T14:34:15Z</dc:date>
    </item>
  </channel>
</rss>