<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックP2010 eSDHC DMA ; multiple blocks write, debe dce erros -&amp;gt; false negative?</title>
    <link>https://community.nxp.com/t5/P-Series/P2010-eSDHC-DMA-multiple-blocks-write-debe-dce-erros-gt-false/m-p/632767#M3757</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I'm using P2010 uC and I have some problem with eSDHC multiple writing. When I use multiple blocks write mode , I'm getting DEBE and DCE (alwyas both) errors in the interrupt (almost every time). However when I remove CRC check at all, then file is properly written always (we have tests to compare written and read file). Is this solution an acceptable workaround or may cause other problems? Is there any other workaround to avoid such problem? I'm using 4 bits mode and 25MHz clock. The problem occurs only while writing. Except DEBE and DCE , CC bit is set when interrupt is received&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Nov 2016 16:51:10 GMT</pubDate>
    <dc:creator>michalszlachetk</dc:creator>
    <dc:date>2016-11-29T16:51:10Z</dc:date>
    <item>
      <title>P2010 eSDHC DMA ; multiple blocks write, debe dce erros -&gt; false negative?</title>
      <link>https://community.nxp.com/t5/P-Series/P2010-eSDHC-DMA-multiple-blocks-write-debe-dce-erros-gt-false/m-p/632767#M3757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I'm using P2010 uC and I have some problem with eSDHC multiple writing. When I use multiple blocks write mode , I'm getting DEBE and DCE (alwyas both) errors in the interrupt (almost every time). However when I remove CRC check at all, then file is properly written always (we have tests to compare written and read file). Is this solution an acceptable workaround or may cause other problems? Is there any other workaround to avoid such problem? I'm using 4 bits mode and 25MHz clock. The problem occurs only while writing. Except DEBE and DCE , CC bit is set when interrupt is received&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Nov 2016 16:51:10 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2010-eSDHC-DMA-multiple-blocks-write-debe-dce-erros-gt-false/m-p/632767#M3757</guid>
      <dc:creator>michalszlachetk</dc:creator>
      <dc:date>2016-11-29T16:51:10Z</dc:date>
    </item>
    <item>
      <title>Re: P2010 eSDHC DMA ; multiple blocks write, debe dce erros -&gt; false negative?</title>
      <link>https://community.nxp.com/t5/P-Series/P2010-eSDHC-DMA-multiple-blocks-write-debe-dce-erros-gt-false/m-p/632768#M3758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;Is it detected using different SD cards?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;We can see that customers do not use CTC check if &lt;/SPAN&gt;&lt;SPAN style="font-size: 10.0pt; color: black;"&gt;eSDHC multiple writing is used.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 09 Dec 2016 16:10:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2010-eSDHC-DMA-multiple-blocks-write-debe-dce-erros-gt-false/m-p/632768#M3758</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-12-09T16:10:57Z</dc:date>
    </item>
  </channel>
</rss>