<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: TDM UMCC synchronization in transparent mode</title>
    <link>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629243#M3727</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for this example.&lt;/P&gt;&lt;P&gt;The issue is solved and the answer was in a previous release of the QEWRM (rev. 4). Unfortunately it was removed from the present release!&lt;/P&gt;&lt;P&gt;It seems that "RCVSYNC = 0xFF7E" is to be set so as to keep data aligned without using the synchronization mechanism.&lt;/P&gt;&lt;P&gt;It now works perfectly for us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sébastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 12 Dec 2016 14:05:40 GMT</pubDate>
    <dc:creator>seblol</dc:creator>
    <dc:date>2016-12-12T14:05:40Z</dc:date>
    <item>
      <title>TDM UMCC synchronization in transparent mode</title>
      <link>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629241#M3725</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We are currently writing a driver&amp;nbsp;to operate a T1040 QuiccEngine TDM link with UMCC feature.&lt;/P&gt;&lt;P&gt;This link is supposed to work in transparent mode, and we do not need to use any synchronization pattern.&lt;/P&gt;&lt;P&gt;We have first tried to deactivate the synchronization by setting CHAMR[SYNC] = 0 but the received data are shifted. This is specified in MCC 23.2.2.2 chapter of the QEIWRM. Even if related to the MCC, I suppose this restriction is also applicable to the UMCC.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="ZDSTATE_register.PNG"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/8800i303178CEC912F001/image-size/large?v=v2&amp;amp;px=999" role="button" title="ZDSTATE_register.PNG" alt="ZDSTATE_register.PNG" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;We have also tried to configure an 8-bit synchronization pattern which works fine for 8-bit time slots, but data in 16-bit time slots is always shifted, even with a 16-bit pattern.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The picture above seems to show a configuration where no pattern is used and data is not shifted (note 3) but the&amp;nbsp;RCVSYNC and ZDSTATE informations are missing...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could someone please provide us with the missing configuration?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks,&lt;/P&gt;&lt;P&gt;Sébastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Nov 2016 16:27:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629241#M3725</guid>
      <dc:creator>seblol</dc:creator>
      <dc:date>2016-11-28T16:27:40Z</dc:date>
    </item>
    <item>
      <title>Re: TDM UMCC synchronization in transparent mode</title>
      <link>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629242#M3726</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;Look at attached file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt; color: black; background: white;"&gt;It is simple program example for the MPC8560 MCC in transparent mode. Compare this example and your settings.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Dec 2016 01:24:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629242#M3726</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-12-08T01:24:23Z</dc:date>
    </item>
    <item>
      <title>Re: TDM UMCC synchronization in transparent mode</title>
      <link>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629243#M3727</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Pavel,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for this example.&lt;/P&gt;&lt;P&gt;The issue is solved and the answer was in a previous release of the QEWRM (rev. 4). Unfortunately it was removed from the present release!&lt;/P&gt;&lt;P&gt;It seems that "RCVSYNC = 0xFF7E" is to be set so as to keep data aligned without using the synchronization mechanism.&lt;/P&gt;&lt;P&gt;It now works perfectly for us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Sébastien&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 12 Dec 2016 14:05:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629243#M3727</guid>
      <dc:creator>seblol</dc:creator>
      <dc:date>2016-12-12T14:05:40Z</dc:date>
    </item>
    <item>
      <title>Re: TDM UMCC synchronization in transparent mode</title>
      <link>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629244#M3728</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for your feedback.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 13 Dec 2016 03:14:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/TDM-UMCC-synchronization-in-transparent-mode/m-p/629244#M3728</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-12-13T03:14:26Z</dc:date>
    </item>
  </channel>
</rss>