<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックSDK1.7 instalation path error</title>
    <link>https://community.nxp.com/t5/P-Series/SDK1-7-instalation-path-error/m-p/625329#M3714</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using P2020 processor, I tried the installation steps mentioned in sdk1.7 document.&lt;/P&gt;&lt;P&gt;prepared the host with required packages, when i tried the below command, the path for build environment was not creating properly. please fnd below log. build directory was not creating&lt;/P&gt;&lt;P&gt;"./poky/fsl-setup-poky -m p2020rdb -j 4 -t 2 -b ../build/p2020rdb"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Run the following commands to start a build:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-full&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-x11&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-minimal&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-flash&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-virt&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-core&lt;BR /&gt;To return to this build environment later please run:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; . /SOURCE_THIS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest if i miss any settings&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Santosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Oct 2016 07:34:30 GMT</pubDate>
    <dc:creator>santosh449</dc:creator>
    <dc:date>2016-10-12T07:34:30Z</dc:date>
    <item>
      <title>SDK1.7 instalation path error</title>
      <link>https://community.nxp.com/t5/P-Series/SDK1-7-instalation-path-error/m-p/625329#M3714</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using P2020 processor, I tried the installation steps mentioned in sdk1.7 document.&lt;/P&gt;&lt;P&gt;prepared the host with required packages, when i tried the below command, the path for build environment was not creating properly. please fnd below log. build directory was not creating&lt;/P&gt;&lt;P&gt;"./poky/fsl-setup-poky -m p2020rdb -j 4 -t 2 -b ../build/p2020rdb"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Log:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Run the following commands to start a build:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-full&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-x11&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-minimal&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-flash&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-virt&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; bitbake fsl-image-core&lt;BR /&gt;To return to this build environment later please run:&lt;BR /&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; . /SOURCE_THIS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest if i miss any settings&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Santosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Oct 2016 07:34:30 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SDK1-7-instalation-path-error/m-p/625329#M3714</guid>
      <dc:creator>santosh449</dc:creator>
      <dc:date>2016-10-12T07:34:30Z</dc:date>
    </item>
    <item>
      <title>Re: SDK1.7 instalation path error</title>
      <link>https://community.nxp.com/t5/P-Series/SDK1-7-instalation-path-error/m-p/625330#M3715</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You specified a custom build path outside the SDK installation directory.&lt;BR /&gt;That may not work as you expect. Suggestions:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. Specify the path _under_ the directory where you installed the SDK&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. The script can create a directory, but it cannot create a directory&lt;BR /&gt;&amp;nbsp;&amp;nbsp; hierarchy. For instance, if the directory &amp;lt;SDK_INST_PATH&amp;gt;/build/ &lt;BR /&gt;&amp;nbsp;&amp;nbsp; does not exist and you specify -b&amp;nbsp; build/p2020rdb, the script will &lt;BR /&gt;&amp;nbsp;&amp;nbsp; not create it for you, mkdir build/ first.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;3. Make sure you _source_ fsl_setup_poky script instead of running &lt;BR /&gt;&amp;nbsp;&amp;nbsp; it in a subshell.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 13 Oct 2016 08:25:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SDK1-7-instalation-path-error/m-p/625330#M3715</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-10-13T08:25:18Z</dc:date>
    </item>
  </channel>
</rss>