<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Can't get past SDC challenge/response using Codewarrior? in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623632#M3713</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yiping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The linked LS1 docs indicate we should set a value in the "Secure Access register", CSU_SA0. What is the equivalent register on the P1010 ? (I can't find CSU_SA0 in the P1010 reference manual).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 28 Feb 2017 11:56:36 GMT</pubDate>
    <dc:creator>ddadson</dc:creator>
    <dc:date>2017-02-28T11:56:36Z</dc:date>
    <item>
      <title>Can't get past SDC challenge/response using Codewarrior?</title>
      <link>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623630#M3711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We're making use the trusted architecture on a P1010 based platform. However, we have found we can only successfully pass the SDC challenge-response if we leave the SFP_DRVR registers unprogrammed (i.e. all zeroes). If we program it with a (suitably hamming-bit encoded value), we instead get a "secure debug violation" reported by Codewarrior (v10.5.0) when we enter the programmed value.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;We have set these fuses:&lt;BR /&gt;SFP_DPR = 0x00000001 (Conditionally closed, without notification)&lt;BR /&gt;SFP_DESSR&amp;nbsp; = 0x00000000&lt;BR /&gt;SFP_DRVR[0] = 0x04000800&lt;BR /&gt;SFP_DRVR[1] = 0x04000800&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We have checked the DRVR value vst gen_drv:&lt;BR /&gt;---&lt;BR /&gt;$./gen_drv_drbg B 0400080004000800&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;DRV[63:0] after Hamming Code is:&lt;BR /&gt;0400080004000800&lt;BR /&gt;&amp;nbsp;NAME&amp;nbsp;&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; BITS&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp;&amp;nbsp; VALUE &amp;nbsp;&lt;BR /&gt;_________|______________|____________&lt;BR /&gt;DRV 0&amp;nbsp;&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp;&amp;nbsp; 31 - 0&amp;nbsp;&amp;nbsp;&amp;nbsp; | 04000800&lt;BR /&gt;DRV 1&amp;nbsp;&amp;nbsp;&amp;nbsp; |&amp;nbsp;&amp;nbsp;&amp;nbsp; 63 - 32&amp;nbsp;&amp;nbsp; | 04000800&lt;BR /&gt;---&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there anything we might have missed when setting fuses, or some configuration for Codewarrior that might be incorrect?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Thanks,&lt;BR /&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 10 Feb 2017 16:31:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623630#M3711</guid>
      <dc:creator>ddadson</dc:creator>
      <dc:date>2017-02-10T16:31:06Z</dc:date>
    </item>
    <item>
      <title>Re: Can't get past SDC challenge/response using Codewarrior?</title>
      <link>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623631#M3712</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;A _jive_internal="true" data-content-finding="Community" data-userid="285406" data-username="ddadson" href="https://community.nxp.com/people/ddadson"&gt;David Dadson&lt;/A&gt;,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please refer to the section "3.5. Programming Debug Challenge/Response Value Register&lt;BR /&gt;(DCVR/DRVR)" and "4. Secure debugging using CodeWarrior" in this document &lt;A href="https://community.nxp.com/docs/DOC-329649"&gt;Secure Boot/Debug Configuration for LS1&lt;/A&gt; .&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 11:17:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623631#M3712</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2017-02-28T11:17:45Z</dc:date>
    </item>
    <item>
      <title>Re: Can't get past SDC challenge/response using Codewarrior?</title>
      <link>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623632#M3713</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Yiping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The linked LS1 docs indicate we should set a value in the "Secure Access register", CSU_SA0. What is the equivalent register on the P1010 ? (I can't find CSU_SA0 in the P1010 reference manual).&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks again,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Feb 2017 11:56:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Can-t-get-past-SDC-challenge-response-using-Codewarrior/m-p/623632#M3713</guid>
      <dc:creator>ddadson</dc:creator>
      <dc:date>2017-02-28T11:56:36Z</dc:date>
    </item>
  </channel>
</rss>