<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Linux SDK V1.3 problem</title>
    <link>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238095#M365</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, you're using the P2041 as an NFS client (i.e. mounting an NFS share that exists on a different machine)? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have access to a P2041, but I've tried this on a P4080 with no issue.I'm currently on SDK 2.3, but I'll try with SDK 1.3 to make sure it wasn't something fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 29 Jan 2013 21:37:15 GMT</pubDate>
    <dc:creator>genuap</dc:creator>
    <dc:date>2013-01-29T21:37:15Z</dc:date>
    <item>
      <title>Linux SDK V1.3 problem</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238094#M364</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm working with the Linux SDK V1.3 on a P2041 processor project and have hit an unexpected issue.&amp;nbsp; Using the P2041 system as a client, I mounted an NFSv3 filesystem from another server and started doing file reads and get a kernel panic 'BUG: scheduling while atomic: kworker/0:1/10/0x10000100' (note that the specified task running when the crash can differ, as I've seen 'kswapd0' and 'top' also).&amp;nbsp; I've gone back to a fairly generic SDK build (few if any modifications to kernel configuration, device tree, or drivers) and am still seeing this issue.&amp;nbsp; I've seen this issue using both the 1G and 10G MACs for server communication and have not seen any other kernel crashes using this ethernet connection before.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone else seen this type of crash and is there a known patch that might address it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you for helping with this,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MatthewH&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jan 2013 19:23:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238094#M364</guid>
      <dc:creator>matthewh</dc:creator>
      <dc:date>2013-01-25T19:23:56Z</dc:date>
    </item>
    <item>
      <title>Re: Linux SDK V1.3 problem</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238095#M365</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So, you're using the P2041 as an NFS client (i.e. mounting an NFS share that exists on a different machine)? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I don't have access to a P2041, but I've tried this on a P4080 with no issue.I'm currently on SDK 2.3, but I'll try with SDK 1.3 to make sure it wasn't something fixed.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2013 21:37:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238095#M365</guid>
      <dc:creator>genuap</dc:creator>
      <dc:date>2013-01-29T21:37:15Z</dc:date>
    </item>
    <item>
      <title>Re: Linux SDK V1.3 problem</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238096#M366</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for checking on this.&amp;nbsp; I've done some more exploring and am not sure the problem was in the NFS client.&amp;nbsp; However, I was doing high load tests on the NFS client code (and not much else) when the kernel crashes occurred.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an expected release date for SDK 2.3?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2013 02:45:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238096#M366</guid>
      <dc:creator>matthewh</dc:creator>
      <dc:date>2013-01-30T02:45:56Z</dc:date>
    </item>
    <item>
      <title>Re: Linux SDK V1.3 problem</title>
      <link>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238097#M367</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My mistake - SDK 1.3 is the latest. I keep going back and forth between the SDK's and older BSPs (before we had a unified SDK). The numbering is very different.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You can always get the latest off of the website:&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX" title="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX"&gt;http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=SDKLINUX&lt;/A&gt;&lt;/P&gt;&lt;P&gt;or off of the freescale git:&lt;/P&gt;&lt;P&gt;&lt;A href="http://git.freescale.com/git/" title="http://git.freescale.com/git/"&gt;Freescale Public GIT&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 30 Jan 2013 13:46:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Linux-SDK-V1-3-problem/m-p/238097#M367</guid>
      <dc:creator>genuap</dc:creator>
      <dc:date>2013-01-30T13:46:52Z</dc:date>
    </item>
  </channel>
</rss>