<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 SRIO for P2040 processor</title>
    <link>https://community.nxp.com/t5/P-Series/SRIO-for-P2040-processor/m-p/601920#M3578</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm referring "QorIQ P2040 Reference Manual, Rev. 4, 6/2016" for bring up SRIO for P2040 Processor.&lt;/P&gt;&lt;P&gt;On page 1255 under chapter - "Serial RapidIO Interface", there is a point that states - "RapidIO endpoint cannot be configured as four 1x or two 2x ports".&lt;/P&gt;&lt;P&gt;Does this mean we cannot use "SerDes Protocol Select" bits as 0xF, which configures for two 2x ports?&lt;/P&gt;&lt;P&gt;Do we have to use some other protocol which configures for 4x operation, if we are to use SRIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 10 Jan 2017 08:33:48 GMT</pubDate>
    <dc:creator>arunthomas</dc:creator>
    <dc:date>2017-01-10T08:33:48Z</dc:date>
    <item>
      <title>SRIO for P2040 processor</title>
      <link>https://community.nxp.com/t5/P-Series/SRIO-for-P2040-processor/m-p/601920#M3578</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm referring "QorIQ P2040 Reference Manual, Rev. 4, 6/2016" for bring up SRIO for P2040 Processor.&lt;/P&gt;&lt;P&gt;On page 1255 under chapter - "Serial RapidIO Interface", there is a point that states - "RapidIO endpoint cannot be configured as four 1x or two 2x ports".&lt;/P&gt;&lt;P&gt;Does this mean we cannot use "SerDes Protocol Select" bits as 0xF, which configures for two 2x ports?&lt;/P&gt;&lt;P&gt;Do we have to use some other protocol which configures for 4x operation, if we are to use SRIO?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regard,&lt;/P&gt;&lt;P&gt;Arun&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Jan 2017 08:33:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SRIO-for-P2040-processor/m-p/601920#M3578</guid>
      <dc:creator>arunthomas</dc:creator>
      <dc:date>2017-01-10T08:33:48Z</dc:date>
    </item>
    <item>
      <title>Re: SRIO for P2040 processor</title>
      <link>https://community.nxp.com/t5/P-Series/SRIO-for-P2040-processor/m-p/601921#M3579</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is a typo, should be written "RapidIO endpoint cannot be configured as four 1x".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Jan 2017 10:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/SRIO-for-P2040-processor/m-p/601921#M3579</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2017-01-13T10:18:33Z</dc:date>
    </item>
  </channel>
</rss>