<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic How do I update the U-Boot on P5040DS in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598265#M3557</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a P5040DS which currently has a u-boot built in 2013.&amp;nbsp; I need to update this to the U-boot binaries that are in the QorIQ 2.0 SDK.&amp;nbsp; I have tried to follow the instructions in section 4.4 of the QorIQ SDK Documentation.&amp;nbsp; I substitute substitute the fields such as &amp;lt;u-boot_start_addr&amp;gt; for the addresses listed in Table 18 (NOR Flash Memory Map) for the alternate u-boot bank (same for the RCW and FMAN Microcode).&amp;nbsp; However, when I do the pixis_reset altbank, the board just hangs.&amp;nbsp; Can anyone provide the exact steps to use here? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 30 Sep 2016 23:07:38 GMT</pubDate>
    <dc:creator>antoniogarcia</dc:creator>
    <dc:date>2016-09-30T23:07:38Z</dc:date>
    <item>
      <title>How do I update the U-Boot on P5040DS</title>
      <link>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598265#M3557</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have a P5040DS which currently has a u-boot built in 2013.&amp;nbsp; I need to update this to the U-boot binaries that are in the QorIQ 2.0 SDK.&amp;nbsp; I have tried to follow the instructions in section 4.4 of the QorIQ SDK Documentation.&amp;nbsp; I substitute substitute the fields such as &amp;lt;u-boot_start_addr&amp;gt; for the addresses listed in Table 18 (NOR Flash Memory Map) for the alternate u-boot bank (same for the RCW and FMAN Microcode).&amp;nbsp; However, when I do the pixis_reset altbank, the board just hangs.&amp;nbsp; Can anyone provide the exact steps to use here? &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Sep 2016 23:07:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598265#M3557</guid>
      <dc:creator>antoniogarcia</dc:creator>
      <dc:date>2016-09-30T23:07:38Z</dc:date>
    </item>
    <item>
      <title>Re: How do I update the U-Boot on P5040DS</title>
      <link>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598266#M3558</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; Can you share the u-boot log. I have similar issue but now it is resolved.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Ram&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 01 Dec 2016 05:01:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598266#M3558</guid>
      <dc:creator>rammurmu</dc:creator>
      <dc:date>2016-12-01T05:01:40Z</dc:date>
    </item>
    <item>
      <title>Re: How do I update the U-Boot on P5040DS</title>
      <link>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598267#M3559</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Is recommended command sequence used from the Section 4.4.10.8 of the SDK 2.0 Documentation?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Send message dump if this command sequence is used.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 07 Dec 2016 02:11:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/How-do-I-update-the-U-Boot-on-P5040DS/m-p/598267#M3559</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-12-07T02:11:21Z</dc:date>
    </item>
  </channel>
</rss>