<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P2020 eth0 ping failed</title>
    <link>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556212#M3425</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is wrong to assign IP addresses from one logical network (192.168.0.x) to 2&amp;nbsp;ethernet interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is better to use different networks, for example 192.168.0.x and 192.168.1.x for 1 interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 25 Aug 2016 02:52:02 GMT</pubDate>
    <dc:creator>b36401</dc:creator>
    <dc:date>2016-08-25T02:52:02Z</dc:date>
    <item>
      <title>P2020 eth0 ping failed</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556211#M3424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using P2020 device. After booting the Linux kernel i want to test the Ethernet&lt;/P&gt;&lt;P&gt;configured the ip address as below&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;root@p2020rdb:~# ifconfig &lt;BR /&gt;eth0 Link encap:Ethernet HWaddr 00:04:9f:02:d9:01 &lt;BR /&gt; inet addr:192.168.0.11 Bcast:192.168.0.255 Mask:255.255.255.0&lt;BR /&gt; inet6 addr: fe80::204:9fff:fe02:d901/64 Scope:Link&lt;BR /&gt; UP BROADCAST RUNNING MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:0 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:91 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:0 (0.0 B) TX bytes:10766 (10.5 KiB)&lt;BR /&gt; Base address:0x8000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;eth2 Link encap:Ethernet HWaddr 00:04:9f:02:d9:03 &lt;BR /&gt; inet addr:192.168.0.12 Bcast:192.168.0.255 Mask:255.255.255.0&lt;BR /&gt; inet6 addr: fe80::204:9fff:fe02:d903/64 Scope:Link&lt;BR /&gt; UP BROADCAST MULTICAST MTU:1500 Metric:1&lt;BR /&gt; RX packets:45 errors:0 dropped:0 overruns:0 frame:0&lt;BR /&gt; TX packets:56 errors:0 dropped:0 overruns:0 carrier:0&lt;BR /&gt; collisions:0 txqueuelen:1000 &lt;BR /&gt; RX bytes:6599 (6.4 KiB) TX bytes:7358 (7.1 KiB)&lt;BR /&gt; Base address:0xc000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I am able to ping to host ip (192.168.0.10) from eth2, but failed in case of eth0 with below message&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;root@p2020rdb:~# ping 192.168.0.10&lt;BR /&gt;PING 192.168.0.10 (192.168.0.10) 56(84) bytes of data.&lt;BR /&gt;From 192.168.0.11 icmp_seq=1 Destination Host Unreachable&lt;BR /&gt;From 192.168.0.11 icmp_seq=2 Destination Host Unreachable&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;am i missing any settings at kernel? please suggest.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Santosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Aug 2016 13:17:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556211#M3424</guid>
      <dc:creator>santosh449</dc:creator>
      <dc:date>2016-08-24T13:17:59Z</dc:date>
    </item>
    <item>
      <title>Re: P2020 eth0 ping failed</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556212#M3425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is wrong to assign IP addresses from one logical network (192.168.0.x) to 2&amp;nbsp;ethernet interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It is better to use different networks, for example 192.168.0.x and 192.168.1.x for 1 interfaces.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Victor&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 25 Aug 2016 02:52:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556212#M3425</guid>
      <dc:creator>b36401</dc:creator>
      <dc:date>2016-08-25T02:52:02Z</dc:date>
    </item>
    <item>
      <title>Re: P2020 eth0 ping failed</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556213#M3426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Victor,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I suspect one reason for the eth0 ping fail as below&lt;/P&gt;&lt;P&gt;we used the reference design of p2020RDB eval board in which eth0 is connected to vitesse switch(VSC7385), but in our board we are not using this switch.&lt;/P&gt;&lt;P&gt;Kernel and DTB are generated from sdk1.7 for p2020 devices, which may by default include the switch settings while generating images.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does any changes needed in source files to use the eth0 without switch?&lt;/P&gt;&lt;P&gt;Please help me to know where i can change in the source files to remove the&amp;nbsp;&lt;SPAN&gt;vitesse&amp;nbsp;&lt;/SPAN&gt;switch in linux kernel or DTB.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please suggest,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Santosh&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 06 Sep 2016 12:17:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556213#M3426</guid>
      <dc:creator>santosh449</dc:creator>
      <dc:date>2016-09-06T12:17:47Z</dc:date>
    </item>
    <item>
      <title>Re: P2020 eth0 ping failed</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556214#M3427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 10.0pt;"&gt;Remove switch setting in the .dtb file.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel Chubakov&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 08 Sep 2016 06:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-eth0-ping-failed/m-p/556214#M3427</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-09-08T06:02:40Z</dc:date>
    </item>
  </channel>
</rss>