<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-Series中的主题 Difference between the P5040DS and P5040RDB?</title>
    <link>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/548594#M3389</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the difference between these two boards from the software perspective?&amp;nbsp; Should anything that references the DS work on the RDB, eg. the image file QorIQ_SDK_V2.0_P5040DS_20160527_NOR_Flash.bin ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 07 Jul 2016 16:40:57 GMT</pubDate>
    <dc:creator>kenmoore</dc:creator>
    <dc:date>2016-07-07T16:40:57Z</dc:date>
    <item>
      <title>Difference between the P5040DS and P5040RDB?</title>
      <link>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/548594#M3389</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;What is the difference between these two boards from the software perspective?&amp;nbsp; Should anything that references the DS work on the RDB, eg. the image file QorIQ_SDK_V2.0_P5040DS_20160527_NOR_Flash.bin ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Jul 2016 16:40:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/548594#M3389</guid>
      <dc:creator>kenmoore</dc:creator>
      <dc:date>2016-07-07T16:40:57Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between the P5040DS and P5040RDB?</title>
      <link>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/548595#M3390</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The image file QorIQ_SDK_V2.0_P5040DS_20160527_NOR_Flash.bin will not work on the RDB. Unfortunately the SDK 2.0 does not support the P5040RDB. &lt;/P&gt;&lt;P&gt;The P5040RDB is shipped with a prebuilt u-boot/Linux image programmed in flash memory. The system includes a Linux board support package (BSP).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jul 2016 17:38:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/548595#M3390</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-07-08T17:38:47Z</dc:date>
    </item>
    <item>
      <title>Re: Difference between the P5040DS and P5040RDB?</title>
      <link>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/1848430#M5190</link>
      <description>&lt;P&gt;I have an P5040 RDB which has had its boot configuration changed and no longer boots. I believe this is limited to just the bootenv. Is there documentation about the u-boot configuration that ships with the P5040 RDB?&lt;/P&gt;</description>
      <pubDate>Tue, 16 Apr 2024 19:21:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Difference-between-the-P5040DS-and-P5040RDB/m-p/1848430#M5190</guid>
      <dc:creator>nickb537</dc:creator>
      <dc:date>2024-04-16T19:21:24Z</dc:date>
    </item>
  </channel>
</rss>