<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックP3041 PCIExpress read/write problem.</title>
    <link>https://community.nxp.com/t5/P-Series/P3041-PCIExpress-read-write-problem/m-p/530916#M3341</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; have problem with read/write memory of device wich is on PCIE bus. I have bases addresses BAR0 = 0xFFC00000, BAR2 = 0xE0000000, and&amp;nbsp; bits settings of register Command/Status (MemorySpaceEnable and I/OSpaceEnable). Inbound window set on CCSR (by default). When reading phys addresses BAR0(0xFFC00000) garbage returns. When reading write data overrides read only registers. How i can config PCIE Bus correclty?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 01 Jul 2016 09:45:57 GMT</pubDate>
    <dc:creator>dshard</dc:creator>
    <dc:date>2016-07-01T09:45:57Z</dc:date>
    <item>
      <title>P3041 PCIExpress read/write problem.</title>
      <link>https://community.nxp.com/t5/P-Series/P3041-PCIExpress-read-write-problem/m-p/530916#M3341</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I&amp;nbsp; have problem with read/write memory of device wich is on PCIE bus. I have bases addresses BAR0 = 0xFFC00000, BAR2 = 0xE0000000, and&amp;nbsp; bits settings of register Command/Status (MemorySpaceEnable and I/OSpaceEnable). Inbound window set on CCSR (by default). When reading phys addresses BAR0(0xFFC00000) garbage returns. When reading write data overrides read only registers. How i can config PCIE Bus correclty?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 01 Jul 2016 09:45:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P3041-PCIExpress-read-write-problem/m-p/530916#M3341</guid>
      <dc:creator>dshard</dc:creator>
      <dc:date>2016-07-01T09:45:57Z</dc:date>
    </item>
    <item>
      <title>Re: P3041 PCIExpress read/write problem.</title>
      <link>https://community.nxp.com/t5/P-Series/P3041-PCIExpress-read-write-problem/m-p/530917#M3342</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; I&amp;nbsp; have problem with read/write memory of device wich is on PCIE bus.&lt;/P&gt;&lt;P&gt;Is this device P3041?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If "yes" please provide:&lt;/P&gt;&lt;P&gt;1) complete PCI configuration header of the device.&lt;/P&gt;&lt;P&gt;2) binary image of the RCW being used&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 02 Jul 2016 04:58:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P3041-PCIExpress-read-write-problem/m-p/530917#M3342</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-07-02T04:58:28Z</dc:date>
    </item>
  </channel>
</rss>