<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P4080DS NOR FLASH RELATIVE ADRESSING</title>
    <link>https://community.nxp.com/t5/P-Series/P4080DS-NOR-FLASH-RELATIVE-ADRESSING/m-p/521077#M3321</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;It is impossible without hardware changing. The Flash address inputs A23–A25 are not connected to the P4080 local bus addresses A7-A5 directly on the P4080DS. The “address toggle” feature by SW7 is implemented by multistaged XOR gate which adds ngPIXIS signals defined by SW7 and P4080’s A7-A5. See details in section “Local bus” of the P4080 Development System User’s Guide. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 16 Jun 2016 10:51:22 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2016-06-16T10:51:22Z</dc:date>
    <item>
      <title>P4080DS NOR FLASH RELATIVE ADRESSING</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-NOR-FLASH-RELATIVE-ADRESSING/m-p/521076#M3320</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have question about nor flash relative adressing. For example when I want to boot p4080ds from nor flash bank 1, I need to set SW 7[0100XXXX] then load RCW and uboot. Basically I want to using direct addressing not related addressing which means when I want to&amp;nbsp; boot p4080ds from nor flash bank 1, I do not need to change SW 7 from [0000XXXX] to [0100XXXX]. Is this possible?&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jun 2016 07:01:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-NOR-FLASH-RELATIVE-ADRESSING/m-p/521076#M3320</guid>
      <dc:creator>yyurtcan</dc:creator>
      <dc:date>2016-06-15T07:01:18Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS NOR FLASH RELATIVE ADRESSING</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-NOR-FLASH-RELATIVE-ADRESSING/m-p/521077#M3321</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;&amp;nbsp; &lt;/P&gt;&lt;P&gt;It is impossible without hardware changing. The Flash address inputs A23–A25 are not connected to the P4080 local bus addresses A7-A5 directly on the P4080DS. The “address toggle” feature by SW7 is implemented by multistaged XOR gate which adds ngPIXIS signals defined by SW7 and P4080’s A7-A5. See details in section “Local bus” of the P4080 Development System User’s Guide. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Jun 2016 10:51:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-NOR-FLASH-RELATIVE-ADRESSING/m-p/521077#M3321</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-06-16T10:51:22Z</dc:date>
    </item>
  </channel>
</rss>