<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Problem with Secure Boot on P2041 in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Problem-with-Secure-Boot-on-P2041/m-p/520344#M3311</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to activate secure boot on P2041RDB.&lt;/P&gt;&lt;P&gt;I am using (rcw_14g_sben_1500mhz.bin) RCW with secure boot and boot hold enabled&lt;/P&gt;&lt;P&gt;(without ITS=1).&lt;/P&gt;&lt;P&gt;I am following procedure from SDK documentation to add SRKH on runtime during boot hold (without blowing fuses):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using CW TAP (USB)&lt;/P&gt;&lt;P&gt;Open CCS (On Ubuntu)&lt;/P&gt;&lt;P&gt;source IDcode.tcl (selected cw usb TAP)&lt;/P&gt;&lt;P&gt;# Connect to CCS and configure Config Chain&lt;/P&gt;&lt;P&gt;ccs::config_chain p2040&lt;/P&gt;&lt;P&gt;display ccs::get_config_chain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#Check Initial SNVS State and Value in SCRATCH Registers&lt;/P&gt;&lt;P&gt;ccs::display_mem 0 0xfe314014 4 0 1&lt;/P&gt;&lt;P&gt;ccs::display_mem 0 0xfe0e0200 4 0 4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#Wrie the SRK Hash Value in Mirror Registers&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e807c 4 0 &amp;lt;SRKH1&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8080 4 0 &amp;lt;SRKH2&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8084 4 0 &amp;lt;SRKH3&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8088 4 0 &amp;lt;SRKH4&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e808c 4 0 &amp;lt;SRKH5&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8090 4 0 &amp;lt;SRKH6&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8094 4 0 &amp;lt;SRKH7&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8098 4 0 &amp;lt;SRKH8&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#Get the Core Out of Boot Hold-Off&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e00e4 4 0 0x00000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is on second debug command &amp;lt;which ever it is&amp;gt; I always get (scan timeout error)&lt;/P&gt;&lt;P&gt;But If I retry again the command works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when I read SSM_ST (Security State of SEC_MON), it goes to "Non-Secure" state.&lt;/P&gt;&lt;P&gt;The cores are still in boot hold but the security state changes to Non-Secure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After releasing boot hold the ISBC gives error "SSM_CHECKSTS" (SEC_MON State Machine&lt;/P&gt;&lt;P&gt;not in CHECK state at start of ISBC) and SoC gets stuck (no output).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help you are able to provide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jun 2016 07:50:49 GMT</pubDate>
    <dc:creator>saadahmad</dc:creator>
    <dc:date>2016-06-14T07:50:49Z</dc:date>
    <item>
      <title>Problem with Secure Boot on P2041</title>
      <link>https://community.nxp.com/t5/P-Series/Problem-with-Secure-Boot-on-P2041/m-p/520344#M3311</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am trying to activate secure boot on P2041RDB.&lt;/P&gt;&lt;P&gt;I am using (rcw_14g_sben_1500mhz.bin) RCW with secure boot and boot hold enabled&lt;/P&gt;&lt;P&gt;(without ITS=1).&lt;/P&gt;&lt;P&gt;I am following procedure from SDK documentation to add SRKH on runtime during boot hold (without blowing fuses):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using CW TAP (USB)&lt;/P&gt;&lt;P&gt;Open CCS (On Ubuntu)&lt;/P&gt;&lt;P&gt;source IDcode.tcl (selected cw usb TAP)&lt;/P&gt;&lt;P&gt;# Connect to CCS and configure Config Chain&lt;/P&gt;&lt;P&gt;ccs::config_chain p2040&lt;/P&gt;&lt;P&gt;display ccs::get_config_chain&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#Check Initial SNVS State and Value in SCRATCH Registers&lt;/P&gt;&lt;P&gt;ccs::display_mem 0 0xfe314014 4 0 1&lt;/P&gt;&lt;P&gt;ccs::display_mem 0 0xfe0e0200 4 0 4&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#Wrie the SRK Hash Value in Mirror Registers&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e807c 4 0 &amp;lt;SRKH1&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8080 4 0 &amp;lt;SRKH2&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8084 4 0 &amp;lt;SRKH3&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8088 4 0 &amp;lt;SRKH4&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e808c 4 0 &amp;lt;SRKH5&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8090 4 0 &amp;lt;SRKH6&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8094 4 0 &amp;lt;SRKH7&amp;gt;&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e8098 4 0 &amp;lt;SRKH8&amp;gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#Get the Core Out of Boot Hold-Off&lt;/P&gt;&lt;P&gt;ccs::write_mem 0 0xfe0e00e4 4 0 0x00000001&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The problem is on second debug command &amp;lt;which ever it is&amp;gt; I always get (scan timeout error)&lt;/P&gt;&lt;P&gt;But If I retry again the command works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;However when I read SSM_ST (Security State of SEC_MON), it goes to "Non-Secure" state.&lt;/P&gt;&lt;P&gt;The cores are still in boot hold but the security state changes to Non-Secure.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After releasing boot hold the ISBC gives error "SSM_CHECKSTS" (SEC_MON State Machine&lt;/P&gt;&lt;P&gt;not in CHECK state at start of ISBC) and SoC gets stuck (no output).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance for any help you are able to provide.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jun 2016 07:50:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Problem-with-Secure-Boot-on-P2041/m-p/520344#M3311</guid>
      <dc:creator>saadahmad</dc:creator>
      <dc:date>2016-06-14T07:50:49Z</dc:date>
    </item>
    <item>
      <title>Re: Problem with Secure Boot on P2041</title>
      <link>https://community.nxp.com/t5/P-Series/Problem-with-Secure-Boot-on-P2041/m-p/520345#M3312</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sorry, but the information you are requesting is treated as confidential info at this time and requires a signed NDA (Non-Disclosure Agreement). Naturally, we cannot discuss this with you in public anyway, this requires to be handled as a Support Case:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-329745"&gt;How to submit a new question for NXP Support&lt;/A&gt; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;Be aware that to give you remote support through an SC, we will still need the confirmation of a Freescale employee that the NDA is in place. If you want to go this route, the next steps will be: If you have already signed a NDA agreement for this product, please contact the person who assisted you or create a SC and name us a Freescale person that can confirm this. If you have not signed an agreement, please contact your local Freescale Distributor Salesperson or FAE for assistance. For a listing of our distributors, refer to: &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Foverview.jsp%3Fcode%3DDISTRIBUTORS" rel="nofollow" target="_blank"&gt;http://www.freescale.com/webapp/sps/site/overview.jsp?code=DISTRIBUTORS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jun 2016 10:58:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Problem-with-Secure-Boot-on-P2041/m-p/520345#M3312</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-06-22T10:58:56Z</dc:date>
    </item>
  </channel>
</rss>