<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックP1011 Core1 Power</title>
    <link>https://community.nxp.com/t5/P-Series/P1011-Core1-Power/m-p/509579#M3187</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello experts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have&amp;nbsp; a P2020 board &lt;/P&gt;&lt;P&gt;to&amp;nbsp; save coset&amp;nbsp; i will plan to use P1011&amp;nbsp; with the same board&lt;/P&gt;&lt;P&gt;to test program&amp;nbsp;&amp;nbsp; i will like to&amp;nbsp; replace P2020 cpu&amp;nbsp; with P1011 cpu&lt;/P&gt;&lt;P&gt;but&amp;nbsp; the board have Core0, Core1 power Pin connected to Power&amp;nbsp; which can not be disconnected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in P1011 datasheet&amp;nbsp; those pins are "NC"&amp;nbsp; &lt;/P&gt;&lt;P&gt;i just double-check&amp;nbsp; it's&amp;nbsp; OK to connect&amp;nbsp; those pins with Power&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 09 May 2016 03:00:09 GMT</pubDate>
    <dc:creator>hyoungkikim</dc:creator>
    <dc:date>2016-05-09T03:00:09Z</dc:date>
    <item>
      <title>P1011 Core1 Power</title>
      <link>https://community.nxp.com/t5/P-Series/P1011-Core1-Power/m-p/509579#M3187</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello experts&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have&amp;nbsp; a P2020 board &lt;/P&gt;&lt;P&gt;to&amp;nbsp; save coset&amp;nbsp; i will plan to use P1011&amp;nbsp; with the same board&lt;/P&gt;&lt;P&gt;to test program&amp;nbsp;&amp;nbsp; i will like to&amp;nbsp; replace P2020 cpu&amp;nbsp; with P1011 cpu&lt;/P&gt;&lt;P&gt;but&amp;nbsp; the board have Core0, Core1 power Pin connected to Power&amp;nbsp; which can not be disconnected&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in P1011 datasheet&amp;nbsp; those pins are "NC"&amp;nbsp; &lt;/P&gt;&lt;P&gt;i just double-check&amp;nbsp; it's&amp;nbsp; OK to connect&amp;nbsp; those pins with Power&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 03:00:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1011-Core1-Power/m-p/509579#M3187</guid>
      <dc:creator>hyoungkikim</dc:creator>
      <dc:date>2016-05-09T03:00:09Z</dc:date>
    </item>
    <item>
      <title>Re: P1011 Core1 Power</title>
      <link>https://community.nxp.com/t5/P-Series/P1011-Core1-Power/m-p/509580#M3188</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, core1 power supply VDD is allowed to be connected to core0/platform power supply VDDC. The following is said in Design Checklist: "In single core devices, VDD can be connected to GND to save power, &lt;STRONG&gt;or else VDD should be connected from VDDC&lt;/STRONG&gt;"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is a direct link to P1020/P1011 design checklist (application note AN4259):&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN4259&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=" title="https://www.nxp.com/webapp/Download?colCode=AN4259&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType="&gt;https://www.nxp.com/webapp/Download?colCode=AN4259&amp;amp;location=null&amp;amp;fsrch=1&amp;amp;sr=1&amp;amp;pageNum=1&amp;amp;Parent_nodeId=&amp;amp;Parent_pageType=&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 May 2016 10:32:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1011-Core1-Power/m-p/509580#M3188</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-05-09T10:32:36Z</dc:date>
    </item>
  </channel>
</rss>