<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: 关于P4040连接仿真器的问题 in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/about-connect-to-P4040-using-USB-TAP/m-p/503847#M3119</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; can directly connected and download the CW project code using USB TAP in codewarrior environment?&lt;/P&gt;&lt;P&gt;It should be possible if the processor is connected in accordance with the Design Checklist and Hardware Specifications.&lt;/P&gt;&lt;P&gt;Please check that RESET_REQ_B is not asserted after the POR completion.&lt;/P&gt;&lt;P&gt;&amp;gt;And how to initialize the DDR memory contorller (DDR for asynchronous mode)?&lt;/P&gt;&lt;P&gt;The DDR has to be initialized by the CodeWarrior using specified initialization script.&lt;/P&gt;&lt;P&gt;For a custom board it will be needed to create new script and in this case it is possible to use the "P4040DS_init_core.tcl" as a reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 05 May 2016 17:05:33 GMT</pubDate>
    <dc:creator>ufedor</dc:creator>
    <dc:date>2016-05-05T17:05:33Z</dc:date>
    <item>
      <title>about connect to P4040 using USB TAP</title>
      <link>https://community.nxp.com/t5/P-Series/about-connect-to-P4040-using-USB-TAP/m-p/503846#M3118</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="background-color: #f2f2f2; color: #434343; font-size: 12px; font-family: Tahoma, Arial, 宋体, 'Malgun Gothic';"&gt;HI ! &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-family: HelveticaLTStd-Bold; font-size: 9pt; color: #000000;"&gt;&lt;SPAN style="color: #434343; font-family: Tahoma, Arial, 宋体, 'Malgun Gothic'; font-size: 12px; background-color: #f2f2f2;"&gt;&lt;SPAN style="color: #434343; font-family: Tahoma, Arial, 宋体, 'Malgun Gothic'; font-size: 12px; background-color: #f2f2f2;"&gt;&amp;nbsp;&amp;nbsp; I get into truble When&amp;nbsp; using P4040. I configure &lt;/SPAN&gt;P4040&amp;nbsp; &lt;SPAN style="font-family: HelveticaLTStd-Bold; font-size: 9pt; color: #000000;"&gt;&lt;STRONG&gt;cfg_rcw_src[0:4]&lt;/STRONG&gt;&lt;/SPAN&gt; to hard - code of 1_1001 model(no burning RCW), &lt;SPAN style="color: #434343; font-family: Tahoma, Arial, 宋体, 'Malgun Gothic'; font-size: 12px; background-color: #f2f2f2;"&gt; can directly connected and download the CW project code &lt;/SPAN&gt;using USB TAP&amp;nbsp; &lt;SPAN style="color: #434343; font-family: Tahoma, Arial, 宋体, 'Malgun Gothic'; font-size: 12px; background-color: #f2f2f2;"&gt;in codewarrior environment&lt;/SPAN&gt;? And how to initialize the DDR memory contorller (DDR for asynchronous mode)?&lt;/SPAN&gt;&lt;BR style="text-align: -webkit-auto;" /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 10:00:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/about-connect-to-P4040-using-USB-TAP/m-p/503846#M3118</guid>
      <dc:creator>liyj</dc:creator>
      <dc:date>2016-05-05T10:00:32Z</dc:date>
    </item>
    <item>
      <title>Re: 关于P4040连接仿真器的问题</title>
      <link>https://community.nxp.com/t5/P-Series/about-connect-to-P4040-using-USB-TAP/m-p/503847#M3119</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; can directly connected and download the CW project code using USB TAP in codewarrior environment?&lt;/P&gt;&lt;P&gt;It should be possible if the processor is connected in accordance with the Design Checklist and Hardware Specifications.&lt;/P&gt;&lt;P&gt;Please check that RESET_REQ_B is not asserted after the POR completion.&lt;/P&gt;&lt;P&gt;&amp;gt;And how to initialize the DDR memory contorller (DDR for asynchronous mode)?&lt;/P&gt;&lt;P&gt;The DDR has to be initialized by the CodeWarrior using specified initialization script.&lt;/P&gt;&lt;P&gt;For a custom board it will be needed to create new script and in this case it is possible to use the "P4040DS_init_core.tcl" as a reference.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 05 May 2016 17:05:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/about-connect-to-P4040-using-USB-TAP/m-p/503847#M3119</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-05-05T17:05:33Z</dc:date>
    </item>
  </channel>
</rss>