<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P4080 DTSEC FIFO Issue</title>
    <link>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495157#M3005</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a control/status register somewhere that might help pin down the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 23 Mar 2016 19:21:35 GMT</pubDate>
    <dc:creator>sharper</dc:creator>
    <dc:date>2016-03-23T19:21:35Z</dc:date>
    <item>
      <title>P4080 DTSEC FIFO Issue</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495156#M3004</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;After a couple of hours running SNMP traffic, the DTSEC only reports DROPPED packets.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Could this be the result of a FIFO overflow/buffer management issue?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;What steps should be taken to help diagnose the cause and/or prevent it from occurring?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;Thanks!&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 22 Mar 2016 23:23:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495156#M3004</guid>
      <dc:creator>sharper</dc:creator>
      <dc:date>2016-03-22T23:23:32Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 DTSEC FIFO Issue</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495157#M3005</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a control/status register somewhere that might help pin down the problem?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 23 Mar 2016 19:21:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495157#M3005</guid>
      <dc:creator>sharper</dc:creator>
      <dc:date>2016-03-23T19:21:35Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 DTSEC FIFO Issue</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495158#M3006</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;RDRP os a low-level conter, it increments for any dropped frame.&lt;/P&gt;&lt;P&gt;There is another counter, RODC, which counts frames dropped due to&lt;/P&gt;&lt;P&gt;no buffer condition. See DPAARM, Section 8.4.4.3.33. Note that Fman&lt;/P&gt;&lt;P&gt;can be configured to send pause frames when it detects a buffer pool&lt;/P&gt;&lt;P&gt;depletion, see Section 8.4.6.18.3. For other error types that may&lt;/P&gt;&lt;P&gt;cause frames to be dropped see Sections 8.3.7 and 8.4.6.18.&lt;/P&gt;&lt;P&gt;Registers that can help in finding the root cause of the problem&lt;/P&gt;&lt;P&gt;are FM_EPI and&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; various BMI statistic counters, see Table 8-42, offsets&lt;/P&gt;&lt;P&gt;from 0x200 and the corresponding register description.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Platon&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Mar 2016 14:22:53 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-DTSEC-FIFO-Issue/m-p/495158#M3006</guid>
      <dc:creator>bpe</dc:creator>
      <dc:date>2016-03-25T14:22:53Z</dc:date>
    </item>
  </channel>
</rss>