<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Ethernet driver combatibility</title>
    <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493776#M3000</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir&lt;/P&gt;&lt;P&gt;How to use the API Lite for creating API and how to use it&amp;nbsp; with the u-boot for the Ethernet PHY&lt;/P&gt;&lt;P&gt; Is there any document reference to use API with u-boot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Jan 2016 11:49:50 GMT</pubDate>
    <dc:creator>jagxin</dc:creator>
    <dc:date>2016-01-19T11:49:50Z</dc:date>
    <item>
      <title>Ethernet driver combatibility</title>
      <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493772#M2996</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; i am using P2041 with 2 RGMII port AND 2 SGMII ports i have configured the rcw properly ox08 is the setting i have kept In u-boot i am unable to find the VSC8572 Driver only VSC8574 is only preset can i use this ethernet driver of vitasee chip for VSC8572 or how to get the driver for the chip now if i am using mii info in u boot one of the port id is not dispalying&lt;/P&gt;&lt;P&gt;=&amp;gt; mii info&lt;/P&gt;&lt;P&gt;PHY 0x04: OUI = 0x01C1, Model = 0x0D, Rev = 0x02, 1000baseT, FDX-----used &lt;/P&gt;&lt;P&gt;PHY 0x05: OUI = 0x01C1, Model = 0x0D, Rev = 0x02,&amp;nbsp; 10baseT, HDX--------used&lt;/P&gt;&lt;P&gt;PHY 0x06: OUI = 0x01C1, Model = 0x0D, Rev = 0x02, 1000baseT, HDX-------------------not connected&lt;/P&gt;&lt;P&gt;PHY 0x07: OUI = 0x01C1, Model = 0x0D, Rev = 0x02, 1000baseT, HDX--------------------not connected&lt;/P&gt;&lt;P&gt;PHY 0x08: OUI = 0&lt;SPAN style="color: #eb7a3d;"&gt;x0000,&lt;/SPAN&gt; Model = 0x00, Rev = 0x00, 1000baseX, HDX-----------id is wrong -connected (why ids are not populated?)&lt;/P&gt;&lt;P&gt;PHY 0x09: OUI = 0x01C1, Model = 0x0D, Rev = 0x02, 1000baseT, FDX-------used&lt;/P&gt;&lt;P&gt;PHY 0x0A: OUI = 0x01C1, Model = 0x0D, Rev = 0x02, 1000baseT, HDX------not used &lt;/P&gt;&lt;P&gt;PHY 0x0B: OUI = 0x01C1, Model = 0x0D, Rev = 0x02, 1000baseT, HDX-------not used &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;now in this 0x4 ------is working i am able to ping to the test pc rgmii&lt;/P&gt;&lt;P&gt;not in this 0x5 ------is not working rgmii&lt;/P&gt;&lt;P&gt;now in this 0x8 ------is working i am able to ping to the test pc sgmii&lt;/P&gt;&lt;P&gt;not in this 0x9 ------is not working sgmii&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Jan 2016 15:17:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493772#M2996</guid>
      <dc:creator>jagxin</dc:creator>
      <dc:date>2016-01-17T15:17:06Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet driver combatibility</title>
      <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493773#M2997</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If I understand properly, VSC8574 is sgmii-only PHY, so I do not think VSC8574 driver may be used instead of VSC8572.&lt;/P&gt;&lt;P&gt;Please double-check with PHY vendor - Vitesse (www.vitesse.com)&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Jan 2016 15:14:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493773#M2997</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-01-18T15:14:58Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet driver combatibility</title>
      <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493774#M2998</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir ,&lt;/P&gt;&lt;P&gt;As per the datasheet pg 42 &lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/33636iC01FB90BEFDC7047/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;By changing the register values we can change the modes of the phy it is not an sgmii only phy and more over in one chip we are using both ports as sgmii and in other chip we are using both the ports as rgmii so it might not be an issue i think&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 03:57:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493774#M2998</guid>
      <dc:creator>jagxin</dc:creator>
      <dc:date>2016-01-19T03:57:39Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet driver combatibility</title>
      <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493775#M2999</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hi&lt;/P&gt;&lt;P&gt;We had checked with the phy vendor they are asking to use API -LITE, to create API and use it with the driver&lt;/P&gt;&lt;P&gt;regards &lt;/P&gt;&lt;P&gt;AGXIN.J&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 04:00:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493775#M2999</guid>
      <dc:creator>jagxin</dc:creator>
      <dc:date>2016-01-19T04:00:40Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet driver combatibility</title>
      <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493776#M3000</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear sir&lt;/P&gt;&lt;P&gt;How to use the API Lite for creating API and how to use it&amp;nbsp; with the u-boot for the Ethernet PHY&lt;/P&gt;&lt;P&gt; Is there any document reference to use API with u-boot&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Jan 2016 11:49:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493776#M3000</guid>
      <dc:creator>jagxin</dc:creator>
      <dc:date>2016-01-19T11:49:50Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet driver combatibility</title>
      <link>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493777#M3001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am also modifying UBOOT for our development board (both P2041 and BSC9132) to use the VSC8572 Phy and wondered if you had a solution yet?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Feb 2016 11:15:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Ethernet-driver-combatibility/m-p/493777#M3001</guid>
      <dc:creator>shermie</dc:creator>
      <dc:date>2016-02-22T11:15:58Z</dc:date>
    </item>
  </channel>
</rss>