<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P1011: Multiple PCIe Controllers and Modes?</title>
    <link>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480350#M2876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the reference to the power-up config options for the PCIe interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 18 Apr 2016 22:50:04 GMT</pubDate>
    <dc:creator>stevebelvin</dc:creator>
    <dc:date>2016-04-18T22:50:04Z</dc:date>
    <item>
      <title>P1011: Multiple PCIe Controllers and Modes?</title>
      <link>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480348#M2874</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Can the P1011 be configured to operate two separate PCI Express controllers at the same time over separate x1 connections?&amp;nbsp; If so, can these two controllers be in different device modes at the same time?&amp;nbsp; That is, can one be configured as a RC on its port while the other is an EP on its port?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 15 Mar 2016 23:36:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480348#M2874</guid>
      <dc:creator>stevebelvin</dc:creator>
      <dc:date>2016-03-15T23:36:14Z</dc:date>
    </item>
    <item>
      <title>Re: P1011: Multiple PCIe Controllers and Modes?</title>
      <link>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480349#M2875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt; can one be configured as a RC on its port while the other is an EP on its port?&lt;/P&gt;&lt;P&gt;This configuration is possible.&lt;/P&gt;&lt;P&gt;Please refer to the P1020 QorIQ Integrated Processor Reference Manual, 4.5.3.5 Host/agent configuration and 4.5.3.6 I/O port selection.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 16 Mar 2016 01:26:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480349#M2875</guid>
      <dc:creator>ufedor</dc:creator>
      <dc:date>2016-03-16T01:26:37Z</dc:date>
    </item>
    <item>
      <title>Re: P1011: Multiple PCIe Controllers and Modes?</title>
      <link>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480350#M2876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thank you for the reference to the power-up config options for the PCIe interfaces.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Apr 2016 22:50:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1011-Multiple-PCIe-Controllers-and-Modes/m-p/480350#M2876</guid>
      <dc:creator>stevebelvin</dc:creator>
      <dc:date>2016-04-18T22:50:04Z</dc:date>
    </item>
  </channel>
</rss>