<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: serdes PLL  timeout  at  P1020 POR configuration</title>
    <link>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479578#M2872</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;According to the P1020 datasheet TRIG_OUT must be pulled-up. In this case the P1020 can boot if no SerDes clock is applied to the P1020.&lt;/P&gt;&lt;P&gt;Unofficially I knew case when on a P1020/P2020 board the P1020 was installed and it was found that&lt;/P&gt;&lt;P&gt;"if cfg_srds_pll_toe = 0, pulled down, no SerDes clock input to P1020, P1020 fail to boot.&lt;/P&gt;&lt;P&gt; if cfg_srds_pll_toe = 1, pulled up, no SerDes clock input to P1020, P1020 can boot up."&lt;/P&gt;&lt;P&gt;where cfg_srds_pll_toe is on TRIG_OUT pin during the poreset in case of the P2020. But again for the P1020 this pin must be high during poreset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Apr 2016 11:41:57 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2016-04-05T11:41:57Z</dc:date>
    <item>
      <title>serdes PLL  timeout  at  P1020 POR configuration</title>
      <link>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479577#M2871</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&amp;nbsp; experts &lt;/P&gt;&lt;P&gt;i&amp;nbsp; am desiging a board&amp;nbsp; with P1020 &lt;/P&gt;&lt;P&gt;i have a question&lt;/P&gt;&lt;P&gt;in P2020&amp;nbsp; Design Checklist&amp;nbsp; ( AN4261, Page 9)&lt;/P&gt;&lt;P&gt;TRIG_OUT is used to configure&amp;nbsp; SerDes PLL clock timeout&amp;nbsp; to prevent boot-up hang-out&lt;/P&gt;&lt;P&gt;but P1020 Design Checklist&amp;nbsp; , there is no commnet about SerDes PLL clock timeout&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;in P1020&amp;nbsp;&amp;nbsp; if SerDes clock isn't used&amp;nbsp;&amp;nbsp; SerDes PLL clock timeout&amp;nbsp; happen&amp;nbsp; so there is no boot-up hang-out&lt;/P&gt;&lt;P&gt;or do i have to set POR-configruation pin&amp;nbsp; &lt;/P&gt;&lt;P&gt;i can't find&amp;nbsp; any infomation&amp;nbsp;&amp;nbsp; if i miss some thing&amp;nbsp; please advice me&lt;/P&gt;&lt;P&gt;thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 02:24:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479577#M2871</guid>
      <dc:creator>hyoungkikim</dc:creator>
      <dc:date>2016-04-05T02:24:56Z</dc:date>
    </item>
    <item>
      <title>Re: serdes PLL  timeout  at  P1020 POR configuration</title>
      <link>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479578#M2872</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;According to the P1020 datasheet TRIG_OUT must be pulled-up. In this case the P1020 can boot if no SerDes clock is applied to the P1020.&lt;/P&gt;&lt;P&gt;Unofficially I knew case when on a P1020/P2020 board the P1020 was installed and it was found that&lt;/P&gt;&lt;P&gt;"if cfg_srds_pll_toe = 0, pulled down, no SerDes clock input to P1020, P1020 fail to boot.&lt;/P&gt;&lt;P&gt; if cfg_srds_pll_toe = 1, pulled up, no SerDes clock input to P1020, P1020 can boot up."&lt;/P&gt;&lt;P&gt;where cfg_srds_pll_toe is on TRIG_OUT pin during the poreset in case of the P2020. But again for the P1020 this pin must be high during poreset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Apr 2016 11:41:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479578#M2872</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-04-05T11:41:57Z</dc:date>
    </item>
    <item>
      <title>Re: serdes PLL  timeout  at  P1020 POR configuration</title>
      <link>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479579#M2873</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;thank you &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Apr 2016 02:25:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/serdes-PLL-timeout-at-P1020-POR-configuration/m-p/479579#M2873</guid>
      <dc:creator>hyoungkikim</dc:creator>
      <dc:date>2016-04-06T02:25:35Z</dc:date>
    </item>
  </channel>
</rss>