<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Model selector in P3041 ibis model in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476748#M2846</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this valid for all models in the ibis file which have the model selector based on slew rate ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 13 Jan 2016 08:46:26 GMT</pubDate>
    <dc:creator>petervuylsteke</dc:creator>
    <dc:date>2016-01-13T08:46:26Z</dc:date>
    <item>
      <title>Model selector in P3041 ibis model</title>
      <link>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476746#M2844</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi. In the ibis model of the P3041, a model selector 'bvdd_io' is used on e.g. the local bus signals. With the 'bvdd_io' model selector you can select 1 of 4 models going from&amp;nbsp; "3.3V I/O slowest slew rate" to " 3.3V I/O fastest slew rate"&amp;nbsp; All four models than have their 'minimum' 'typical' and 'maximum' simulation cases according the ibis specification.&amp;nbsp; As I don't see any setting to change drive strengths on the local bus, what is the relation between the slew rate model selector and the corner cases min-typ-max of the ibis file.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 Jan 2016 13:31:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476746#M2844</guid>
      <dc:creator>petervuylsteke</dc:creator>
      <dc:date>2016-01-08T13:31:34Z</dc:date>
    </item>
    <item>
      <title>Re: Model selector in P3041 ibis model</title>
      <link>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476747#M2845</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry for delayed response&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The output buffer has several options by design, but not all these options are available for user.&lt;/P&gt;&lt;P&gt;The only one option is available (permanently selected)&lt;/P&gt;&lt;P&gt;Please use option "01" - slow slew rate&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Alexander&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 12 Jan 2016 17:10:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476747#M2845</guid>
      <dc:creator>alexander_yakov</dc:creator>
      <dc:date>2016-01-12T17:10:51Z</dc:date>
    </item>
    <item>
      <title>Re: Model selector in P3041 ibis model</title>
      <link>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476748#M2846</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for your answer.&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this valid for all models in the ibis file which have the model selector based on slew rate ? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Peter&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Jan 2016 08:46:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Model-selector-in-P3041-ibis-model/m-p/476748#M2846</guid>
      <dc:creator>petervuylsteke</dc:creator>
      <dc:date>2016-01-13T08:46:26Z</dc:date>
    </item>
  </channel>
</rss>