<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: Unused eSDHC Interface Pin Recommendations in P1022 Processor</title>
    <link>https://community.nxp.com/t5/P-Series/Unused-eSDHC-Interface-Pin-Recommendations-in-P1022-Processor/m-p/468667#M2769</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If pins are configured as SDHC, tie to inactive state through 10–100k&lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;pull-up resistors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;It is common practice. To ensure reliable operation, it is highly recommended to connect unused inputs to an appropriate signal level.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 28 Jan 2016 05:32:31 GMT</pubDate>
    <dc:creator>Pavel</dc:creator>
    <dc:date>2016-01-28T05:32:31Z</dc:date>
    <item>
      <title>Unused eSDHC Interface Pin Recommendations in P1022 Processor</title>
      <link>https://community.nxp.com/t5/P-Series/Unused-eSDHC-Interface-Pin-Recommendations-in-P1022-Processor/m-p/468666#M2768</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is specified in P1022 design checklist that if eSDHC interface is not used SDHC_DAT0/GPIO1_[25], SDHC_DAT[1:2], SDHC_DAT3 should be configured as GPIO Output, leave floating. But SDHC_DAT[1:2] pins cannot be configured as GPIO output. What should be recommendation for unused SDHC_DAT[1:2] pins?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 27 Jan 2016 10:19:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unused-eSDHC-Interface-Pin-Recommendations-in-P1022-Processor/m-p/468666#M2768</guid>
      <dc:creator>prasantahalder</dc:creator>
      <dc:date>2016-01-27T10:19:37Z</dc:date>
    </item>
    <item>
      <title>Re: Unused eSDHC Interface Pin Recommendations in P1022 Processor</title>
      <link>https://community.nxp.com/t5/P-Series/Unused-eSDHC-Interface-Pin-Recommendations-in-P1022-Processor/m-p/468667#M2769</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;If pins are configured as SDHC, tie to inactive state through 10–100k&lt;/SPAN&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;pull-up resistors.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN lang="EN-US" style="font-size: 10.0pt;"&gt;It is common practice. To ensure reliable operation, it is highly recommended to connect unused inputs to an appropriate signal level.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 28 Jan 2016 05:32:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/Unused-eSDHC-Interface-Pin-Recommendations-in-P1022-Processor/m-p/468667#M2769</guid>
      <dc:creator>Pavel</dc:creator>
      <dc:date>2016-01-28T05:32:31Z</dc:date>
    </item>
  </channel>
</rss>