<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: P4080DS  System Clock Speed in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467680#M2760</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The eLBC clock is derived from the platform clock (can be 1/8, 1/16, 1/32). So because you already has maximum of the platform clock frequency you cannot increase eLBC clok by sysclock frequency increasing.&lt;/P&gt;&lt;P&gt;The LCRR register (LCRR[CLKDIV]) controls eLBC clock:&lt;/P&gt;&lt;P&gt;“CLKDIV&amp;nbsp; Clock divider. Sets the frequency ratio between the platform clock and the local bus clock. Only the values shown below are allowed. Note that the reset value of CLKDIV depends on the RCW source configuration(cfg_rcw_src[0:4]).&lt;/P&gt;&lt;P&gt;00000-00001 Reserved&lt;/P&gt;&lt;P&gt;00010 8&lt;/P&gt;&lt;P&gt;00011 Reserved&lt;/P&gt;&lt;P&gt;00100 16&lt;/P&gt;&lt;P&gt;00101-00111 Reserved&lt;/P&gt;&lt;P&gt;01000 32&lt;/P&gt;&lt;P&gt;01001-11111 Reserved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: It is critical that no transactions are being executed via the local bus while CLKDIV is being modified. As such, prior to modification, the user must ensure that code is not executing out of the &lt;/P&gt;&lt;P&gt;local bus. Once LCRR[CLKDIV] is written, the register should be read, and then an isync should be executed.”&lt;/P&gt;&lt;P&gt;Take into account that the specifications limit eLBC clock to 100 MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Jun 2016 12:56:12 GMT</pubDate>
    <dc:creator>r8070z</dc:creator>
    <dc:date>2016-06-02T12:56:12Z</dc:date>
    <item>
      <title>P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467677#M2757</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;I want to change the system clock speed. However, to do that I need to change SW3 6-8 bits(Default 100). When I change from 100 to 110 which is 125 MHz, the system could not boot. Please find the output in the attachment.&lt;/P&gt;&lt;P&gt;Then I have tried all combination, the result is that I can cont increase system clock more than 100MHz.However I can decrease to 75 MHz. So why does system clock speed inrease? How can I increase that? &lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 10:55:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467677#M2757</guid>
      <dc:creator>yaseryurtcan</dc:creator>
      <dc:date>2016-06-01T10:55:41Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467678#M2758</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;According to the P4080 QorIQ Integrated Processor Hardware Specifications, for the fastest P4080 device max CPU frequency is 1500 MHz, max CCB frequency is 800 MHz, max DDR clock frequency is 667 MHz. As I can see for the Reset Configuration Word (RCW) which you used these values is achieved at sysclock frequency = 100 MHz. I.e. when you simply increase sysclock to 125 MHz you violate the P4080 specifications. If you want to use 125 MHz then you should change the RCW fields which define CPU, CCB and DDR frequencies in way which satisfies the P4080 specifications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 01 Jun 2016 17:40:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467678#M2758</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-06-01T17:40:46Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467679#M2759</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;As far as I understoond, I need to change CPU,CBU and DDR max clock frequency vaules in RCW in order to meet system requirement when I change SYSCLK from 100 MHz to 125 MHz. I have checked RCW but I could not find where to change in RCW (I have not deep knowledge about RCW). One last question, I want to increase SYSCLK to achieve the higher ELBC frequency so that NOR FLASH read access time will decrease. Is this a good way? Does this violate other the system operation?&lt;/P&gt;&lt;P&gt;Best regards. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 07:05:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467679#M2759</guid>
      <dc:creator>yaseryurtcan</dc:creator>
      <dc:date>2016-06-02T07:05:50Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467680#M2760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The eLBC clock is derived from the platform clock (can be 1/8, 1/16, 1/32). So because you already has maximum of the platform clock frequency you cannot increase eLBC clok by sysclock frequency increasing.&lt;/P&gt;&lt;P&gt;The LCRR register (LCRR[CLKDIV]) controls eLBC clock:&lt;/P&gt;&lt;P&gt;“CLKDIV&amp;nbsp; Clock divider. Sets the frequency ratio between the platform clock and the local bus clock. Only the values shown below are allowed. Note that the reset value of CLKDIV depends on the RCW source configuration(cfg_rcw_src[0:4]).&lt;/P&gt;&lt;P&gt;00000-00001 Reserved&lt;/P&gt;&lt;P&gt;00010 8&lt;/P&gt;&lt;P&gt;00011 Reserved&lt;/P&gt;&lt;P&gt;00100 16&lt;/P&gt;&lt;P&gt;00101-00111 Reserved&lt;/P&gt;&lt;P&gt;01000 32&lt;/P&gt;&lt;P&gt;01001-11111 Reserved&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;NOTE: It is critical that no transactions are being executed via the local bus while CLKDIV is being modified. As such, prior to modification, the user must ensure that code is not executing out of the &lt;/P&gt;&lt;P&gt;local bus. Once LCRR[CLKDIV] is written, the register should be read, and then an isync should be executed.”&lt;/P&gt;&lt;P&gt;Take into account that the specifications limit eLBC clock to 100 MHz.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 12:56:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467680#M2760</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-06-02T12:56:12Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467681#M2761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;To make sure that as you stated increasing system clock does not increase elbc clock which is &lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;derived from the platform clock. Is this right? (But I can increase CPU, CCB and DDR clock by increasing system clock). As far as I know system clock determine platform clock which is determine elbc clock. So, My knowledge would be wrong now. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Second question I want to reduce&amp;nbsp; read access time to NOR FLASH so that decrease boot time. Is there any other way for that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Best regards.&lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Jun 2016 16:53:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467681#M2761</guid>
      <dc:creator>yaseryurtcan</dc:creator>
      <dc:date>2016-06-02T16:53:13Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467682#M2762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&amp;gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;Is this right? &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;No I wrote that you already has maximum of the platform clock frequency you cannot increase eLBC clok by sysclock frequency increasing. I.e. at sysclock=100MHz you ypu already got the platform clock maximal.&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&amp;gt;But I can increase CPU, CCB and DDR clock by increasing system clock&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;You over clocked device, it may operate incorrectly (as you could see) or even can be damaged due to extra power consumption.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&amp;gt;Second question I want to reduce&amp;nbsp; read access time to NOR FLASH so that decrease boot time. &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, helvetica, 'helvetica neue', verdana, sans-serif;"&gt;&amp;gt;Is there any other way for that?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;I do not see simple way. Check your bootlader, if it first load small piece code&amp;nbsp; to the memory which than re-programs the eLBC NOR bank to load the rest with maximal possible rate. Or use the PBL to configure the eLBC NOR bank to the maximal possible read rate.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 03 Jun 2016 09:19:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467682#M2762</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2016-06-03T09:19:19Z</dc:date>
    </item>
    <item>
      <title>Re: P4080DS  System Clock Speed</title>
      <link>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467683#M2763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;After you stated that I need to change RCW&amp;nbsp; values in order to achieve higher frequency of CPU, CCB, DDR, and Elbc bus, I want to keep other RCW values and SYSCLK the same and change CPU clock frequency by changing RCW[CC1_PLL_RAT] either from 01111(which is 15:1, 1,5 GHz) to 10000 (which is 16:1, 1,6 GHz) or from 01111(which is 15:1, 1,5 GHz) to 01100 (which is 12:1, 1,2 GHz). In both cases, the demo board could not boot. Why is the reason for that? Basically I want to keep CPU, and CCB clock frequency the same, but increase DDR clock frequency to 1300 MHz and ELBC to 133 MHz. To do that what are the steps that I should follow? I think that I need to change SYSCLK and RCW(I don’t know which part I change in RCW. Could you provide new RCW for that?).&lt;/P&gt;&lt;P&gt;Best regards. &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 06 Jun 2016 08:37:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080DS-System-Clock-Speed/m-p/467683#M2763</guid>
      <dc:creator>yyurtcan</dc:creator>
      <dc:date>2016-06-06T08:37:47Z</dc:date>
    </item>
  </channel>
</rss>