<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P2020 QorIQ enabling the second core</title>
    <link>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445036#M2594</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene Abramsky,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the question "How should I define the TLB for the second core?"&lt;/P&gt;&lt;P&gt;All TLB&amp;nbsp; mapping is created in kernel and driver, not defined as u-boot, users don't need to care more about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 14 May 2015 03:14:01 GMT</pubDate>
    <dc:creator>lunminliang</dc:creator>
    <dc:date>2015-05-14T03:14:01Z</dc:date>
    <item>
      <title>P2020 QorIQ enabling the second core</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445034#M2592</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/336646"&gt;P2020 QorIQ eTSEC multiple TxBD rings&lt;/A&gt;Hi,&lt;/P&gt;&lt;P&gt;I am working on P2020 QoriIQ.&lt;/P&gt;&lt;P&gt;The system starts on core #0 while the core #1 is turned off.&lt;/P&gt;&lt;P&gt;When I start the second core, it gets Instruction Access Exception.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there any steps I should make before enabling the second core?&lt;/P&gt;&lt;P&gt;How should I define the TLB for the second core?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for help :smileyhappy:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 26 Apr 2015 08:29:02 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445034#M2592</guid>
      <dc:creator>transporter</dc:creator>
      <dc:date>2015-04-26T08:29:02Z</dc:date>
    </item>
    <item>
      <title>Re: P2020 QorIQ enabling the second core</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445035#M2593</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eugene Abramsky,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Assume you are using U-Boot? What's value of register BPTR? When second core start, is boot code ready? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flow in U-Boot:&lt;/P&gt;&lt;P&gt;1. Prepare boot code in memory;&lt;/P&gt;&lt;P&gt;2. Write BPTR register to setup boot page;&lt;/P&gt;&lt;P&gt;3. Release the second core.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 08 May 2015 07:28:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445035#M2593</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-05-08T07:28:46Z</dc:date>
    </item>
    <item>
      <title>Re: P2020 QorIQ enabling the second core</title>
      <link>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445036#M2594</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Eugene Abramsky,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For the question "How should I define the TLB for the second core?"&lt;/P&gt;&lt;P&gt;All TLB&amp;nbsp; mapping is created in kernel and driver, not defined as u-boot, users don't need to care more about it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Lunmin&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 14 May 2015 03:14:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020-QorIQ-enabling-the-second-core/m-p/445036#M2594</guid>
      <dc:creator>lunminliang</dc:creator>
      <dc:date>2015-05-14T03:14:01Z</dc:date>
    </item>
  </channel>
</rss>