<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic P4080 NAND support in P-Series</title>
    <link>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230042#M257</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am just looking into a P4080 design and would like to use a 2GByte SLC NAND for booting and storage.&amp;nbsp; The device that I am considering is&lt;/P&gt;&lt;P&gt;the MT29F16G08ABA device (x8 data bus with page size 4096 + 224).&amp;nbsp;&amp;nbsp; The page size looks larger than what the manual states (2048) so I&lt;/P&gt;&lt;P&gt;am wondering if such a device is supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 18 Jan 2013 16:27:13 GMT</pubDate>
    <dc:creator>dickginther</dc:creator>
    <dc:date>2013-01-18T16:27:13Z</dc:date>
    <item>
      <title>P4080 NAND support</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230042#M257</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I am just looking into a P4080 design and would like to use a 2GByte SLC NAND for booting and storage.&amp;nbsp; The device that I am considering is&lt;/P&gt;&lt;P&gt;the MT29F16G08ABA device (x8 data bus with page size 4096 + 224).&amp;nbsp;&amp;nbsp; The page size looks larger than what the manual states (2048) so I&lt;/P&gt;&lt;P&gt;am wondering if such a device is supported.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2013 16:27:13 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230042#M257</guid>
      <dc:creator>dickginther</dc:creator>
      <dc:date>2013-01-18T16:27:13Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 NAND support</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230043#M258</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is not supported.&amp;nbsp; There has been some effort towards a use-at-your-own-risk hack to make it work -- see &lt;A href="http://patchwork.ozlabs.org/patch/168855/" title="http://patchwork.ozlabs.org/patch/168855/"&gt;[U-Boot,v4] nand: Hack to support 4k page in fsl_elbc_nand - Patchwork.&lt;BR /&gt;&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;That patch has not yet been fully reviewed and tested, nor is there a Linux equivalent yet.&amp;nbsp; Another option may be to connect the NAND via UPM rather than FCM, but then you lose hardware ECC and the ability to boot from NAND.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please use a 2K-page NAND chip if at all possible.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2013 19:13:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230043#M258</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2013-01-18T19:13:01Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 NAND support</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230044#M259</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Also note that hardware ECC on eLBC FCM is limited to 1-bit correction per 512 data bytes, so if your NAND chip requires 4-bit ECC correction you'll have to use software ECC regardless.&amp;nbsp; Using software ECC with the eLBC FCM driver is not currently supported, though it should not be difficult to enable compared to dealing with the 4K page issue.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Jan 2013 19:19:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230044#M259</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2013-01-18T19:19:15Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 NAND support</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230045#M260</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, that helps.&amp;nbsp; Do you know if the Samsung K9K8G08UD0-SIB000 has software/hardware support for the P4080.&amp;nbsp; This is a 2K device that we already use for some i.mx5 apps.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Jan 2013 14:29:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230045#M260</guid>
      <dc:creator>dickginther</dc:creator>
      <dc:date>2013-01-28T14:29:00Z</dc:date>
    </item>
    <item>
      <title>Re: P4080 NAND support</title>
      <link>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230046#M261</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I don't have datasheets for specific NAND chips.&amp;nbsp; If it's a 2K-page device and only requires 1 bit of ECC per 512 data bytes, and is 8-bit wide, it should work -- barring any unexpected weirdness, of course.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Jan 2013 01:13:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P4080-NAND-support/m-p/230046#M261</guid>
      <dc:creator>scottwood</dc:creator>
      <dc:date>2013-01-29T01:13:47Z</dc:date>
    </item>
  </channel>
</rss>