<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P1016 DDR ECC testing</title>
    <link>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424673#M2412</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a better way to do this? Verify the generation of the machine check exception for a DDR ECC error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed the address parity error injection suggests it only generates one error. So would this prevent a seconds MCE occurring?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 23 Jul 2015 08:06:51 GMT</pubDate>
    <dc:creator>PaulWalker</dc:creator>
    <dc:date>2015-07-23T08:06:51Z</dc:date>
    <item>
      <title>P1016 DDR ECC testing</title>
      <link>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424671#M2410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to test out DDR ECC on a P1016 based board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I single-bit error scenarios all seems ok - the &lt;SPAN style="font-size: 11.0pt; font-family: 'Calibri','sans-serif';"&gt;DDR_ERR_SBE register happily counts the error occurences.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When inducing multi-bit errors, I expected a machine check exception. However the core just seems to hang.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor set-up bascally as below.&lt;/P&gt;&lt;P&gt;IVOR1 installed&lt;/P&gt;&lt;P&gt;HID1[RFXE]=1&lt;/P&gt;&lt;P&gt;DDR_ERR_DISABLE = 0&lt;/P&gt;&lt;P&gt;DDR_DDR_SDRAM_CFG[ECC_EN] = 1&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mulit-bit error injection&lt;/P&gt;&lt;P&gt;DDR_ERR_INJECT[EIEN] = 1&lt;/P&gt;&lt;P&gt;DDR_DATA_ERR_INJECT_HI = 0x00000003&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp; {processor hangs}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All seems to align with E500 and P1025 reference manual.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Am I doing something wrong?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2015 15:01:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424671#M2410</guid>
      <dc:creator>PaulWalker</dc:creator>
      <dc:date>2015-07-20T15:01:42Z</dc:date>
    </item>
    <item>
      <title>Re: P1016 DDR ECC testing</title>
      <link>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424672#M2411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Most probably the core enters into checkstop state. This happens when a machine check exeption (MCE) occurs while MSR[ME] bit is cleared. Typical scenaio is when second MCE occurs while previous MCE is being processed in the interrupt handler.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 21 Jul 2015 05:25:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424672#M2411</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-07-21T05:25:44Z</dc:date>
    </item>
    <item>
      <title>Re: P1016 DDR ECC testing</title>
      <link>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424673#M2412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a better way to do this? Verify the generation of the machine check exception for a DDR ECC error.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I noticed the address parity error injection suggests it only generates one error. So would this prevent a seconds MCE occurring?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Paul&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Jul 2015 08:06:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424673#M2412</guid>
      <dc:creator>PaulWalker</dc:creator>
      <dc:date>2015-07-23T08:06:51Z</dc:date>
    </item>
    <item>
      <title>Re: P1016 DDR ECC testing</title>
      <link>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424674#M2413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;As I can see HID1[RFXE]=1 in your case. Did you try keep it 0 (HID1[RFXE]=0)? Potentially this can be the root of the second MCE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Bulat&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Jul 2015 14:16:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1016-DDR-ECC-testing/m-p/424674#M2413</guid>
      <dc:creator>Bulat</dc:creator>
      <dc:date>2015-07-30T14:16:41Z</dc:date>
    </item>
  </channel>
</rss>