<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックRe: P2020DS Image creation using SDK 1.8</title>
    <link>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424233#M2406</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yiping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your inputs. I've been trying to port SDK 1.8 for P2020DS and have been partially successful. As mentioned earlier I was able to create kernel but u-boot never got created and same fails the rootfs creation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would appreciate if you could tell me what and where i need to be looking at exactly for a successful port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jyotisankar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 29 Jul 2015 10:04:45 GMT</pubDate>
    <dc:creator>jyotisankarpand</dc:creator>
    <dc:date>2015-07-29T10:04:45Z</dc:date>
    <item>
      <title>P2020DS Image creation using SDK 1.8</title>
      <link>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424231#M2404</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to create the images using Linux SDK 1.8 for P2020DS baord. This board support was removed from 1.8 SDK but after going through the community web pages, i created a .conf file and was able to partially create the image. I've certain issues which i would like some help with.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1. When i ran bitbake fsl-image-minimal/core it worked fine without any error, but inside the images/p2020ds directory i can see u-boot files missing completely.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2. When i run bitbake fsl-image-full i end up in having following error while creating the rootfs.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ERROR: u-boot-qoriq-images not found in the base feeds (p2020ds ppce500v2 noarch any all).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm kind of new to all this and trying to learn as much as possible from on-line but not able to have any luck yet, any help is appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Panda&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Jul 2015 11:00:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424231#M2404</guid>
      <dc:creator>jyotisankarpand</dc:creator>
      <dc:date>2015-07-20T11:00:43Z</dc:date>
    </item>
    <item>
      <title>Re: P2020DS Image creation using SDK 1.8</title>
      <link>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424232#M2405</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello &lt;SPAN class="replyToName"&gt;Jyotisankar Panda,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;This is because P2020DS is not included in SDK 1.8 u-boot source code at all, in the folders configs, include/configs/ and board/freescale/, there are no P2020DS supporting.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Actually P2020DS has already been removed since SDK 1.2 release.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;If it is necessary for you to use SDK 1.8, you have to do the porting by yourself according P2020DS source code provided previously.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;If you are doing target board bringing up, you also could refer to P2020RDB, which is supported in SDK 1.8.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN class="replyToName"&gt;Previously other customers asked similar questions, you could refer to &lt;A href="https://community.nxp.com/message/450354"&gt;Problem booting P2020DS with SDK 1.6 images.&lt;/A&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Yiping&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Jul 2015 10:34:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424232#M2405</guid>
      <dc:creator>yipingwang</dc:creator>
      <dc:date>2015-07-22T10:34:38Z</dc:date>
    </item>
    <item>
      <title>Re: P2020DS Image creation using SDK 1.8</title>
      <link>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424233#M2406</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Yiping,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your inputs. I've been trying to port SDK 1.8 for P2020DS and have been partially successful. As mentioned earlier I was able to create kernel but u-boot never got created and same fails the rootfs creation.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I would appreciate if you could tell me what and where i need to be looking at exactly for a successful port.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Jyotisankar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Jul 2015 10:04:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P2020DS-Image-creation-using-SDK-1-8/m-p/424233#M2406</guid>
      <dc:creator>jyotisankarpand</dc:creator>
      <dc:date>2015-07-29T10:04:45Z</dc:date>
    </item>
  </channel>
</rss>