<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックP1015 Performance Monitoring - is sample driver code available for enabling and displaying the Performance Monitoring data specifically for PCIe/</title>
    <link>https://community.nxp.com/t5/P-Series/P1015-Performance-Monitoring-is-sample-driver-code-available-for/m-p/406635#M2290</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to get PCIe utilization using the performance monitoring capabilities on the P1015 processor (we are running VxWorks 6.9).&amp;nbsp; If sample code for enabling and displaying this data can be provided, that would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Randy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 12 Nov 2015 22:24:37 GMT</pubDate>
    <dc:creator>rhilderman</dc:creator>
    <dc:date>2015-11-12T22:24:37Z</dc:date>
    <item>
      <title>P1015 Performance Monitoring - is sample driver code available for enabling and displaying the Performance Monitoring data specifically for PCIe/</title>
      <link>https://community.nxp.com/t5/P-Series/P1015-Performance-Monitoring-is-sample-driver-code-available-for/m-p/406635#M2290</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We are trying to get PCIe utilization using the performance monitoring capabilities on the P1015 processor (we are running VxWorks 6.9).&amp;nbsp; If sample code for enabling and displaying this data can be provided, that would be appreciated.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Randy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Nov 2015 22:24:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1015-Performance-Monitoring-is-sample-driver-code-available-for/m-p/406635#M2290</guid>
      <dc:creator>rhilderman</dc:creator>
      <dc:date>2015-11-12T22:24:37Z</dc:date>
    </item>
    <item>
      <title>Re: P1015 Performance Monitoring - is sample driver code available for enabling and displaying the Performance Monitoring data specifically for PCIe/</title>
      <link>https://community.nxp.com/t5/P-Series/P1015-Performance-Monitoring-is-sample-driver-code-available-for/m-p/406636#M2291</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;You can make use of performance monitor hardware from scratch.&lt;/P&gt;&lt;P&gt;&lt;A class="jive-link-external-small" href="http://cache.freescale.com/files/32bit/doc/app_note/AN3636.pdf" rel="nofollow"&gt;http://cache.freescale.com/files/32bit/doc/app_note/AN3636.pdf&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The e500 performance monitor driver exists in the kernel. The core API is in arch/powerpc/perf/core-fsl-emb.c and e500 related stuff is in arch/powerpc/perf/e500-pmu.c.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bare-board example in CodeWarrior PA:&lt;/P&gt;&lt;P&gt;&amp;lt;CodeWarrior&amp;gt;\PA\CodeWarrior_Examples\Bareboard_Examples\e500mcPerformanceMonitor_eabi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Pavel&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Nov 2015 08:22:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/P1015-Performance-Monitoring-is-sample-driver-code-available-for/m-p/406636#M2291</guid>
      <dc:creator>LPP</dc:creator>
      <dc:date>2015-11-13T08:22:35Z</dc:date>
    </item>
  </channel>
</rss>