<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>P-SeriesのトピックECC Support on P2020rdb</title>
    <link>https://community.nxp.com/t5/P-Series/ECC-Support-on-P2020rdb/m-p/401577#M2239</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the P2020rdb from Freescale with VxWorks 6.9 and a compatible current BSP from WindRiver. When I want to activted the ECC support the boot loader did not boot anymore. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question: Is the P2020rdb ready to use the ECC feature or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ask because I found this comment in the VxWorks BSP: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* possibly this is not supported check your DDR undefined for safety */&lt;/P&gt;&lt;P&gt;#undef&amp;nbsp; INCLUDE_DDR_ECC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the P2020RDB-PCA&amp;nbsp; Rev B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 15 Oct 2015 11:05:07 GMT</pubDate>
    <dc:creator>aratarorome</dc:creator>
    <dc:date>2015-10-15T11:05:07Z</dc:date>
    <item>
      <title>ECC Support on P2020rdb</title>
      <link>https://community.nxp.com/t5/P-Series/ECC-Support-on-P2020rdb/m-p/401577#M2239</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I use the P2020rdb from Freescale with VxWorks 6.9 and a compatible current BSP from WindRiver. When I want to activted the ECC support the boot loader did not boot anymore. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;My question: Is the P2020rdb ready to use the ECC feature or not?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I ask because I found this comment in the VxWorks BSP: &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;/* possibly this is not supported check your DDR undefined for safety */&lt;/P&gt;&lt;P&gt;#undef&amp;nbsp; INCLUDE_DDR_ECC&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have the P2020RDB-PCA&amp;nbsp; Rev B.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Andreas&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 15 Oct 2015 11:05:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/ECC-Support-on-P2020rdb/m-p/401577#M2239</guid>
      <dc:creator>aratarorome</dc:creator>
      <dc:date>2015-10-15T11:05:07Z</dc:date>
    </item>
    <item>
      <title>Re: ECC Support on P2020rdb</title>
      <link>https://community.nxp.com/t5/P-Series/ECC-Support-on-P2020rdb/m-p/401578#M2240</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The P2020RDB-PCA rev.B is not ready to use the ECC feature. It has 64-bit DDR memory (4 x 16-bit DDR devices). There is not DDR memory device for ECC on the P2020rdb nor place to install it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 18 Oct 2015 16:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/P-Series/ECC-Support-on-P2020rdb/m-p/401578#M2240</guid>
      <dc:creator>r8070z</dc:creator>
      <dc:date>2015-10-18T16:27:16Z</dc:date>
    </item>
  </channel>
</rss>